Represents an External Route configuration.
Public Attributes#
The IPv6 prefix.
uint16_t
The border router's RLOC16 (value ignored on config add).
signed int
A 2-bit signed int preference (OT_ROUTE_PREFERENCE_* values). 
bool
Whether this is a NAT64 prefix.
bool
Whether this configuration is considered Stable Network Data.
bool
Whether the next hop is this device (value ignored on config add).
bool
Whether or not BR is advertising a ULA prefix in PIO (AP flag).
Public Attribute Documentation#
mRloc16#
uint16_t otExternalRouteConfig::mRloc16
The border router's RLOC16 (value ignored on config add).
mPreference#
signed int otExternalRouteConfig::mPreference
A 2-bit signed int preference (OT_ROUTE_PREFERENCE_* values). 
mStable#
bool otExternalRouteConfig::mStable
Whether this configuration is considered Stable Network Data.
mNextHopIsThisDevice#
bool otExternalRouteConfig::mNextHopIsThisDevice
Whether the next hop is this device (value ignored on config add).
mAdvPio#
bool otExternalRouteConfig::mAdvPio
Whether or not BR is advertising a ULA prefix in PIO (AP flag).