You are viewing documentation for version:
Represents the IP level counters. 
Public Attributes#
uint32_t
The number of IPv6 packets successfully transmitted. 
uint32_t
The number of IPv6 packets successfully received. 
uint32_t
The number of IPv6 packets failed to transmit. 
uint32_t
The number of IPv6 packets failed to receive. 
Public Attribute Documentation#
mTxSuccess#
uint32_t otIpCounters::mTxSuccess
The number of IPv6 packets successfully transmitted. 
mRxSuccess#
uint32_t otIpCounters::mRxSuccess
The number of IPv6 packets successfully received. 
mTxFailure#
uint32_t otIpCounters::mTxFailure
The number of IPv6 packets failed to transmit. 
mRxFailure#
uint32_t otIpCounters::mRxFailure
The number of IPv6 packets failed to receive.