You are viewing documentation for version:
Represents the MLE Parent Response data. 
Public Attributes#
IEEE 802.15.4 Extended Address of the Parent. 
uint16_t
Short address of the Parent. 
bool
Is the node receiving parent response attached. 
Public Attribute Documentation#
mExtAddr#
otExtAddress otThreadParentResponseInfo::mExtAddr
IEEE 802.15.4 Extended Address of the Parent. 
mRloc16#
uint16_t otThreadParentResponseInfo::mRloc16
Short address of the Parent. 
mRssi
int8_t otThreadParentResponseInfo::mRssi
Rssi of the Parent. 
mPriority#
int8_t otThreadParentResponseInfo::mPriority
Parent priority. 
mLinkQuality3#
uint8_t otThreadParentResponseInfo::mLinkQuality3
Parent Link Quality 3. 
mLinkQuality2#
uint8_t otThreadParentResponseInfo::mLinkQuality2
Parent Link Quality 2. 
mLinkQuality1#
uint8_t otThreadParentResponseInfo::mLinkQuality1
Parent Link Quality 1. 
mIsAttached#
bool otThreadParentResponseInfo::mIsAttached
Is the node receiving parent response attached.