Holds diagnostic information for a neighboring Thread node.
Public Attributes#
IEEE 802.15.4 Extended Address.
uint32_t
Seconds since last heard.
uint32_t
Seconds since link establishment (requires CONFIG_UPTIME_ENABLE) 
uint16_t
RLOC16.
uint32_t
Link Frame Counter.
uint32_t
MLE Frame Counter.
uint8_t
Link Quality In.
int8_t
Average RSSI.
int8_t
Last observed RSSI.
uint8_t
Link Margin.
uint16_t
Frame error rate (0xffff->100%). Requires error tracking feature.
uint16_t
(IPv6) msg error rate (0xffff->100%). Requires error tracking feature.
uint16_t
Thread version of the neighbor.
bool
rx-on-when-idle
bool
Full Thread Device.
bool
Full Network Data.
bool
Is the neighbor a child.
Public Attribute Documentation#
mConnectionTime#
uint32_t otNeighborInfo::mConnectionTime
Seconds since link establishment (requires CONFIG_UPTIME_ENABLE) 
mFrameErrorRate#
uint16_t otNeighborInfo::mFrameErrorRate
Frame error rate (0xffff->100%). Requires error tracking feature.
mMessageErrorRate#
uint16_t otNeighborInfo::mMessageErrorRate
(IPv6) msg error rate (0xffff->100%). Requires error tracking feature.