You are viewing documentation for version:
Holds diagnostic information for a Thread Router. 
Public Attributes#
IEEE 802.15.4 Extended Address. 
bool
Router ID allocated or not. 
bool
Link established with Router ID or not. 
uint8_t
Parent CSL parameters are only relevant when OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE is enabled. 
uint8_t
CSL uncertainty, in ±10 us. 
Public Attribute Documentation#
mExtAddress#
otExtAddress otRouterInfo::mExtAddress
IEEE 802.15.4 Extended Address. 
mRloc16#
uint16_t otRouterInfo::mRloc16
RLOC16. 
mRouterId#
uint8_t otRouterInfo::mRouterId
Router ID. 
mNextHop#
uint8_t otRouterInfo::mNextHop
Next hop to router. 
mPathCost#
uint8_t otRouterInfo::mPathCost
Path cost to router. 
mLinkQualityIn#
uint8_t otRouterInfo::mLinkQualityIn
Link Quality In. 
mLinkQualityOut#
uint8_t otRouterInfo::mLinkQualityOut
Link Quality Out. 
mAge#
uint8_t otRouterInfo::mAge
Time last heard. 
mAllocated#
bool otRouterInfo::mAllocated
Router ID allocated or not. 
mLinkEstablished#
bool otRouterInfo::mLinkEstablished
Link established with Router ID or not. 
mVersion#
uint8_t otRouterInfo::mVersion
Thread version. 
mCslClockAccuracy#
uint8_t otRouterInfo::mCslClockAccuracy
Parent CSL parameters are only relevant when OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE is enabled. 
CSL clock accuracy, in ± ppm 
mCslUncertainty#
uint8_t otRouterInfo::mCslUncertainty
CSL uncertainty, in ±10 us.