You are viewing documentation for version:
PDFHolds diagnostic information for a Thread Router.
Public Attributes#
IEEE 802.15.4 Extended Address.
bool
Router ID allocated or not.
bool
Link established with Router ID or not.
uint8_t
Parent CSL parameters are only relevant when OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE is enabled.
uint8_t
CSL uncertainty, in ±10 us.
Public Attribute Documentation#
mExtAddress#
otExtAddress otRouterInfo::mExtAddress
IEEE 802.15.4 Extended Address.
mRloc16#
uint16_t otRouterInfo::mRloc16
RLOC16.
mRouterId#
uint8_t otRouterInfo::mRouterId
Router ID.
mNextHop#
uint8_t otRouterInfo::mNextHop
Next hop to router.
mPathCost#
uint8_t otRouterInfo::mPathCost
Path cost to router.
mLinkQualityIn#
uint8_t otRouterInfo::mLinkQualityIn
Link Quality In.
mLinkQualityOut#
uint8_t otRouterInfo::mLinkQualityOut
Link Quality Out.
mAge#
uint8_t otRouterInfo::mAge
Time last heard.
mAllocated#
bool otRouterInfo::mAllocated
Router ID allocated or not.
mLinkEstablished#
bool otRouterInfo::mLinkEstablished
Link established with Router ID or not.
mVersion#
uint8_t otRouterInfo::mVersion
Thread version.
mCslClockAccuracy#
uint8_t otRouterInfo::mCslClockAccuracy
Parent CSL parameters are only relevant when OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE is enabled.
CSL clock accuracy, in ± ppm
mCslUncertainty#
uint8_t otRouterInfo::mCslUncertainty
CSL uncertainty, in ±10 us.