You are viewing documentation for version:
PDFRepresents the MLE Parent Response data.
Public Attributes#
IEEE 802.15.4 Extended Address of the Parent.
uint16_t
Short address of the Parent.
bool
Is the node receiving parent response attached.
Public Attribute Documentation#
mExtAddr#
otExtAddress otThreadParentResponseInfo::mExtAddr
IEEE 802.15.4 Extended Address of the Parent.
mRloc16#
uint16_t otThreadParentResponseInfo::mRloc16
Short address of the Parent.
mRssi
int8_t otThreadParentResponseInfo::mRssi
Rssi of the Parent.
mPriority#
int8_t otThreadParentResponseInfo::mPriority
Parent priority.
mLinkQuality3#
uint8_t otThreadParentResponseInfo::mLinkQuality3
Parent Link Quality 3.
mLinkQuality2#
uint8_t otThreadParentResponseInfo::mLinkQuality2
Parent Link Quality 2.
mLinkQuality1#
uint8_t otThreadParentResponseInfo::mLinkQuality1
Parent Link Quality 1.
mIsAttached#
bool otThreadParentResponseInfo::mIsAttached
Is the node receiving parent response attached.