Data Structures
Here are the data structures with brief descriptions:
| RAIL_AddrConfig_t | A structure to configure the address filtering functionality in RAIL |
| RAIL_AntennaConfig_t | Configuration for Antenna switch pins |
| RAIL_AutoAckConfig_t | Enables/disables the auto ACK algorithm, based on "enable" |
| RAIL_BLE_State_t | State structure for BLE |
| RAIL_CalValues_t | Calibration value structure |
| RAIL_ChannelConfig_t | Channel configuration structure, which defines the channel meaning when a channel number is passed into a RAIL function, e.g., RAIL_StartTx() and RAIL_StartRx() |
| RAIL_ChannelConfigEntry_t | Channel configuration entry structure, which defines a channel range and parameters across which a corresponding radio configuration is valid |
| RAIL_ChannelConfigEntryAttr_t | Channel configuration entry attribute structure |
| RAIL_Config_t | RAIL configuration and internal state structure |
| RAIL_CsmaConfig_t | Configuration structure for the CSMA transmit algorithm |
| RAIL_DataConfig_t | RAIL data configuration structure |
| RAIL_FrameType_t | Configure if there is a frame type in your frame and the lengths of each frame |
| RAIL_IEEE802154_AddrConfig_t | Configuration structure for IEEE 802.15.4 Address Filtering |
| RAIL_IEEE802154_Address_t | Representation of 802.15.4 address This structure is only used for a received address, which needs to be parsed to discover the type |
| RAIL_IEEE802154_Config_t | Configuration structure for IEEE 802.15.4 in RAIL |
| RAIL_LbtConfig_t | Configuration structure for the LBT transmit algorithm |
| RAIL_MultiTimer_t | RAIL timer state structure |
| RAIL_PacketTimeStamp_t | Information needed to calculate and represent a packet timestamp |
| RAIL_PtiConfig_t | Configuration for PTI |
| RAIL_RxPacketDetails_t | Successfully received packet details obtained via RAIL_GetRxPacketDetails() |
| RAIL_RxPacketInfo_t | Basic information about a packet being received or already completed and awaiting processing, including memory pointers to its data in the circular RX FIFO buffer |
| RAIL_SchedulerInfo_t | A structure to hold information used by the scheduler |
| RAIL_ScheduleRxConfig_t | Configures the scheduled RX algorithm |
| RAIL_ScheduleTxConfig_t | Configuration structure for a scheduled transmit |
| RAIL_StateTiming_t | Timing configuration structure for the RAIL State Machine |
| RAIL_StateTransitions_t | Used to specify radio states to transition to on success or failure |
| RAIL_TxPacketDetails_t | Detailed information requested and about the packet that was just transmitted |
| RAIL_TxPowerConfig_t | Structure containing values used to initialize the power amplifiers |
| RAIL_VerifyConfig_t | The configuration array provided to RAIL for use by the radio state verification feature |
| RAIL_Version_t | Contains RAIL Library Version Information |
| RAILSched_Config_t | Multiprotocol scheduler configuration and internal state |