General
Basic APIs to set up and interact with the RAIL library.
Data Structures |
|
| struct | RAIL_Version_t |
|
Contains RAIL Library Version Information.
|
|
| struct | RAIL_Config_t |
|
RAIL configuration and internal state structure.
|
|
Macros |
|
| #define | RAIL_STATE_UINT32_BUFFER_SIZE 70 |
|
The size, in 32-bit words, of RAIL_StateBuffer_t to store RAIL internal state.
|
|
Typedefs |
|
| typedef void * | RAIL_Handle_t |
|
Handle of a RAIL instance, as returned from
RAIL_Init()
.
|
|
| typedef uint32_t | RAIL_StateBuffer_t [70] |
|
A buffer to store RAIL internal state.
|
|
| typedef void(* | RAIL_InitCompleteCallbackPtr_t ) ( RAIL_Handle_t railHandle) |
|
A pointer to init complete callback function.
|
|
Enumerations |
|
| enum |
RAIL_Status_t
{
RAIL_STATUS_NO_ERROR , RAIL_STATUS_INVALID_PARAMETER , RAIL_STATUS_INVALID_STATE , RAIL_STATUS_INVALID_CALL , RAIL_STATUS_SUSPENDED } |
|
Status returned by many RAIL API calls indicating their success or failure.
|
|
Functions |
|
| void | RAIL_GetVersion ( RAIL_Version_t *version, bool verbose) |
|
Gets the version information for the compiled RAIL library.
|
|
| RAIL_Handle_t | RAIL_Init ( RAIL_Config_t *railCfg, RAIL_InitCompleteCallbackPtr_t cb) |
|
Initializes RAIL.
|
|
| uint16_t | RAIL_GetRadioEntropy ( RAIL_Handle_t railHandle, uint8_t *buffer, uint16_t bytes) |
|
Collects entropy from the radio if available.
|
|
Detailed Description
Basic APIs to set up and interact with the RAIL library.
Typedef Documentation
◆ RAIL_InitCompleteCallbackPtr_t
| typedef void(* RAIL_InitCompleteCallbackPtr_t) ( RAIL_Handle_t railHandle) |
A pointer to init complete callback function.
- Parameters
-
[in] railHandleA handle for RAIL instance.
- Returns
- void.
Definition at line
772
of file
rail_types.h
.
Enumeration Type Documentation
◆ RAIL_Status_t
| enum RAIL_Status_t |
Status returned by many RAIL API calls indicating their success or failure.
Definition at line
701
of file
rail_types.h
.
Function Documentation
◆ RAIL_GetRadioEntropy()
| uint16_t RAIL_GetRadioEntropy | ( | RAIL_Handle_t |
railHandle,
|
| uint8_t * |
buffer,
|
||
| uint16_t |
bytes
|
||
| ) |
Collects entropy from the radio if available.
- Parameters
-
[in] railHandleA RAIL instance handle. [out] bufferThe buffer to write the collected entropy. [in] bytesThe number of bytes to fill in in the input buffer.
- Returns
- Returns the number of bytes of entropy collected. For chips that don't support entropy collection, the function returns 0. Values less than the requested amount may also be returned on platforms that use entropy pools to collect random data periodically.
Attempts to fill the provided buffer with the requested number of bytes of entropy. If the requested number of bytes can't be provided, as many bytes as possible will be filled and returned. For chips that do not support this function, 0 bytes will always be returned. For information about the specific mechanism for gathering entropy, see documentation for the chip family.
◆ RAIL_GetVersion()
| void RAIL_GetVersion | ( | RAIL_Version_t * |
version,
|
| bool |
verbose
|
||
| ) |
Gets the version information for the compiled RAIL library.
- Parameters
-
[out] versionA pointer to RAIL_Version_t structure to populate with version information. [in] verbosePopulate RAIL_Version_t struct with verbose information.
- Returns
- void.
The version information contains a major version number, a minor version number, and a rev (revision) number.
◆ RAIL_Init()
| RAIL_Handle_t RAIL_Init | ( | RAIL_Config_t * |
railCfg,
|
| RAIL_InitCompleteCallbackPtr_t |
cb
|
||
| ) |
Initializes RAIL.
- Parameters
-
[in,out] railCfgThe configuration and state structure for setting up the library, which contains memory and other options needed by RAIL. This structure must be allocated in application global read-write memory. RAIL may modify fields within or referenced by this structure during its operation. [in] cbA callback that notifies the application when the radio is finished initializing and is ready for further configuration. This callback is useful for potential transceiver products that require a power up sequence before further configuration is available. After the callback fires, the radio is ready for additional configuration before transmit and receive operations.
- Returns
- Handle for initialized rail instance or NULL if an invalid value was passed in the railCfg.