Calibration
APIs for calibrating the radio.
Modules |
|
| EFR32 | |
|
EFR32 Specific CalibrationsThe EFR32 has two supported calibrations.
|
|
Typedefs |
|
| typedef uint32_t | RAIL_CalMask_t |
|
Calibration mask type.
|
|
Functions |
|
| RAIL_Status_t | RAIL_ConfigCal ( RAIL_Handle_t railHandle, RAIL_CalMask_t calEnable) |
|
Initialize RAIL Calibration.
|
|
| RAIL_Status_t | RAIL_Calibrate ( RAIL_Handle_t railHandle, RAIL_CalValues_t *calValues, RAIL_CalMask_t calForce) |
|
Starts the calibration process.
|
|
| RAIL_CalMask_t | RAIL_GetPendingCal ( RAIL_Handle_t railHandle) |
|
Returns the current set of pending calibrations.
|
|
| void | RAIL_EnablePaCal (bool enable) |
|
Enable/Disable PA calibration.
|
|
Detailed Description
APIs for calibrating the radio.
These APIs can be used to calibrate the radio. The RAIL library determines which calibrations are necessary. Calibrations can be enabled/disabled with the RAIL_CalMask_t parameter.
Some calibrations produce values that can be saved and reapplied to save repetition of the calibration process.
Calibrations can either be run with RAIL_Calibrate , or with the individual chip-specific calibration routines. An example for running code with RAIL_Calibrate looks like:
Alternatively, if the image rejection calibration for your chip can be determined ahead of time, such as by running the calibration on a separate firmware image on each chip, then the following calibration process will result in smaller code.
Typedef Documentation
◆ RAIL_CalMask_t
Calibration mask type.
This type is a bitmask of different RAIL calibration values. The exact meaning of these bits depends on what a particular chip supports.
Definition at line
2160
of file
rail_types.h
.
Function Documentation
◆ RAIL_Calibrate()
| RAIL_Status_t RAIL_Calibrate | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_CalValues_t * |
calValues,
|
||
| RAIL_CalMask_t |
calForce
|
||
| ) |
Starts the calibration process.
- Parameters
-
[in] railHandleA RAIL instance handle. [in,out] calValuesA structure of calibration values to apply. If a valid calibration values structure is provided and the structure contains valid calibration values, those values will be applied to the hardware, and the RAIL library will cache those values for use again later. If a valid calibration values structure is provided and the structure contains a calibration value of RAIL_CAL_INVALID_VALUE for the desired calibration, the desired calibration will run, the calibration values structure will be updated with a valid calibration value, and the RAIL library will cache that value for use again later. If a NULL pointer is provided, the desired calibration will run, and the RAIL library will cache that value for use again later; however, the valid calibration value will not be returned to the application. [in] calForceA mask to force specific calibration(s) to execute. To run all pending calibrations, use the value RAIL_CAL_ALL_PENDING . Only the calibrations specified will run, even if not enabled during initialization.
- Returns
- Status code indicating success of the function call.
If calibrations were performed previously and the application saves the calibration values (i.e. call this function with a calibration values structure containing calibration values of RAIL_CAL_INVALID_VALUE before a reset), the application can later bypass the time it would normally take to recalibrate hardware by reusing previous calibration values (i.e. call this function with a calibration values structure containing valid calibration values after a reset).
If multiple protocols are used, this function will return RAIL_STATUS_INVALID_STATE if it is called and the given railHandle is not active. The caller must attempt to re-call this function later, in that case.
- Note
- Instead of this function, consider using the individual chip-specific functions. Using the individual functions will allow for better dead-stripping if not all calibrations are run.
- Some calibrations should only be executed when the radio is IDLE. See chip-specific documentation for more details.
Referenced by
RAIL_CopyRxPacket()
.
◆ RAIL_ConfigCal()
| RAIL_Status_t RAIL_ConfigCal | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_CalMask_t |
calEnable
|
||
| ) |
Initialize RAIL Calibration.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] calEnableA bitmask of which calibrations to enable for callback notification. The exact meaning of these bits is chip specific.
- Returns
- Status code indicating success of the function call.
Calibration initialization provides the calibration settings that correspond to the current radio configuration.
Referenced by
RAIL_CopyRxPacket()
.
◆ RAIL_EnablePaCal()
| void RAIL_EnablePaCal | ( | bool |
enable
|
) |
Enable/Disable PA calibration.
- Parameters
-
[in] enableEnables/Disables PA calibration
- Returns
- void.
Enabling this will ensure that the PA power remains constant chip to chip. By default this feature is disabled after reset.
- Note
- this function should be called before RAIL_ConfigTxPower() if this feature is desired.
Referenced by
RAIL_CopyRxPacket()
.
◆ RAIL_GetPendingCal()
| RAIL_CalMask_t RAIL_GetPendingCal | ( | RAIL_Handle_t |
railHandle
|
) |
Returns the current set of pending calibrations.
- Parameters
-
[in] railHandleA RAIL instance handle.
- Returns
- A mask of all pending calibrations that the user has been asked to perform.
This function returns a full set of pending calibrations. The only way to clear pending calibrations is to perform them using the RAIL_Calibrate() API with the appropriate list of calibrations.
Referenced by
RAIL_CopyRxPacket()
.