Enables/disables the auto ACK algorithm, based on "enable".
#include <
rail_types.h
>
Data Fields |
|
| bool | enable |
|
Indicate whether auto-acking should be enabled or disabled.
|
|
| uint16_t | ackTimeout |
|
Define the RX ACK timeout duration in µs.
|
|
| RAIL_StateTransitions_t | rxTransitions |
|
State transitions to do after receiving a packet.
|
|
| RAIL_StateTransitions_t | txTransitions |
|
State transitions to do after transmitting a packet.
|
|
Enables/disables the auto ACK algorithm, based on "enable".
The structure provides a default state (the "success" of tx/rxTransitions when acking is being enabled) for the radio to return to after an ACK operation occurs (transmitting or attempting to receive an ACK), or normal state transitions to return to in the case that acking is being disabled. Regardless whether the ACK operation was successful, the radio returns to the specified success state.
ackTimeout specifies how long to stay in receive and wait for an ACK before issuing a RAIL_EVENT_RX_ACK_TIMEOUT event and return to the default state.
Definition at line
2113
of file
rail_types.h
.
Field Documentation
◆ ackTimeout
| uint16_t RAIL_AutoAckConfig_t::ackTimeout |
Define the RX ACK timeout duration in µs.
Limited to a maximum 65.535 ms. Only applied when auto acking is enabled. Triggers a RAIL_EVENT_RX_ACK_TIMEOUT event if this threshold is exceeded.
Definition at line
2123
of file
rail_types.h
.
◆ rxTransitions
| RAIL_StateTransitions_t RAIL_AutoAckConfig_t::rxTransitions |
State transitions to do after receiving a packet.
When auto acking is enabled, the "error" transition is always ignored and the radio will return to the "success" state after any acking sequence. See RAIL_ConfigAutoAck for more details on this.
Definition at line
2130
of file
rail_types.h
.
◆ txTransitions
| RAIL_StateTransitions_t RAIL_AutoAckConfig_t::txTransitions |
State transitions to do after transmitting a packet.
When auto acking is enabled, the "error" transition is always ignored and the radio will return to the "success" state after any acking sequence. See RAIL_ConfigAutoAck for more details on this.
Definition at line
2137
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h