Successfully received packet details obtained via RAIL_GetRxPacketDetails() .
#include <
rail_types.h
>
Data Fields |
|
| RAIL_PacketTimeStamp_t | timeReceived |
|
Timestamp of the received packet in the RAIL timebase.
|
|
| bool | crcPassed |
|
Indicates whether the CRC passed or failed for the receive packet.
|
|
| bool | isAck |
|
Indicates whether the received packet is an ACK.
|
|
| int8_t | rssi |
|
RSSI of the received packet in integer dBm.
|
|
| uint8_t | lqi |
|
Link quality indicator of the received packet.
|
|
| uint8_t | syncWordId |
|
For radios and PHY configurations that support multiple sync words, this number is the ID of the sync word that was used for this packet.
|
|
| uint8_t | subPhyId |
|
In configurations where the radio has the option of receiving a given packet in multiple ways, indicates which of the sub-PHY options was used to receive the packet.
|
|
| uint8_t | antennaId |
|
For configurations where the device has multiple antennas, indicates which antenna received the packets.
|
|
Successfully received packet details obtained via RAIL_GetRxPacketDetails() .
Definition at line
1969
of file
rail_types.h
.
Field Documentation
◆ antennaId
| uint8_t RAIL_RxPacketDetails_t::antennaId |
For configurations where the device has multiple antennas, indicates which antenna received the packets.
For hardware configurations with only one antenna, this will be set to the default of 0.
Definition at line
2014
of file
rail_types.h
.
◆ crcPassed
| bool RAIL_RxPacketDetails_t::crcPassed |
Indicates whether the CRC passed or failed for the receive packet.
It is set to 0 for fail and 1 for pass.
Definition at line
1979
of file
rail_types.h
.
◆ isAck
| bool RAIL_RxPacketDetails_t::isAck |
Indicates whether the received packet is an ACK.
An 'ACK' is defined as a packet received during the RX ACK window when auto ACK is enabled. Set to 0 if not an ACK, and 1 for an ACK. It is always 0 if auto ACK is not enabled.
Definition at line
1986
of file
rail_types.h
.
◆ lqi
| uint8_t RAIL_RxPacketDetails_t::lqi |
Link quality indicator of the received packet.
It is calculated as the average correlation for the first 8 symbols in a frame.
Definition at line
1996
of file
rail_types.h
.
◆ rssi
| int8_t RAIL_RxPacketDetails_t::rssi |
RSSI of the received packet in integer dBm.
It is latched when the sync word is detected for the packet.
Definition at line
1991
of file
rail_types.h
.
◆ subPhyId
| uint8_t RAIL_RxPacketDetails_t::subPhyId |
In configurations where the radio has the option of receiving a given packet in multiple ways, indicates which of the sub-PHY options was used to receive the packet.
Most radio configurations do not have this ability, and the subPhy is set to 0 in those cases.
Definition at line
2008
of file
rail_types.h
.
◆ timeReceived
| RAIL_PacketTimeStamp_t RAIL_RxPacketDetails_t::timeReceived |
Timestamp of the received packet in the RAIL timebase.
The time is the end of the sync word of the received packet.
Definition at line
1974
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h