Events
APIs related to events.
Macros |
|
| #define | RAIL_EVENTS_NONE 0ULL |
|
A value representing no events.
|
|
| #define | RAIL_EVENT_RSSI_AVERAGE_DONE (1ULL << RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT) |
|
Occurs when the hardware-averaged RSSI is done in response to
RAIL_StartAverageRssi()
to indicate that the hardware has completed averaging.
|
|
| #define | RAIL_EVENT_RX_ACK_TIMEOUT (1ULL << RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT) |
|
Occurs when the timeout for receiving an ACK packet has expired without receiving the expected ACK.
|
|
| #define | RAIL_EVENT_RX_FIFO_ALMOST_FULL (1ULL << RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT) |
|
Occurs when the number of bytes in the receive FIFO exceeds the configured threshold value.
|
|
| #define | RAIL_EVENT_RX_PACKET_RECEIVED (1ULL << RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT) |
|
Occurs whenever a packet is received with
RAIL_RX_PACKET_READY_SUCCESS
or
RAIL_RX_PACKET_READY_CRC_ERROR
.
|
|
| #define | RAIL_EVENT_RX_PREAMBLE_LOST (1ULL << RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT) |
|
Occurs when the radio has lost a preamble.
|
|
| #define | RAIL_EVENT_RX_PREAMBLE_DETECT (1ULL << RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT) |
|
Occurs when the radio has detected a preamble.
|
|
| #define | RAIL_EVENT_RX_SYNC1_DETECT (1ULL << RAIL_EVENT_RX_SYNC1_DETECT_SHIFT) |
|
Occurs when the first sync word is detected.
|
|
| #define | RAIL_EVENT_RX_SYNC2_DETECT (1ULL << RAIL_EVENT_RX_SYNC2_DETECT_SHIFT) |
|
Occurs when the second sync word is detected.
|
|
| #define | RAIL_EVENT_RX_FRAME_ERROR (1ULL << RAIL_EVENT_RX_FRAME_ERROR_SHIFT) |
|
Occurs when a receive is aborted with
RAIL_RX_PACKET_ABORT_CRC_ERROR
which only happens after any filtering has passed.
|
|
| #define | RAIL_EVENT_RX_FIFO_OVERFLOW (1ULL << RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT) |
|
Occurs when a receive is aborted with
RAIL_RX_PACKET_ABORT_OVERFLOW
due to RX buffer overflow.
|
|
| #define | RAIL_EVENT_RX_ADDRESS_FILTERED (1ULL << RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT) |
|
Occurs when a receive is aborted with
RAIL_RX_PACKET_ABORT_FILTERED
because its address does not match the filtering settings.
|
|
| #define | RAIL_EVENT_RX_TIMEOUT (1ULL << RAIL_EVENT_RX_TIMEOUT_SHIFT) |
|
Occurs when an RX event times out.
|
|
| #define | RAIL_EVENT_RX_SCHEDULED_RX_END (1ULL << RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT) |
|
Occurs when the scheduled RX window ends.
|
|
| #define | RAIL_EVENT_RX_PACKET_ABORTED (1ULL << RAIL_EVENT_RX_PACKET_ABORTED_SHIFT) |
|
Occurs when a receive is aborted during filtering with
RAIL_RX_PACKET_ABORT_FORMAT
or after filtering with
RAIL_RX_PACKET_ABORT_ABORTED
for reasons other than address filtering mismatch (which triggers
RAIL_EVENT_RX_ADDRESS_FILTERED
instead).
|
|
| #define | RAIL_EVENT_RX_FILTER_PASSED (1ULL << RAIL_EVENT_RX_FILTER_PASSED_SHIFT) |
|
Occurs when the packet has passed any configured address and frame filtering options.
|
|
| #define | RAIL_EVENT_RX_TIMING_LOST (1ULL << RAIL_EVENT_RX_TIMING_LOST_SHIFT) |
|
Occurs when the modem timing is lost.
|
|
| #define | RAIL_EVENT_RX_TIMING_DETECT (1ULL << RAIL_EVENT_RX_TIMING_DETECT_SHIFT) |
|
Occurs when the modem timing is detected.
|
|
| #define | RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE (1ULL << RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT) |
|
Occurs when RX Channel Hopping is enabled and channel hopping finishes receiving on the last channel in its sequence.
|
|
| #define | RAIL_EVENT_RX_DUTY_CYCLE_RX_END (1ULL << RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT) |
|
Occurs during RX duty cycle mode when the radio finishes its time in receive mode.
|
|
| #define | RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND (1ULL << RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT) |
|
Indicates a Data Request is received when using IEEE 802.15.4 functionality.
|
|
| #define | RAIL_EVENT_ZWAVE_BEAM (1ULL << RAIL_EVENT_ZWAVE_BEAM_SHIFT) |
|
Indicates a Z-Wave Beam Request relevant to the node was received.
|
|
| #define | RAIL_EVENTS_RX_COMPLETION |
|
The mask representing all events that determine the end of a received packet.
|
|
| #define | RAIL_EVENT_TX_FIFO_ALMOST_EMPTY (1ULL << RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT) |
|
Occurs when the number of bytes in the transmit FIFO falls below the configured threshold value.
|
|
| #define | RAIL_EVENT_TX_PACKET_SENT (1ULL << RAIL_EVENT_TX_PACKET_SENT_SHIFT) |
|
Occurs after a packet has been transmitted.
|
|
| #define | RAIL_EVENT_TXACK_PACKET_SENT (1ULL << RAIL_EVENT_TXACK_PACKET_SENT_SHIFT) |
|
Occurs after an ACK packet has been transmitted.
|
|
| #define | RAIL_EVENT_TX_ABORTED (1ULL << RAIL_EVENT_TX_ABORTED_SHIFT) |
|
Occurs when a transmit is aborted by the user.
|
|
| #define | RAIL_EVENT_TXACK_ABORTED (1ULL << RAIL_EVENT_TXACK_ABORTED_SHIFT) |
|
Occurs when an ACK transmit is aborted by the user.
|
|
| #define | RAIL_EVENT_TX_BLOCKED (1ULL << RAIL_EVENT_TX_BLOCKED_SHIFT) |
|
Occurs when a transmit is blocked from occurring because
RAIL_EnableTxHoldOff()
was called.
|
|
| #define | RAIL_EVENT_TXACK_BLOCKED (1ULL << RAIL_EVENT_TXACK_BLOCKED_SHIFT) |
|
Occurs when an ACK transmit is blocked from occurring because
RAIL_EnableTxHoldOff()
was called.
|
|
| #define | RAIL_EVENT_TX_UNDERFLOW (1ULL << RAIL_EVENT_TX_UNDERFLOW_SHIFT) |
|
Occurs when the transmit buffer underflows.
|
|
| #define | RAIL_EVENT_TXACK_UNDERFLOW (1ULL << RAIL_EVENT_TXACK_UNDERFLOW_SHIFT) |
|
Occurs when the ACK transmit buffer underflows.
|
|
| #define | RAIL_EVENT_TX_CHANNEL_CLEAR (1ULL << RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT) |
|
Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) succeeds.
|
|
| #define | RAIL_EVENT_TX_CHANNEL_BUSY (1ULL << RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT) |
|
Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) fails.
|
|
| #define | RAIL_EVENT_TX_CCA_RETRY (1ULL << RAIL_EVENT_TX_CCA_RETRY_SHIFT) |
|
Occurs during CSMA or LBT when an individual Clear Channel Assessment (CCA) check fails, but there are more tries needed before the overall operation completes.
|
|
| #define | RAIL_EVENT_TX_START_CCA (1ULL << RAIL_EVENT_TX_START_CCA_SHIFT) |
|
Occurs when a Clear Channel Assessment (CCA) check begins.
|
|
| #define | RAIL_EVENTS_TX_COMPLETION |
|
A mask representing all events that determine the end of a transmitted packet.
|
|
| #define | RAIL_EVENTS_TXACK_COMPLETION |
|
A mask representing all events that determine the end of a transmitted ACK packet.
|
|
| #define | RAIL_EVENT_CONFIG_UNSCHEDULED (1ULL << RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT) |
|
Occurs when the scheduler switches away from this configuration.
|
|
| #define | RAIL_EVENT_CONFIG_SCHEDULED (1ULL << RAIL_EVENT_CONFIG_SCHEDULED_SHIFT) |
|
Occurs when the scheduler switches to this configuration.
|
|
| #define | RAIL_EVENT_SCHEDULER_STATUS (1ULL << RAIL_EVENT_SCHEDULER_STATUS_SHIFT) |
|
Occurs when the scheduler has a status to report.
|
|
| #define | RAIL_EVENT_CAL_NEEDED (1ULL << RAIL_EVENT_CAL_NEEDED_SHIFT) |
|
Occurs when the application needs to run a calibration, as determined by the RAIL library.
|
|
| #define | RAIL_EVENTS_ALL 0xFFFFFFFFFFFFFFFFULL |
|
A value representing all possible events.
|
|
Functions |
|
| RAIL_Status_t | RAIL_ConfigEvents ( RAIL_Handle_t railHandle, RAIL_Events_t mask, RAIL_Events_t events) |
|
Configures radio events.
|
|
Detailed Description
APIs related to events.
Macro Definition Documentation
| #define RAIL_EVENT_CAL_NEEDED (1ULL << RAIL_EVENT_CAL_NEEDED_SHIFT) |
Occurs when the application needs to run a calibration, as determined by the RAIL library.
The application determines the opportune time to call RAIL_Calibrate() .
Definition at line
1072
of file
rail_types.h
.
| #define RAIL_EVENT_CONFIG_SCHEDULED (1ULL << RAIL_EVENT_CONFIG_SCHEDULED_SHIFT) |
Occurs when the scheduler switches to this configuration.
This event will occur in dynamic multiprotocol scenarios each time a protocol is starting up. When it does occur, it will be the only event passed to RAIL_Config_t::eventsCallback . Therefore, in order to optimize protocol switch time, this event should be handled among the first in that callback, and then the application can return immediately.
- Note
- : To minimize protocol switch time, Silicon Labs recommends this event event being turned off unless it is used.
Definition at line
1044
of file
rail_types.h
.
| #define RAIL_EVENT_CONFIG_UNSCHEDULED (1ULL << RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT) |
Occurs when the scheduler switches away from this configuration.
This event will occur in dynamic multiprotocol scenarios each time a protocol is shutting down. When it does occur, it will be the only event passed to RAIL_Config_t::eventsCallback . Therefore, in order to optimize protocol switch time, this event should be handled among the first in that callback, and then the application can return immediately.
- Note
- : To minimize protocol switch time, Silicon Labs recommends this event event being turned off unless it is used.
Definition at line
1030
of file
rail_types.h
.
| #define RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND (1ULL << RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT) |
Indicates a Data Request is received when using IEEE 802.15.4 functionality.
It occurs when the command byte of an incoming ACK-requesting MAC Control frame is for a data request. This callback is called before the packet is fully received to allow the node to have more time to decide whether to indicate a frame is pending in the outgoing ACK. This event only occurs if the RAIL IEEE 802.15.4 functionality is enabled, but will never occur if promiscuous mode is enabled via RAIL_IEEE802154_SetPromiscuousMode() .
Call RAIL_IEEE802154_GetAddress() to get the source address of the packet.
Definition at line
805
of file
rail_types.h
.
| #define RAIL_EVENT_RSSI_AVERAGE_DONE (1ULL << RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT) |
Occurs when the hardware-averaged RSSI is done in response to RAIL_StartAverageRssi() to indicate that the hardware has completed averaging.
Call RAIL_GetAverageRssi() to get the result.
Definition at line
597
of file
rail_types.h
.
| #define RAIL_EVENT_RX_ACK_TIMEOUT (1ULL << RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT) |
Occurs when the timeout for receiving an ACK packet has expired without receiving the expected ACK.
This event only occurs after calling RAIL_ConfigAutoAck() and after transmitting a packet with RAIL_TX_OPTION_WAIT_FOR_ACK set.
Definition at line
606
of file
rail_types.h
.
| #define RAIL_EVENT_RX_ADDRESS_FILTERED (1ULL << RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT) |
Occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_FILTERED because its address does not match the filtering settings.
This event can only occur after calling RAIL_EnableAddressFilter() .
Definition at line
694
of file
rail_types.h
.
| #define RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE (1ULL << RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT) |
Occurs when RX Channel Hopping is enabled and channel hopping finishes receiving on the last channel in its sequence.
The intent behind this event is to allow the user to keep the radio on for as short a time as possible. That is, once the channel sequence is complete, the application will receive this event and can trigger a sleep/idle until it is necessary to cycle through the channels again. If this event is left on indefinitely and not handled it will likely be a fairly noisy event, as it continues to fire each time the hopping algorithm cycles through the channel sequence.
Definition at line
780
of file
rail_types.h
.
| #define RAIL_EVENT_RX_DUTY_CYCLE_RX_END (1ULL << RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT) |
Occurs during RX duty cycle mode when the radio finishes its time in receive mode.
The application can then trigger a sleep/idle until it needs to listen again.
Definition at line
789
of file
rail_types.h
.
| #define RAIL_EVENT_RX_FIFO_ALMOST_FULL (1ULL << RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT) |
Occurs when the number of bytes in the receive FIFO exceeds the configured threshold value.
Call RAIL_GetRxFifoBytesAvailable() to get the number of bytes available. When using this event, the threshold should be set via RAIL_SetRxFifoThreshold() .
Definition at line
616
of file
rail_types.h
.
| #define RAIL_EVENT_RX_FIFO_OVERFLOW (1ULL << RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT) |
Occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_OVERFLOW due to RX buffer overflow.
This causes the radio to stop receiving packets until the packet causing the overflow is processed.
Definition at line
686
of file
rail_types.h
.
| #define RAIL_EVENT_RX_FILTER_PASSED (1ULL << RAIL_EVENT_RX_FILTER_PASSED_SHIFT) |
Occurs when the packet has passed any configured address and frame filtering options.
This event will only occur between the start of the packet, indicated by RAIL_EVENT_RX_SYNC1_DETECT or RAIL_EVENT_RX_SYNC2_DETECT and one of the events in the RAIL_EVENTS_RX_COMPLETION mask. It will always occur before or concurrently with RAIL_EVENT_RX_PACKET_RECEIVED . If IEEE 802.15.4 frame and address filtering are enabled, this event will occur immediately after destination address filtering.
Definition at line
748
of file
rail_types.h
.
| #define RAIL_EVENT_RX_FRAME_ERROR (1ULL << RAIL_EVENT_RX_FRAME_ERROR_SHIFT) |
Occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_CRC_ERROR which only happens after any filtering has passed.
For EFR32 parts, this event includes CRC errors, block decoding errors, and illegal frame length – when detected after filtering. (When such errors are detected during filtering, they're signalled as RAIL_EVENT_RX_PACKET_ABORTED instead.)
If RAIL_RX_OPTION_IGNORE_CRC_ERRORS is set, this event will not occur for CRC errors, but could still occur for the other errors.
Definition at line
677
of file
rail_types.h
.
| #define RAIL_EVENT_RX_PACKET_ABORTED (1ULL << RAIL_EVENT_RX_PACKET_ABORTED_SHIFT) |
Occurs when a receive is aborted during filtering with RAIL_RX_PACKET_ABORT_FORMAT or after filtering with RAIL_RX_PACKET_ABORT_ABORTED for reasons other than address filtering mismatch (which triggers RAIL_EVENT_RX_ADDRESS_FILTERED instead).
For EFR32 parts, this event includes CRC errors, block decoding errors, illegal frame length, and other RAIL built-in protocol-specific packet content errors – when detected during filtering. (When such errors are detected after filtering, they're signalled as RAIL_EVENT_RX_FRAME_ERROR instead.) It also includes application or multiprotocol scheduler aborting a receive after filtering has passed.
Definition at line
734
of file
rail_types.h
.
| #define RAIL_EVENT_RX_PACKET_RECEIVED (1ULL << RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT) |
Occurs whenever a packet is received with RAIL_RX_PACKET_READY_SUCCESS or RAIL_RX_PACKET_READY_CRC_ERROR .
Call RAIL_GetRxPacketInfo() to get basic information about the packet along with a handle to this packet for subsequent use with RAIL_PeekRxPacket() , RAIL_GetRxPacketDetails() , RAIL_HoldRxPacket() , and RAIL_ReleaseRxPacket() as needed.
Definition at line
627
of file
rail_types.h
.
| #define RAIL_EVENT_RX_PREAMBLE_DETECT (1ULL << RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT) |
Occurs when the radio has detected a preamble.
This event can occur multiple times while searching for a packet and is generally used for diagnostic purposes. It can only occur after a RAIL_EVENT_RX_TIMING_DETECT event has already occurred.
Definition at line
647
of file
rail_types.h
.
| #define RAIL_EVENT_RX_PREAMBLE_LOST (1ULL << RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT) |
Occurs when the radio has lost a preamble.
This event can occur multiple times while searching for a packet and is generally used for diagnostic purposes. It can only occur after a RAIL_EVENT_RX_PREAMBLE_DETECT event has already occurred.
Definition at line
637
of file
rail_types.h
.
| #define RAIL_EVENT_RX_SCHEDULED_RX_END (1ULL << RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT) |
Occurs when the scheduled RX window ends.
This event only occurs in response to a scheduled receive timeout after calling RAIL_ScheduleRx() . If RAIL_ScheduleRxConfig_t::rxTransitionEndSchedule was passed as false, this event will occur unless the receive is aborted (due to a call to RAIL_Idle() or a scheduler preemption, for instance). If RAIL_ScheduleRxConfig_t::rxTransitionEndSchedule was passed as true, any of the RAIL_EVENTS_RX_COMPLETION events occurring will also cause this event not to occur, since the scheduled receive will end with the transition at the end of the packet.
Definition at line
718
of file
rail_types.h
.
| #define RAIL_EVENT_RX_SYNC1_DETECT (1ULL << RAIL_EVENT_RX_SYNC1_DETECT_SHIFT) |
Occurs when the first sync word is detected.
After this event occurs, one of the events in the RAIL_EVENTS_RX_COMPLETION mask will occur.
Definition at line
655
of file
rail_types.h
.
| #define RAIL_EVENT_RX_SYNC2_DETECT (1ULL << RAIL_EVENT_RX_SYNC2_DETECT_SHIFT) |
Occurs when the second sync word is detected.
After this event occurs, one of the events in the RAIL_EVENTS_RX_COMPLETION mask will occur.
Definition at line
663
of file
rail_types.h
.
| #define RAIL_EVENT_RX_TIMEOUT (1ULL << RAIL_EVENT_RX_TIMEOUT_SHIFT) |
Occurs when an RX event times out.
This event can only occur if the RAIL_StateTiming_t::rxSearchTimeout passed to RAIL_SetStateTiming() is not zero.
Definition at line
703
of file
rail_types.h
.
| #define RAIL_EVENT_RX_TIMING_DETECT (1ULL << RAIL_EVENT_RX_TIMING_DETECT_SHIFT) |
Occurs when the modem timing is detected.
This event can occur multiple times while searching for a packet and is generally used for diagnostic purposes.
Definition at line
766
of file
rail_types.h
.
| #define RAIL_EVENT_RX_TIMING_LOST (1ULL << RAIL_EVENT_RX_TIMING_LOST_SHIFT) |
Occurs when the modem timing is lost.
This event can occur multiple times while searching for a packet and is generally used for diagnostic purposes. It can only occur after a RAIL_EVENT_RX_TIMING_DETECT event has already occurred.
Definition at line
758
of file
rail_types.h
.
| #define RAIL_EVENT_SCHEDULER_STATUS (1ULL << RAIL_EVENT_SCHEDULER_STATUS_SHIFT) |
Occurs when the scheduler has a status to report.
The exact status can be found with RAIL_GetSchedulerStatus() . See RAIL_SchedulerStatus_t for more details. When this event does occur, it will be the only event passed to RAIL_Config_t::eventsCallback . Therefore in order to optimize protocol switch time, this event should be handled among the first in that callback, and then the application can return immediately.
- Note
- RAIL_GetSchedulerStatus() is only valid to call during the time frame of the RAIL_Config_t::eventsCallback .
- : To minimize protocol switch time, Silicon Labs recommends this event event being turned off unless it is used.
Definition at line
1062
of file
rail_types.h
.
| #define RAIL_EVENT_TX_ABORTED (1ULL << RAIL_EVENT_TX_ABORTED_SHIFT) |
Occurs when a transmit is aborted by the user.
This can happen due to calling RAIL_Idle() or due to a scheduler preemption.
- Note
- The TX FIFO is left in an indeterminate state and should be reset prior to reuse for sending a new packet. Contrast this with RAIL_EVENT_TX_BLOCKED .
Definition at line
890
of file
rail_types.h
.
| #define RAIL_EVENT_TX_BLOCKED (1ULL << RAIL_EVENT_TX_BLOCKED_SHIFT) |
Occurs when a transmit is blocked from occurring because RAIL_EnableTxHoldOff() was called.
- Note
- Since the transmit never started, the TX FIFO remains intact after this event – no packet data was consumed from it. Contrast this with RAIL_EVENT_TX_ABORTED .
Definition at line
909
of file
rail_types.h
.
| #define RAIL_EVENT_TX_CCA_RETRY (1ULL << RAIL_EVENT_TX_CCA_RETRY_SHIFT) |
Occurs during CSMA or LBT when an individual Clear Channel Assessment (CCA) check fails, but there are more tries needed before the overall operation completes.
This event can occur multiple times based on the configuration of the ongoing CSMA or LBT transmission. It can only happen after calling RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx() .
Definition at line
971
of file
rail_types.h
.
| #define RAIL_EVENT_TX_CHANNEL_BUSY (1ULL << RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT) |
Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) fails.
This event can only happen after calling RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx() .
- Note
- Since the transmit never started, the TX FIFO remains intact after this event – no packet data was consumed from it.
Definition at line
960
of file
rail_types.h
.
| #define RAIL_EVENT_TX_CHANNEL_CLEAR (1ULL << RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT) |
Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) succeeds.
This event can only happen after calling RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx() .
Definition at line
948
of file
rail_types.h
.
| #define RAIL_EVENT_TX_FIFO_ALMOST_EMPTY (1ULL << RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT) |
Occurs when the number of bytes in the transmit FIFO falls below the configured threshold value.
This event does not occur on initialization or after resetting the transmit FIFO with RAIL_ResetFifo() .
Call RAIL_GetTxFifoSpaceAvailable() to get the number of bytes available in the transmit FIFO at the time of the callback dispatch. When using this event, the threshold should be set via RAIL_SetTxFifoThreshold() .
Definition at line
857
of file
rail_types.h
.
| #define RAIL_EVENT_TX_PACKET_SENT (1ULL << RAIL_EVENT_TX_PACKET_SENT_SHIFT) |
Occurs after a packet has been transmitted.
Call RAIL_GetTxPacketDetails() to get information about the packet that was transmitted.
- Note
- RAIL_GetTxPacketDetails() is only valid to call during the time frame of the RAIL_Config_t::eventsCallback .
Definition at line
867
of file
rail_types.h
.
| #define RAIL_EVENT_TX_START_CCA (1ULL << RAIL_EVENT_TX_START_CCA_SHIFT) |
Occurs when a Clear Channel Assessment (CCA) check begins.
This event can occur multiple times based on the configuration of the ongoing CSMA or LBT transmission. It can only happen after calling RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx() .
Definition at line
981
of file
rail_types.h
.
| #define RAIL_EVENT_TX_UNDERFLOW (1ULL << RAIL_EVENT_TX_UNDERFLOW_SHIFT) |
Occurs when the transmit buffer underflows.
This can happen due to the transmitted packet specifying an unintended length based on the current radio configuration or due to RAIL_WriteTxFifo() calls not keeping up with the transmit rate if the entire packet isn't loaded at once.
Definition at line
927
of file
rail_types.h
.
| #define RAIL_EVENT_TXACK_ABORTED (1ULL << RAIL_EVENT_TXACK_ABORTED_SHIFT) |
Occurs when an ACK transmit is aborted by the user.
This event can only occur after calling RAIL_ConfigAutoAck() , which can happen due to calling RAIL_Idle() or due to a scheduler preemption.
Definition at line
899
of file
rail_types.h
.
| #define RAIL_EVENT_TXACK_BLOCKED (1ULL << RAIL_EVENT_TXACK_BLOCKED_SHIFT) |
Occurs when an ACK transmit is blocked from occurring because RAIL_EnableTxHoldOff() was called.
This event can only occur after calling RAIL_ConfigAutoAck() .
Definition at line
917
of file
rail_types.h
.
| #define RAIL_EVENT_TXACK_PACKET_SENT (1ULL << RAIL_EVENT_TXACK_PACKET_SENT_SHIFT) |
Occurs after an ACK packet has been transmitted.
Call RAIL_GetTxPacketDetails() to get information about the packet that was transmitted. This event can only occur after calling RAIL_ConfigAutoAck() .
- Note
- RAIL_GetTxPacketDetails() is only valid to call during the time frame of the RAIL_Config_t::eventsCallback .
Definition at line
878
of file
rail_types.h
.
| #define RAIL_EVENT_TXACK_UNDERFLOW (1ULL << RAIL_EVENT_TXACK_UNDERFLOW_SHIFT) |
Occurs when the ACK transmit buffer underflows.
This can happen due to the transmitted packet specifying an unintended length based on the current radio configuration or due to RAIL_WriteAutoAckFifo() not being called at all before an ACK transmit.
This event can only occur after calling RAIL_ConfigAutoAck() .
Definition at line
939
of file
rail_types.h
.
| #define RAIL_EVENT_ZWAVE_BEAM (1ULL << RAIL_EVENT_ZWAVE_BEAM_SHIFT) |
Indicates a Z-Wave Beam Request relevant to the node was received.
This event only occurs if the RAIL Z-Wave functionality is enabled and its RAIL_ZWAVE_OPTION_DETECT_BEAM_FRAMES is enabled. This event is used in lieu of RAIL_EVENT_RX_PACKET_RECEIVED , which is reserved for Z-Wave packets other than Beams.
Call RAIL_ZWAVE_GetBeamNodeId() to get the NodeId to which the Beam was targeted, which would be either the broadcast id 0xFF or the node's own single-cast id.
- Note
- All Z-Wave Beam requests are generally discarded, triggering RAIL_EVENT_RX_PACKET_ABORTED .
Definition at line
822
of file
rail_types.h
.
| #define RAIL_EVENTS_RX_COMPLETION |
rail_types.h:677
rail_types.h:627
rail_types.h:694
rail_types.h:686
rail_types.h:734
The mask representing all events that determine the end of a received packet.
After a RAIL_EVENT_RX_SYNC1_DETECT or a RAIL_EVENT_RX_SYNC2_DETECT , exactly one of the following events will occur. When one of these events occurs, a state transition will take place based on the parameter passed to RAIL_SetRxTransitions() . The RAIL_StateTransitions_t::success transition will be followed only if the RAIL_EVENT_RX_PACKET_RECEIVED event occurs. Any of the other events will trigger the RAIL_StateTransitions_t::error transition.
Definition at line
837
of file
rail_types.h
.
| #define RAIL_EVENTS_TX_COMPLETION |
rail_types.h:927
rail_types.h:867
rail_types.h:909
rail_types.h:960
rail_types.h:890
A mask representing all events that determine the end of a transmitted packet.
After a RAIL_STATUS_NO_ERROR return value from one of the transmit functions, exactly one of the following events will occur. When one of these events occurs, a state transition takes place based on the parameter passed to RAIL_SetTxTransitions() . The RAIL_StateTransitions_t::success transition will be followed only if the RAIL_EVENT_TX_PACKET_SENT event occurs. Any of the other events will trigger the RAIL_StateTransitions_t::error transition.
Definition at line
993
of file
rail_types.h
.
| #define RAIL_EVENTS_TXACK_COMPLETION |
rail_types.h:878
rail_types.h:899
rail_types.h:939
rail_types.h:917
A mask representing all events that determine the end of a transmitted ACK packet.
After an ACK-requesting receive, exactly one of the following events will occur. When one of these events occurs, a state transition takes place based on the RAIL_AutoAckConfig_t::rxTransitions passed to RAIL_ConfigAutoAck() . The receive transitions are used because the transmitted ACK packet is considered a part of the ACK-requesting received packet. The RAIL_StateTransitions_t::success transition will be followed only if the RAIL_EVENT_TXACK_PACKET_SENT event occurs. Any of the other events will trigger the RAIL_StateTransitions_t::error transition.
Definition at line
1010
of file
rail_types.h
.
Enumeration Type Documentation
| enum RAIL_Events_t |
RAIL events passed to the event callback.
More than one event may be indicated due to interrupt latency.
| Enumerator | |
|---|---|
| RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT |
Shift position of RAIL_EVENT_RSSI_AVERAGE_DONE bit. |
| RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT |
Shift position of RAIL_EVENT_RX_ACK_TIMEOUT bit. |
| RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT |
Shift position of RAIL_EVENT_RX_FIFO_ALMOST_FULL bit. |
| RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT |
Shift position of RAIL_EVENT_RX_PACKET_RECEIVED bit. |
| RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT |
Shift position of RAIL_EVENT_RX_PREAMBLE_LOST bit. |
| RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT |
Shift position of RAIL_EVENT_RX_PREAMBLE_DETECT bit. |
| RAIL_EVENT_RX_SYNC1_DETECT_SHIFT |
Shift position of RAIL_EVENT_RX_SYNC1_DETECT bit. |
| RAIL_EVENT_RX_SYNC2_DETECT_SHIFT |
Shift position of RAIL_EVENT_RX_SYNC2_DETECT bit. |
| RAIL_EVENT_RX_FRAME_ERROR_SHIFT |
Shift position of RAIL_EVENT_RX_FRAME_ERROR bit. |
| RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT |
Shift position of RAIL_EVENT_RX_FIFO_OVERFLOW bit. |
| RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT |
Shift position of RAIL_EVENT_RX_ADDRESS_FILTERED bit. |
| RAIL_EVENT_RX_TIMEOUT_SHIFT |
Shift position of RAIL_EVENT_RX_TIMEOUT bit. |
| RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT |
Shift position of RAIL_EVENT_RX_SCHEDULED_RX_END bit. |
| RAIL_EVENT_RX_PACKET_ABORTED_SHIFT |
Shift position of RAIL_EVENT_RX_PACKET_ABORTED bit. |
| RAIL_EVENT_RX_FILTER_PASSED_SHIFT |
Shift position of RAIL_EVENT_RX_FILTER_PASSED bit. |
| RAIL_EVENT_RX_TIMING_LOST_SHIFT |
Shift position of RAIL_EVENT_RX_TIMING_LOST bit. |
| RAIL_EVENT_RX_TIMING_DETECT_SHIFT |
Shift position of RAIL_EVENT_RX_TIMING_DETECT bit. |
| RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT |
Shift position of RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE bit. |
| RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT |
Shift position of RAIL_EVENT_RX_DUTY_CYCLE_RX_END bit. |
| RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT |
Shift position of RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND bit. |
| RAIL_EVENT_ZWAVE_BEAM_SHIFT |
Shift position of RAIL_EVENT_ZWAVE_BEAM bit. |
| RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT |
Shift position of RAIL_EVENT_TX_FIFO_ALMOST_EMPTY bit. |
| RAIL_EVENT_TX_PACKET_SENT_SHIFT |
Shift position of RAIL_EVENT_TX_PACKET_SENT bit. |
| RAIL_EVENT_TXACK_PACKET_SENT_SHIFT |
Shift position of RAIL_EVENT_TXACK_PACKET_SENT bit. |
| RAIL_EVENT_TX_ABORTED_SHIFT |
Shift position of RAIL_EVENT_TX_ABORTED bit. |
| RAIL_EVENT_TXACK_ABORTED_SHIFT |
Shift position of RAIL_EVENT_TXACK_ABORTED bit. |
| RAIL_EVENT_TX_BLOCKED_SHIFT |
Shift position of RAIL_EVENT_TX_BLOCKED bit. |
| RAIL_EVENT_TXACK_BLOCKED_SHIFT |
Shift position of RAIL_EVENT_TXACK_BLOCKED bit. |
| RAIL_EVENT_TX_UNDERFLOW_SHIFT |
Shift position of RAIL_EVENT_TX_UNDERFLOW bit. |
| RAIL_EVENT_TXACK_UNDERFLOW_SHIFT |
Shift position of RAIL_EVENT_TXACK_UNDERFLOW bit. |
| RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT |
Shift position of RAIL_EVENT_TX_CHANNEL_CLEAR bit. |
| RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT |
Shift position of RAIL_EVENT_TX_CHANNEL_BUSY bit. |
| RAIL_EVENT_TX_CCA_RETRY_SHIFT |
Shift position of RAIL_EVENT_TX_CCA_RETRY bit. |
| RAIL_EVENT_TX_START_CCA_SHIFT |
Shift position of RAIL_EVENT_TX_START_CCA bit. |
| RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT |
Shift position of RAIL_EVENT_CONFIG_UNSCHEDULED bit. |
| RAIL_EVENT_CONFIG_SCHEDULED_SHIFT |
Shift position of RAIL_EVENT_CONFIG_SCHEDULED bit. |
| RAIL_EVENT_SCHEDULER_STATUS_SHIFT |
Shift position of RAIL_EVENT_SCHEDULER_STATUS bit. |
| RAIL_EVENT_CAL_NEEDED_SHIFT |
Shift position of RAIL_EVENT_CAL_NEEDED bit. |
Definition at line
495
of file
rail_types.h
.
Function Documentation
| RAIL_Status_t RAIL_ConfigEvents | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_Events_t |
mask,
|
||
| RAIL_Events_t |
events
|
||
| ) |
Configures radio events.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] maskA bitmask of events to configure. [in] eventsA bitmask of events to trigger RAIL_Config_t::eventsCallback For a full list of available callbacks, see RAIL_EVENT_* set of defines.
- Returns
- Status code indicating success of the function call.
Sets up which radio interrupts generate a RAIL event. The full list of options is in RAIL_Events_t .