RAIL_MultiTimer_t Struct Reference
RAIL timer state structure.
#include <
rail_types.h
>
Data Fields |
|
| RAIL_Time_t | absOffset |
|
Absolute time before the next event.
|
|
| RAIL_Time_t | relPeriodic |
|
Relative, periodic time between events; 0 = timer is oneshot.
|
|
| RAIL_MultiTimerCallback_t | callback |
|
A user callback.
|
|
| void * | cbArg |
|
A user callback argument.
|
|
| struct RAIL_MultiTimer * | next |
|
A pointer to the next soft timer structure.
|
|
| uint8_t | priority |
|
A priority of the callback; 0 = highest priority; 255 = lowest.
|
|
| bool | isRunning |
|
Indicates the timer is currently running.
|
|
| bool | doCallback |
|
Indicates the callback needs to run.
|
|
RAIL timer state structure.
This structure is filled out and maintained internally only. The user/application should not alter any elements of this structure.
Definition at line
215
of file
rail_types.h
.
Field Documentation
| RAIL_Time_t RAIL_MultiTimer_t::absOffset |
Absolute time before the next event.
Definition at line
216
of file
rail_types.h
.
| RAIL_MultiTimerCallback_t RAIL_MultiTimer_t::callback |
A user callback.
Definition at line
218
of file
rail_types.h
.
| void* RAIL_MultiTimer_t::cbArg |
A user callback argument.
Definition at line
219
of file
rail_types.h
.
| bool RAIL_MultiTimer_t::doCallback |
Indicates the callback needs to run.
Definition at line
223
of file
rail_types.h
.
| bool RAIL_MultiTimer_t::isRunning |
Indicates the timer is currently running.
Definition at line
222
of file
rail_types.h
.
| struct RAIL_MultiTimer* RAIL_MultiTimer_t::next |
A pointer to the next soft timer structure.
Definition at line
220
of file
rail_types.h
.
| uint8_t RAIL_MultiTimer_t::priority |
A priority of the callback; 0 = highest priority; 255 = lowest.
Definition at line
221
of file
rail_types.h
.
| RAIL_Time_t RAIL_MultiTimer_t::relPeriodic |
Relative, periodic time between events; 0 = timer is oneshot.
Definition at line
217
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h