A configuration structure for the CSMA transmit algorithm.
#include <
rail_types.h
>
Data Fields | |
uint8_t | csmaMinBoExp |
The minimum (starting) exponent for CSMA random backoff (2^exp - 1). | |
uint8_t | csmaMaxBoExp |
The maximum exponent for CSMA random backoff (2^exp - 1). | |
uint8_t | csmaTries |
The number of backoff-then-CCA iterations that can fail before reporting RAIL_EVENT_TX_CHANNEL_BUSY. | |
int8_t | ccaThreshold |
The CCA RSSI threshold, in dBm, above which the channel is considered 'busy'. | |
uint16_t | ccaBackoff |
The backoff unit period in RAIL's microsecond time base. | |
uint16_t | ccaDuration |
The minimum desired CCA check duration in microseconds. | |
RAIL_Time_t | csmaTimeout |
An overall timeout, in RAIL's microsecond time base, for the operation. |
A configuration structure for the CSMA transmit algorithm.
One of RAIL's schemes for polite spectrum access is an implementation of a Carrier-Sense Multiple Access (CSMA) algorithm based on IEEE 802.15.4 (unslotted).
In pseudo-code it works like this, showing relevant event notifications:
Definition at line 1932
of file rail_types.h
.
Field Documentation
uint16_t RAIL_CsmaConfig_t::ccaBackoff |
The backoff unit period in RAIL's microsecond time base.
It is multiplied by the random backoff exponential controlled by csmaMinBoExp and csmaMaxBoExp to determine the overall backoff period. For random backoffs, any value above 511 microseconds will be truncated. For fixed backoffs it can go up to 65535 microseconds.
Definition at line 1964
of file rail_types.h
.
uint16_t RAIL_CsmaConfig_t::ccaDuration |
The minimum desired CCA check duration in microseconds.
- Note
- Depending on the radio configuration, due to hardware constraints, the actual duration may be longer.
Definition at line 1971
of file rail_types.h
.
uint8_t RAIL_CsmaConfig_t::csmaMaxBoExp |
The maximum exponent for CSMA random backoff (2^exp - 1).
It can range from 0 to RAIL_MAX_CSMA_EXPONENT and must be greater than or equal to csmaMinBoExp.
If both exponents are 0, a non-random fixed backoff of ccaBackoff duration results.
Definition at line 1945
of file rail_types.h
.
uint8_t RAIL_CsmaConfig_t::csmaMinBoExp |
The minimum (starting) exponent for CSMA random backoff (2^exp - 1).
It can range from 0 to RAIL_MAX_CSMA_EXPONENT.
Definition at line 1937
of file rail_types.h
.
RAIL_Time_t RAIL_CsmaConfig_t::csmaTimeout |
An overall timeout, in RAIL's microsecond time base, for the operation.
If the transmission doesn't start before this timeout expires, the transmission will fail with RAIL_EVENT_TX_CHANNEL_BUSY. A value 0 means no timeout is imposed.
Definition at line 1978
of file rail_types.h
.
uint8_t RAIL_CsmaConfig_t::csmaTries |
The number of backoff-then-CCA iterations that can fail before reporting RAIL_EVENT_TX_CHANNEL_BUSY.
It can range from 1 to RAIL_MAX_LBT_TRIES; other values are disallowed.
Definition at line 1951
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h