Detailed information requested and about the packet that was just transmitted.
#include <
rail_types.h
>
Data Fields | |
RAIL_PacketTimeStamp_t | timeSent |
The timestamp of the transmitted packet in the RAIL timebase, filled in by RAIL_GetTxPacketDetails(). | |
bool | isAck |
Indicates whether the transmitted packet was an automatic ACK. |
Detailed information requested and about the packet that was just transmitted.
Definition at line 1792
of file rail_types.h
.
Field Documentation
bool RAIL_TxPacketDetails_t::isAck |
Indicates whether the transmitted packet was an automatic ACK.
In a generic sense, an automatic ACK is defined as a packet sent in response to a received ACK-requesting frame when auto-ACK is enabled. In a protocol specific sense this definition may be more or less restrictive to match the specification and you should refer to that protocol's documentation.
Definition at line 1805
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h