RX Channel Hopping
Hardware accelerated hopping between channels while waiting for a packet in receive.
Data Structures |
|
| struct | RAIL_RxChannelHoppingConfigEntry_t |
|
Structure that represents one of the channels that is part of a sequence of channels used in channel hopping.
|
|
| struct | RAIL_RxChannelHoppingConfig_t |
|
Wrapper struct that will contain the sequence of
RAIL_RxChannelHoppingConfig_t
that represent the channel sequence to use during RX Channel Hopping.
|
|
| struct | RAIL_RxDutyCycleConfig_t |
|
Structure to configure duty cycled receive mode.
|
|
Macros |
|
| #define | RAIL_CHANNEL_HOPPING_INVALID_INDEX (0xFEU) |
|
A sentinel value to flag an invalid channel hopping index.
|
|
| #define | RAIL_CHANNEL_HOPPING_BUFFER_SIZE_PER_CHANNEL (25U) |
|
The static amount of memory needed per channel for channel hopping, regardless of the size of radio configuration structures.
|
|
Enumerations |
|
| enum |
RAIL_RxChannelHoppingMode_t
{
RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL , RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT , RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE , RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE } |
|
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
|
|
| enum | RAIL_RxChannelHoppingDelayMode_t { RAIL_RX_CHANNEL_HOPPING_DELAY_MODE_STATIC } |
|
Modes by which
RAIL_RxChannelHoppingConfigEntry_t::delay
timing can be applied to the time gap between channels.
|
|
Functions |
|
| RAIL_Status_t | RAIL_ConfigRxChannelHopping ( RAIL_Handle_t railHandle, RAIL_RxChannelHoppingConfig_t *config) |
|
Configure RX Channel Hopping.
|
|
| RAIL_Status_t | RAIL_EnableRxChannelHopping ( RAIL_Handle_t railHandle, bool enable, bool reset) |
|
Enable RX Channel Hopping.
|
|
| int16_t | RAIL_GetChannelHoppingRssi ( RAIL_Handle_t railHandle, uint8_t channelIndex) |
|
Get RSSI of one channel in the channel hopping sequence, during channel hopping.
|
|
| RAIL_Status_t | RAIL_ConfigRxDutyCycle ( RAIL_Handle_t railHandle, const RAIL_RxDutyCycleConfig_t *config) |
|
Configure RX duty cycle mode.
|
|
| RAIL_Status_t | RAIL_EnableRxDutyCycle ( RAIL_Handle_t railHandle, bool enable) |
|
Enable RX duty cycle mode.
|
|
Detailed Description
Hardware accelerated hopping between channels while waiting for a packet in receive.
Channel hopping provides a hardware accelerated method for scanning across multiple channels quickly, as part of a receive protocol. While it is possible to call RAIL_StartRx on different channels, back to back, and listen on many channels sequentially in that way, the time it takes to switch channels with that method may be too long for some protocols. This API pre-computes necessary channel change operations for a given list of channels, so that the radio can move from channel to channel much faster. Additionally, it leads to more succinct code as channel changes will be done implicitly, without requiring numerous calls to RAIL_StartRx . Currently, while this feature is enabled, the radio will hop channels in the given sequence each time it enters RX.
The following code gives an example of how to use the RX Channel Hopping API.
Macro Definition Documentation
| #define RAIL_CHANNEL_HOPPING_BUFFER_SIZE_PER_CHANNEL (25U) |
The static amount of memory needed per channel for channel hopping, regardless of the size of radio configuration structures.
Definition at line
698
of file
rail_chip_specific.h
.
Enumeration Type Documentation
Modes by which RAIL_RxChannelHoppingConfigEntry_t::delay timing can be applied to the time gap between channels.
Definition at line
2775
of file
rail_types.h
.
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
Definition at line
2733
of file
rail_types.h
.
Function Documentation
| RAIL_Status_t RAIL_ConfigRxChannelHopping | ( | RAIL_Handle_t |
railHandle,
|
| RAIL_RxChannelHoppingConfig_t * |
config
|
||
| ) |
Configure RX Channel Hopping.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] configConfiguration parameters for RX Channel Hopping.
- Returns
- Status code indicating success of the function call.
Configure Channel Hopping channels, conditions, and parameters. This API must be called before RAIL_EnableChannelHopping. This API must never be called while the radio is on with RX Duty Cycle or Channel Hopping enabled.
- Note
- This feature/API is not supported on the EFR32XG1 family of chips.
- This feature/API is currently not supported in multiprotocol.
- Calling this function will overwrite any settings configured with RAIL_ConfigRxDutyCycle .
| RAIL_Status_t RAIL_ConfigRxDutyCycle | ( | RAIL_Handle_t |
railHandle,
|
| const RAIL_RxDutyCycleConfig_t * |
config
|
||
| ) |
Configure RX duty cycle mode.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] configConfiguration structure to specify duty cycle parameters.
- Returns
- Status code indicating success of the function call.
Configure RX duty cycle mode. With this mode enabled, every time the radio enters RX, it will duty cycle on and off to save power. The duty cycle ratio can be altered dynamically and intelligently by the hardware by staying on longer if a preamble or other packet segments are detected in the air. This API must never be called while the radio is on with RX Duty Cycle or Channel Hopping enabled.
- Note
- This feature/API is not supported on the EFR32XG1 family of chips.
- Calling this function will overwrite any settings configured with RAIL_ConfigRxChannelHopping .
- This feature/API is currently not supported in multiprotocol.
| RAIL_Status_t RAIL_EnableRxChannelHopping | ( | RAIL_Handle_t |
railHandle,
|
| bool |
enable,
|
||
| bool |
reset
|
||
| ) |
Enable RX Channel Hopping.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] enableEnable (true) or disable (false) RX Channel Hopping. [in] resetStart from the first channel of the channel hopping sequence (true) or from wherever hopping left off last time the code left RX.
- Returns
- Status code indicating success of the function call.
Enable or disable Channel Hopping. Additionally, specify whether hopping should be reset to start from the channel at index zero, or continue from the channel last hopped to. The radio should not be on when this API is called. RAIL_ConfigChannelHopping must be called before this API is called.
- Note
- This feature/API is not supported on the EFR32XG1 family of chips.
- This feature/API is currently not supported in multiprotocol.
- RX Channel Hopping may not be enabled while auto-ACKing is enabled.
- Calling this function will overwrite any settings configured with RAIL_EnableRxDutyCycle .
| RAIL_Status_t RAIL_EnableRxDutyCycle | ( | RAIL_Handle_t |
railHandle,
|
| bool |
enable
|
||
| ) |
Enable RX duty cycle mode.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] enableEnable (true) or disable (false) RX Duty Cycling.
- Returns
- Status code indicating success of the function call.
Enable or disable RX duty cycle mode. After this is called, the radio will begin duty cycling each time it enters RX, based on the configuration passed to RAIL_ConfigRxDutyCycle . This API must not be called while the radio is on.
- Note
- This feature/API is not supported on the EFR32XG1 family of chips.
- Calling this function will overwrite any settings configured with RAIL_EnableRxChannelHopping .
- This feature/API is currently not supported in multiprotocol.
| int16_t RAIL_GetChannelHoppingRssi | ( | RAIL_Handle_t |
railHandle,
|
| uint8_t |
channelIndex
|
||
| ) |
Get RSSI of one channel in the channel hopping sequence, during channel hopping.
- Parameters
-
[in] railHandleA RAIL instance handle. [in] channelIndexIndex in the channel hopping sequence of the channel of interest
- Returns
- Latest RSSI for the channel at the specified index.
- Note
- This feature/API is not supported on the EFR32XG1 family of chips.
- This feature/API is currently not supported in multiprotocol.
- RAIL_ConfigRxChannelHopping must be called successfully before this API is called.