Public Attributes#

uint8_t

Address type of the advertising device.

uint8_t

Address of the advertising device.

uint8_t

Raw advertisement data length.

uint8_t

advertisement data

int8_t

Signal strength.

uint8_t

Report type 0x00 Connectable and scannable undirected advertising (ADV_IND) 0x01 Connectable directed advertising (ADV_DIRECT_IND) 0x02 Scannable undirected advertising (ADV_SCAN_IND) 0x03 Non connectable undirected advertising (ADV_NONCONN_IND) 0x04 Scan Response (SCAN_RSP) All other values Reserved for future use.

Public Attribute Documentation#

dev_addr_type#

uint8_t rsi_ble_event_adv_report_s::dev_addr_type

Address type of the advertising device.


dev_addr#

uint8_t rsi_ble_event_adv_report_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the advertising device.


adv_data_len#

uint8_t rsi_ble_event_adv_report_s::adv_data_len

Raw advertisement data length.


adv_data#

uint8_t rsi_ble_event_adv_report_s::adv_data[RSI_MAX_ADV_REPORT_SIZE]

advertisement data


rssi#

int8_t rsi_ble_event_adv_report_s::rssi

Signal strength.


report_type#

uint8_t rsi_ble_event_adv_report_s::report_type

Report type 0x00 Connectable and scannable undirected advertising (ADV_IND) 0x01 Connectable directed advertising (ADV_DIRECT_IND) 0x02 Scannable undirected advertising (ADV_SCAN_IND) 0x03 Non connectable undirected advertising (ADV_NONCONN_IND) 0x04 Scan Response (SCAN_RSP) All other values Reserved for future use.