Public Attributes#
Device address type of the Connected Remote Device.
Device address of the remote device.
Local Device resolvable address.
Remote Device resolvable address.
The role of the device - master/ slave.
Connection interval used on this connection.
Slave latency for the connection in number of connection events.
Connection supervision timeout.
Only applicable for slave ,for master this value is set to 0x00.
Status of the Connection - success/failure.
Public Attribute Documentation#
dev_addr_type#
uint8_t rsi_ble_event_enhnace_conn_status_s::dev_addr_type
Device address type of the Connected Remote Device.
94
of file components/si91x/ble/inc/rsi_ble_apis.h
dev_addr#
uint8_t rsi_ble_event_enhnace_conn_status_s::dev_addr[RSI_DEV_ADDR_LEN]
Device address of the remote device.
96
of file components/si91x/ble/inc/rsi_ble_apis.h
local_resolvlable_addr#
uint8_t rsi_ble_event_enhnace_conn_status_s::local_resolvlable_addr[RSI_DEV_ADDR_LEN]
Local Device resolvable address.
98
of file components/si91x/ble/inc/rsi_ble_apis.h
peer_resolvlable_addr#
uint8_t rsi_ble_event_enhnace_conn_status_s::peer_resolvlable_addr[RSI_DEV_ADDR_LEN]
Remote Device resolvable address.
100
of file components/si91x/ble/inc/rsi_ble_apis.h
role#
uint8_t rsi_ble_event_enhnace_conn_status_s::role
The role of the device - master/ slave.
102
of file components/si91x/ble/inc/rsi_ble_apis.h
conn_interval#
uint16_t rsi_ble_event_enhnace_conn_status_s::conn_interval
Connection interval used on this connection.
Range: 0x0006 to 0x0C80
104
of file components/si91x/ble/inc/rsi_ble_apis.h
conn_latency#
uint16_t rsi_ble_event_enhnace_conn_status_s::conn_latency
Slave latency for the connection in number of connection events.
Range: 0x0000 to 0x01F3
106
of file components/si91x/ble/inc/rsi_ble_apis.h
supervision_timeout#
uint16_t rsi_ble_event_enhnace_conn_status_s::supervision_timeout
Connection supervision timeout.
Range: 0x000A to 0x0C80
108
of file components/si91x/ble/inc/rsi_ble_apis.h
master_clock_accuracy#
uint8_t rsi_ble_event_enhnace_conn_status_s::master_clock_accuracy
Only applicable for slave ,for master this value is set to 0x00.
110
of file components/si91x/ble/inc/rsi_ble_apis.h
status#
uint8_t rsi_ble_event_enhnace_conn_status_s::status
Status of the Connection - success/failure.
112
of file components/si91x/ble/inc/rsi_ble_apis.h