Public Attributes#
uint8_t
Device address of the remote device.
uint16_t
Minimum connection interval.
uint16_t
Maximum connection interval.
uint16_t
Connection Latency.
uint16_t
Supervision Timeout.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_event_remote_conn_param_req_s::dev_addr[6]
Device address of the remote device.
Definition at line
311
of file components/si91x/ble/inc/rsi_ble_apis.h
conn_interval_min#
uint16_t rsi_ble_event_remote_conn_param_req_s::conn_interval_min
Minimum connection interval.
Definition at line
313
of file components/si91x/ble/inc/rsi_ble_apis.h
conn_interval_max#
uint16_t rsi_ble_event_remote_conn_param_req_s::conn_interval_max
Maximum connection interval.
Definition at line
315
of file components/si91x/ble/inc/rsi_ble_apis.h
conn_latency#
uint16_t rsi_ble_event_remote_conn_param_req_s::conn_latency
Connection Latency.
Definition at line
317
of file components/si91x/ble/inc/rsi_ble_apis.h
timeout#
uint16_t rsi_ble_event_remote_conn_param_req_s::timeout
Supervision Timeout.
Definition at line
319
of file components/si91x/ble/inc/rsi_ble_apis.h