Public Attributes#
Remote device Address.
Status of the Encryption ENCRYPT_ENABLED BIT(0) --> To indicate or set encryption is enabled AUTH_LTK_OR_STK_ENC BIT(1) --> To indicate or set Authenticated Pairing and Encryption UN_AUTH_LTK_OR_STK_ENC BIT(2) --> To indicate or set UnAuthenticated pairing and Encryption AUTH_LTK_WITH_LE_SC_ENC BIT(3) --> To indicate or set Authenticated Pairing and Enc with LE SC.
BLE Secure Connections Enable/disable indication 0 --> Disable 1 --> Enable.
Local device EDIV.
Local RAND.
Local Long term Key.
Remote Device Address type.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_bt_event_encryption_enabled_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device Address.
171
of file components/si91x/ble/inc/rsi_ble_apis.h
enabled#
uint8_t rsi_bt_event_encryption_enabled_s::enabled
Status of the Encryption ENCRYPT_ENABLED BIT(0) --> To indicate or set encryption is enabled AUTH_LTK_OR_STK_ENC BIT(1) --> To indicate or set Authenticated Pairing and Encryption UN_AUTH_LTK_OR_STK_ENC BIT(2) --> To indicate or set UnAuthenticated pairing and Encryption AUTH_LTK_WITH_LE_SC_ENC BIT(3) --> To indicate or set Authenticated Pairing and Enc with LE SC.
177
of file components/si91x/ble/inc/rsi_ble_apis.h
sc_enable#
uint8_t rsi_bt_event_encryption_enabled_s::sc_enable
BLE Secure Connections Enable/disable indication 0 --> Disable 1 --> Enable.
181
of file components/si91x/ble/inc/rsi_ble_apis.h
localediv#
uint16_t rsi_bt_event_encryption_enabled_s::localediv
Local device EDIV.
183
of file components/si91x/ble/inc/rsi_ble_apis.h
localrand#
uint8_t rsi_bt_event_encryption_enabled_s::localrand[8]
Local RAND.
185
of file components/si91x/ble/inc/rsi_ble_apis.h
localltk#
uint8_t rsi_bt_event_encryption_enabled_s::localltk[16]
Local Long term Key.
187
of file components/si91x/ble/inc/rsi_ble_apis.h
dev_addr_type#
uint8_t rsi_bt_event_encryption_enabled_s::dev_addr_type
Remote Device Address type.
189
of file components/si91x/ble/inc/rsi_ble_apis.h