Public Attributes#
address of remote device
Device input output capability 0x00 - Display Only 0x01 - Display Yes/No 0x02 - Keyboard Only 0x03 - No Input No Output 0x04 - Keyboard Display.
Out Of the Band data.
Authentication Request contains bonding type MITM Request - BIT(2) Secure Connections - BIT(3) Keypress - BIT(4) CT2 - BIT(5)
Minimum required key size.
Initiator generates/requires the no .of keys after successful paring BIT(0) - EncKey: Initiator distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Initiator distributes the IRK followed by its address BIT(2) - Sign : Initiator distributes the CSRK BIT(3) - BIT(7): Reserved for future use.
Responder generates/requires the no .of keys after successful paring BIT(0) - EncKey: Responder distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Responder distributes the IRK followed by its address BIT(2) - Sign : Responder distributes the CSRK BIT(3) - BIT(7): Reserved for future use.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_bt_event_smp_resp_s::dev_addr[6]
address of remote device
204
of file components/si91x/ble/inc/rsi_ble_apis.h
io_cap#
uint8_t rsi_bt_event_smp_resp_s::io_cap
Device input output capability 0x00 - Display Only 0x01 - Display Yes/No 0x02 - Keyboard Only 0x03 - No Input No Output 0x04 - Keyboard Display.
211
of file components/si91x/ble/inc/rsi_ble_apis.h
oob_data#
uint8_t rsi_bt_event_smp_resp_s::oob_data
Out Of the Band data.
213
of file components/si91x/ble/inc/rsi_ble_apis.h
auth_req#
uint8_t rsi_bt_event_smp_resp_s::auth_req
Authentication Request contains bonding type MITM Request - BIT(2) Secure Connections - BIT(3) Keypress - BIT(4) CT2 - BIT(5)
219
of file components/si91x/ble/inc/rsi_ble_apis.h
min_req_key_size#
uint8_t rsi_bt_event_smp_resp_s::min_req_key_size
Minimum required key size.
221
of file components/si91x/ble/inc/rsi_ble_apis.h
ini_key_distrb#
uint8_t rsi_bt_event_smp_resp_s::ini_key_distrb
Initiator generates/requires the no .of keys after successful paring BIT(0) - EncKey: Initiator distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Initiator distributes the IRK followed by its address BIT(2) - Sign : Initiator distributes the CSRK BIT(3) - BIT(7): Reserved for future use.
227
of file components/si91x/ble/inc/rsi_ble_apis.h
resp_key_distrb#
uint8_t rsi_bt_event_smp_resp_s::resp_key_distrb
Responder generates/requires the no .of keys after successful paring BIT(0) - EncKey: Responder distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Responder distributes the IRK followed by its address BIT(2) - Sign : Responder distributes the CSRK BIT(3) - BIT(7): Reserved for future use.
233
of file components/si91x/ble/inc/rsi_ble_apis.h