Structure to hold various interrupt flags of config-timer.

Public Attributes#

boolean_t

true to enable counter-0 interrupt on event occurrence, false to disable it

boolean_t

true to enable counter-0 interrupt on FIFO full, false to disable it

boolean_t

true to enable counter-0 interrupt on zero count value, false to disable it

boolean_t

true to enable counter-0 interrupt on match-value, false to disable it

boolean_t

true to enable counter-1 interrupt on event occurrence, false to disable it

boolean_t

true to enable counter-1 interrupt on FIFO full, false to disable it

boolean_t

true to enable counter-1 interrupt on zero count value, false to disable it

boolean_t

true to enable counter-1 interrupt on match-value, false to disable it

Public Attribute Documentation#

is_counter0_event_interrupt_enabled#

boolean_t sl_config_timer_interrupt_flags_t::is_counter0_event_interrupt_enabled

true to enable counter-0 interrupt on event occurrence, false to disable it


Definition at line 268 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter0_fifo_full_interrupt_enabled#

boolean_t sl_config_timer_interrupt_flags_t::is_counter0_fifo_full_interrupt_enabled

true to enable counter-0 interrupt on FIFO full, false to disable it


Definition at line 270 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter0_hit_zero_interrupt_enabled#

boolean_t sl_config_timer_interrupt_flags_t::is_counter0_hit_zero_interrupt_enabled

true to enable counter-0 interrupt on zero count value, false to disable it


Definition at line 272 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter0_hit_peak_interrupt_enabled#

boolean_t sl_config_timer_interrupt_flags_t::is_counter0_hit_peak_interrupt_enabled

true to enable counter-0 interrupt on match-value, false to disable it


Definition at line 274 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_event_interrupt_enabled#

boolean_t sl_config_timer_interrupt_flags_t::is_counter1_event_interrupt_enabled

true to enable counter-1 interrupt on event occurrence, false to disable it


Definition at line 276 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_fifo_full_interrupt_enabled#

boolean_t sl_config_timer_interrupt_flags_t::is_counter1_fifo_full_interrupt_enabled

true to enable counter-1 interrupt on FIFO full, false to disable it


Definition at line 278 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_hit_zero_interrupt_enabled#

boolean_t sl_config_timer_interrupt_flags_t::is_counter1_hit_zero_interrupt_enabled

true to enable counter-1 interrupt on zero count value, false to disable it


Definition at line 280 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_hit_peak_interrupt_enabled#

boolean_t sl_config_timer_interrupt_flags_t::is_counter1_hit_peak_interrupt_enabled

true to enable counter-1 interrupt on match-value, false to disable it


Definition at line 282 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h