Pulse Width Modulation#
Introduction#
The Motor Control Pulse Width Modulation (MCPWM) controller is used to generate a periodic pulse waveform, which is useful in motor control and power control applications. The MCPWM controller acts as a timer to count up to a period count value. The time period and the duty cycle of the pulses are both programmable.
Features of Pulse Width Modulation:
Supports up to eight PWM outputs with four duty cycle generators
Complementary and Independent output modes are supported
Dead time insertion in Complementary mode
Manual override option for PWM output pins. Output pin polarity is programmable
Supports generation of interrupt for different events
Supports two hardware fault input pins
Special event trigger for synchronizing analog-to-digital conversions
Configuration#
The configurable parameters of Pulse Width Modulation are frequency, mode, timer counter, duty cycle, output polarity, duty cycle. And the apis used to call them are:
For more information on configuring available parameters refer to the respective peripheral example readme document.
Usage#
The driver PWM exhibits the production of a 50% duty cycle, continuous ON/OFF digital signal at a frequency of 25 kHz. Since this component may be instantiated, several named instances can be made of it.An initialization struct set in accordance with the configuration is constructed for every instance. An instance of channel_0 is generated by default. and the APIs utilized to set up and initialize PWM are
Modules#
Enumerations#
Enum to control dead time.
Enum to control duty cycle.
Enum to control output fault.
Enumeration for PWM channels(1-4)
Enumeration for PWM timer.
Enumeration for PWM polarity low.
Enumeration for PWM polarity high.
Enumeration for PWM base timer modes.
Enumeration for PWM output complementary pairs.
Enumeration for PWM special event trigger time base.
Enumeration for PWM Time base output post scale bits.
Enumeration for PWM input clock pre scale select value.
Enumeration for fault input override value.
Enumeration for output override control.
Enumeration for override value.
PWM enable external triggering.
Typedefs#
PWM structure.
PWM Special Event trigger configuration parameters structure.
PWM DeadTime configuration parameters structure.
PWM Callback structure.
Variables#
Release version number.
major version number
minor version number
PWM channel selection(ch0 to ch4)
PWM frequency.
PWM output polarity for low side.
PWM output polarity for high side.
PWM mode(independent/complementary)
PWM base time counter initial value.
PWM duty cycle.
PWM base timer mode.
PWM channel timer selection.
PWM GPIO output low side port.
PWM GPIO output low side pin.
PWM GPIO output high side port.
PWM GPIO output high side pin.
PWM GPIO output low side mux.
PWM GPIO output high side mux.
PWM GPIO output low side pad.
PWM GPIO output high side pad.
PWM GPIO port.
PWM GPIO pin.
PWM GPIO mux.
PWM GPIO pad.
Functions#
This API is used to de-initialize the PWM peripheral.
This API is used to get the API version of PWM.
This API sets the PWM configuration parameters.
This API is used to set output polarity for Motor Control Pulse Width Modulation (MCPWM).
This API is used to start the Motor Control Pulse Width Modulation (MCPWM).
This API is used to stop the Motor Control Pulse Width Modulation (MCPWM) operation for the required channel.
This API is used to select number of base timers as four base timers for four channels or one base timer for all channels of Motor Control Pulse Width Modulation (MCPWM).
This API is used to set time period and counter initial value for the required Motor Control Pulse Width Modulation (MCPWM) channel.
This API is used to configure special event trigger generation for required Motor Control Pulse Width Modulation (MCPWM) channel which allows the A/D converter to be synchronized to the PWM time base.
This API is used to configure Dead time insertion parameters for Motor Control Pulse Width Modulation (MCPWM).
This API is used to reset the required channel of Motor Control Pulse Width Modulation (MCPWM).
This API is used to reset the counter from the required channel of Motor Control Pulse Width Modulation (MCPWM)
This API is used to set base time period control for the required Motor Control Pulse Width Modulation (MCPWM) channel.
This API is used to control fault A/B pin output value to be overridden when fault condition occurs.
This API is used to set the mode of base timer for required channel.
This API is used to set output mode for the Motor Control Pulse Width Modulation (MCPWM).
Handles all interrupt flags of Motor Control Pulse Width Modulation (MCPWM).
Unregisters the PWM event.
This API is used to read the counter current value for required Motor Control Pulse Width Modulation (MCPWM) channel.
This API is used to get time period counter direction status of required Motor Control Pulse Width Modulation (MCPWM) channel whether counter up / down.
Controls dead time insertion at rise edge (or) fall edge of any four channels.
This API is used to clear the interrupts of Motor Control Pulse Width Modulation (MCPWM)
This API is used to get the interrupt status of interrupt flags of Motor Control Pulse Width Modulation (MCPWM).
This API is used to control duty cycle control parameters for the required Motor Control Pulse Width Modulation (MCPWM) channel.
This API is used to control the output override operation of Motor Control Pulse Width Modulation (MCPWM).
This API is used to control the override control parameter and output is in sync with PWM time period depending on operating mode.
This API is used to control override value for the required output of Motor Control Pulse Width Modulation (MCPWM)
This API is used to control output fault in pwm module.
This API is used to control the special event trigger.
This API is used to control the dead time.
This API is used to select duty cycle for the required Motor Control Pulse Width Modulation (MCPWM) channel.
This API is used to get duty cycle for the required Motor Control Pulse Width Modulation (MCPWM) channel.
This API is used to enables an external trigger.
Get time period for the required channel.
This API is used to initialize PWM pins and clock.
This API is used to initialize PWM event pins.
This API is used to disable the reset for the required channel of MCPWM.
This API is used to disable the counter reset for the required channel of MCPWM.
Enumeration Documentation#
sl_pwm_fault_t#
sl_pwm_fault_t
Enum to control fault a and fault b.
| Enumerator | |
|---|---|
| SL_FAULTA | PWM fault A. |
| SL_FAULTB | PWM fault B. |
| SL_FAULT_LAST | Last member of enum for validation. |
sl_pwm_dead_time_t#
sl_pwm_dead_time_t
Enum to control dead time.
| Enumerator | |
|---|---|
| SL_DEAD_TIME_DISABLE | PWM dead time disable. |
| SL_DEAD_TIME_ENABLE | PWM dead time enable. |
| SL_DEAD_TIME_LAST | Last member of enum for validation. |
sl_pwm_duty_cycle_t#
sl_pwm_duty_cycle_t
Enum to control duty cycle.
| Enumerator | |
|---|---|
| SL_DUTY_CYCLE_DISABLE | PWM duty cycle disable. |
| SL_DUTY_CYCLE_ENABLE | PWM duty cycle enable. |
| SL_DUTY_CYCLE_LAST | Last member of enum for validation. |
sl_pwm_override_t#
sl_pwm_override_t
Enum to control override.
| Enumerator | |
|---|---|
| SL_OVERRIDE_RESET | PWM override reset. |
| SL_OVERRIDE_SET | PWM override set. |
| SL_OVERRIDE_LAST | Last member of enum for validation. |
sl_pwm_output_fault_t#
sl_pwm_output_fault_t
Enum to control output fault.
| Enumerator | |
|---|---|
| SL_OUTPUT_FAULT_RESET | PWM output fault reset. |
| SL_OUTPUT_FAULT_SET | PWM output fault set. |
| SL_OUTPUT_FAULT_LAST | Last member of enum for validation. |
sl_pwm_event_t#
sl_pwm_event_t
Enum to control events.
| Enumerator | |
|---|---|
| SL_EVENT_DISABLE | PWM event disable. |
| SL_EVENT_ENABLE | PWM event enable. |
| SL_EVENT_LAST | Last member of enum for validation. |
sl_pwm_channel_t#
sl_pwm_channel_t
Enumeration for PWM channels(1-4)
| Enumerator | |
|---|---|
| SL_CHANNEL_1 | PWM channel 1. |
| SL_CHANNEL_2 | PWM channel 2. |
| SL_CHANNEL_3 | PWM channel 3. |
| SL_CHANNEL_4 | PWM channel 4. |
| SL_CHANNEL_LAST | Last member of enum for validation. |
sl_pwm_timer_t#
sl_pwm_timer_t
Enumeration for PWM timer.
| Enumerator | |
|---|---|
| SL_BASE_TIMER_EACH_CHANNEL | PWM timer for each channel. |
| SL_BASE_TIMER_ALL_CHANNEL | PWM timer for all channels. |
| SL_BASE_TIMER_LAST | Last member of enum for validation. |
sl_pwm_polarity_low_t#
sl_pwm_polarity_low_t
Enumeration for PWM polarity low.
| Enumerator | |
|---|---|
| SL_POLARITYL_LOW | PWM output polarity for low side(L0-L3)-low. |
| SL_POLARITYL_HIGH | PWM output polarity for low side(H0-H3)-high. |
| SL_POLARITYL_LAST | Last member of enum for validation. |
sl_pwm_polarity_high_t#
sl_pwm_polarity_high_t
Enumeration for PWM polarity high.
| Enumerator | |
|---|---|
| SL_POLARITYH_LOW | PWM output polarity for high side(L0-L3)-low. |
| SL_POLARITYH_HIGH | PWM output polarity for high side(H0-H3)-high. |
| SL_POLARITYH_LAST | Last member of enum for validation. |
sl_pwm_mode_t#
sl_pwm_mode_t
Enumeration for PWM mode.
| Enumerator | |
|---|---|
| SL_MODE_INDEPENDENT | PWM independent mode. |
| SL_MODE_COMPLEMENTARY | PWM complementary mode. |
| SL_MODE_LAST | Last member of enum for validation. |
sl_pwm_base_timer_mode_t#
sl_pwm_base_timer_mode_t
Enumeration for PWM base timer modes.
| Enumerator | |
|---|---|
| SL_FREE_RUN_MODE | PWM free run mode. |
| SL_SINGLE_EVENT_MODE | PWM single event mode. |
| SL_DOWN_COUNT_MODE | PWM down count mode. |
| SL_UP_DOWN_MODE | PWM up/down mode. |
| SL_UP_DOWN_DOUBLE_UPDATE | PWM up/down double update mode. |
| SL_BASE_TIMER_MODE_LAST | Last member of enum for validation. |
sl_pwm_output_t#
sl_pwm_output_t
Enumeration for PWM output complementary pairs.
| Enumerator | |
|---|---|
| SL_OUTPUT_LOW0 | PWM output L0. |
| SL_OUTPUT_LOW1 | PWM output L1. |
| SL_OUTPUT_LOW2 | PWM output L2. |
| SL_OUTPUT_LOW3 | PWM output L3. |
| SL_OUTPUT_HIGH0 | PWM output H0. |
| SL_OUTPUT_HIGH1 | PWM output H1. |
| SL_OUTPUT_HIGH2 | PWM output H2. |
| SL_OUTPUT_HIGH3 | PWM output H3. |
| SL_OUTPUT_LAST | Last member of enum for validation. |
sl_pwm_svt_t#
sl_pwm_svt_t
Enumeration for PWM special event trigger time base.
| Enumerator | |
|---|---|
| SL_SVT_COUNT_UP | Special event trigger occurs when time base is counting up. |
| SL_SVT_COUNT_DOWN | Special event trigger occurs when time base is counting down. |
| SL_SVT_COUNT_LAST | Last member of enum for validation. |
sl_pwm_post_t#
sl_pwm_post_t
Enumeration for PWM Time base output post scale bits.
| Enumerator | |
|---|---|
| SL_TIME_PERIOD_POSTSCALE_1_1 | 1:1 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_2 | 1:2 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_3 | 1:3 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_4 | 1:4 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_5 | 1:5 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_6 | 1:6 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_7 | 1:7 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_8 | 1:8 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_9 | 1:9 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_10 | 1:10 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_11 | 1:11 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_12 | 1:12 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_13 | 1:13 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_14 | 1:14 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_15 | 1:15 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_16 | 1:16 post scale |
| SL_TIME_PERIOD_POSTSCALE_1_LAST | Last member of enum for validation. |
sl_pwm_pre_t#
sl_pwm_pre_t
Enumeration for PWM input clock pre scale select value.
| Enumerator | |
|---|---|
| SL_TIME_PERIOD_PRESCALE_1 | 1x input clock period |
| SL_TIME_PERIOD_PRESCALE_2 | 2x input clock period |
| SL_TIME_PERIOD_PRESCALE_4 | 4x input clock period |
| SL_TIME_PERIOD_PRESCALE_8 | 8x input clock period |
| SL_TIME_PERIOD_PRESCALE_16 | 16x input clock period |
| SL_TIME_PERIOD_PRESCALE_32 | 32x input clock period |
| SL_TIME_PERIOD_PRESCALE_64 | 64x input clock period |
| SL_TIME_PERIOD_PRESCALE_LAST | Last member of enum for validation. |
sl_pwm_fault_input_t#
sl_pwm_fault_input_t
Enumeration for fault input override value.
| Enumerator | |
|---|---|
| SL_VALUE_INACTIVE | PWM output pin is driven inactive on an external fault input A/B event. |
| SL_VALUE_ACTIVE | PWM output pin is driven active on an external fault input A/B event. |
| SL_VALUE_LAST | Last member of enum for validation. |
sl_pwm_output_override_t#
sl_pwm_output_override_t
Enumeration for output override control.
| Enumerator | |
|---|---|
| SL_OP_OVERRIDE_UNSYNC | no effect. |
| SL_OP_OVERRIDE_SYNC | Output override is in sync with pwm time period depending on operating mode. |
| SL_OP_OVERRIDE_LAST | Last member of enum for validation. |
sl_pwm_override_value_t#
sl_pwm_override_value_t
Enumeration for override value.
| Enumerator | |
|---|---|
| SL_OVERRIDE_VALUE0 | Override value 0. |
| SL_OVERRIDE_VALUE1 | Override value 1. |
| SL_OVERRIDE_VALUE_LAST | Last member of enum for validation. |
sl_pwm_trigger_t#
sl_pwm_trigger_t
PWM enable external triggering.
| Enumerator | |
|---|---|
| SL_TRIGGER_DISABLE | Disabling external triggering. |
| SL_TRIGGER_ENABLE | Enabling external triggering. |
| SL_TRIGGER_LAST | Last member of enum for validation. |
Typedef Documentation#
sl_si91x_pwm_svt_config_t#
typedef RSI_MCPWM_SVT_CONFIG_T sl_si91x_pwm_svt_config_t
PWM Special Event trigger configuration parameters structure.
sl_si91x_pwm_dt_config_t#
typedef RSI_MCPWM_DT_CONFIG_T sl_si91x_pwm_dt_config_t
PWM DeadTime configuration parameters structure.
sl_si91x_pwm_callback_t#
typedef RSI_MCPWM_CALLBACK_T sl_si91x_pwm_callback_t
PWM Callback structure.
Variable Documentation#
base_time_counter_initial_value#
uint32_t sl_pwm_config_t::base_time_counter_initial_value
PWM base time counter initial value.
channel_timer_selection#
uint8_t sl_pwm_config_t::channel_timer_selection
PWM channel timer selection.
Function Documentation#
sl_si91x_pwm_deinit#
void sl_si91x_pwm_deinit (void )
This API is used to de-initialize the PWM peripheral.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This will de-initialize the PWM peripheral and also it disables PWM module clock.
Pre-conditions:
Returns
none
sl_si91x_pwm_get_version#
sl_pwm_version_t sl_si91x_pwm_get_version (void )
This API is used to get the API version of PWM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
version which includes Release, SQA and DEV version numbers of PWM Returns
returns structure of type sl_pwm_version_t
sl_si91x_pwm_set_configuration#
sl_status_t sl_si91x_pwm_set_configuration (sl_pwm_config_t * pwm_config)
This API sets the PWM configuration parameters.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_config_t * | [in] | pwm_config | pointer to configuration parameters of type sl_pwm_config_t |
It configures the output polarity, set time period, output mode, set duty cycle set base timer mode and base timer selection for each channel.
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_set_output_polarity#
sl_status_t sl_si91x_pwm_set_output_polarity (boolean_t polarity_low, boolean_t polarity_high)
This API is used to set output polarity for Motor Control Pulse Width Modulation (MCPWM).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| boolean_t | [in] | polarity_low | Output polarity for low side (L3, L2, L1, L0) |
| boolean_t | [in] | polarity_high | Output polarity for high side (H3, H2, H1, H0) |
Setting polarity positive sets the digital pulse ON for the duty cycle and off for remainder of the period. Setting polarity negative is vice-versa of positive polarity set.
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_start#
sl_status_t sl_si91x_pwm_start (sl_pwm_channel_t channel)
This API is used to start the Motor Control Pulse Width Modulation (MCPWM).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
Operation for required channel is based on duty cycle set, polarity and all other configurations done for respective channels.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_stop#
sl_status_t sl_si91x_pwm_stop (sl_pwm_channel_t channel)
This API is used to stop the Motor Control Pulse Width Modulation (MCPWM) operation for the required channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_control_base_timer#
sl_status_t sl_si91x_pwm_control_base_timer (sl_pwm_timer_t base_timer)
This API is used to select number of base timers as four base timers for four channels or one base timer for all channels of Motor Control Pulse Width Modulation (MCPWM).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_timer_t | [in] | base_timer | PWM base timer of type sl_pwm_timer_t |
One base timer is used when single timer to be selected for all channels. Instead of only one base timer, there is also one base timer for each channel selection, where separate base timers are used for separate channels.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_set_time_period#
sl_status_t sl_si91x_pwm_set_time_period (sl_pwm_channel_t channel, uint32_t period, uint32_t init_val)
This API is used to set time period and counter initial value for the required Motor Control Pulse Width Modulation (MCPWM) channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t. |
| uint32_t | [in] | period | Time period value in the range of 0 - 65535. |
| uint32_t | [in] | init_val | Update the base time counter initial value, in the range of 0 - 65535. |
It updates the base timer period and base timer counter initial values for required channel.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_trigger_special_event#
sl_status_t sl_si91x_pwm_trigger_special_event (sl_pwm_svt_t direction, sl_si91x_pwm_svt_config_t * pwm_config)
This API is used to configure special event trigger generation for required Motor Control Pulse Width Modulation (MCPWM) channel which allows the A/D converter to be synchronized to the PWM time base.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_svt_t | [in] | direction | Special event trigger for time base direction of type sl_pwm_svt_t |
| sl_si91x_pwm_svt_config_t * | [in] | pwm_config | Pointer to the structure of type sl_si91x_pwm_svt_config_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_configure_dead_time#
sl_status_t sl_si91x_pwm_configure_dead_time (sl_si91x_pwm_dt_config_t * dead_time, sl_pwm_channel_t channel)
This API is used to configure Dead time insertion parameters for Motor Control Pulse Width Modulation (MCPWM).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_pwm_dt_config_t * | [in] | dead_time | Pointer to the structure of type sl_si91x_pwm_dt_config_t |
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
Dead time is a small amount of time inserted between the switching edges of PWM signals.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_reset_channel#
sl_status_t sl_si91x_pwm_reset_channel (sl_pwm_channel_t channel)
This API is used to reset the required channel of Motor Control Pulse Width Modulation (MCPWM).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_reset_counter#
sl_status_t sl_si91x_pwm_reset_counter (sl_pwm_channel_t channel)
This API is used to reset the counter from the required channel of Motor Control Pulse Width Modulation (MCPWM)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_control_period#
sl_status_t sl_si91x_pwm_control_period (sl_pwm_post_t post_scale, sl_pwm_pre_t pre_scale, sl_pwm_channel_t channel)
This API is used to set base time period control for the required Motor Control Pulse Width Modulation (MCPWM) channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_post_t | [in] | post_scale | Time base output post scale bits of type sl_pwm_post_t |
| sl_pwm_pre_t | [in] | pre_scale | Base timer input clock pre scale select value of type sl_pwm_pre_t |
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
This sets the base timer output post scalar bits and base timer input clock prescalar value.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_control_fault#
sl_status_t sl_si91x_pwm_control_fault (sl_pwm_fault_t fault, sl_pwm_output_t pwm_output, sl_pwm_override_value_t value)
This API is used to control fault A/B pin output value to be overridden when fault condition occurs.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_fault_t | [in] | fault | Enum of type sl_pwm_fault_t |
| sl_pwm_output_t | [in] | pwm_output | Enum of type sl_pwm_output_t |
| sl_pwm_override_value_t | [in] | value | Fault input A/B PWM output override value of type sl_pwm_override_value_t |
When it is asserted, these pins can optionally drive each of the PWM I/O pins to a defined state.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_set_base_timer_mode#
sl_status_t sl_si91x_pwm_set_base_timer_mode (sl_pwm_base_timer_mode_t mode, sl_pwm_channel_t channel)
This API is used to set the mode of base timer for required channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_base_timer_mode_t | [in] | mode | Base timer operating mode of type sl_pwm_base_timer_mode_t |
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
There are different modes set like free running mode, single event mode etc.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_set_output_mode#
sl_status_t sl_si91x_pwm_set_output_mode (sl_pwm_mode_t mode, sl_pwm_channel_t channel)
This API is used to set output mode for the Motor Control Pulse Width Modulation (MCPWM).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_mode_t | [in] | mode | PWM Output mode of type sl_pwm_mode_t |
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
There are two modes we can configure i.e., independent mode (or) complementary mode.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_register_callback#
sl_status_t sl_si91x_pwm_register_callback (sl_si91x_pwm_callback_t * callback_event, uint16_t flag)
Handles all interrupt flags of Motor Control Pulse Width Modulation (MCPWM).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_si91x_pwm_callback_t * | [in] | callback_event | Structure of type sl_si91x_pwm_callback_t |
| uint16_t | [in] | flag | It is the logical OR of different interrupts generated on multiple channels(in the range of 0 - 65535). |
It handles IRQ handler, Timer interrupt and callback event which handles different events.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is a null pointer
sl_si91x_pwm_unregister_callback#
sl_status_t sl_si91x_pwm_unregister_callback (uint16_t flag)
Unregisters the PWM event.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | flag | It is the logical OR of different interrupts generated on multiple channels(in the range of 0 - 65535). |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is a null pointer
sl_si91x_pwm_read_counter#
sl_status_t sl_si91x_pwm_read_counter (uint16_t * counter_value, sl_pwm_channel_t channel)
This API is used to read the counter current value for required Motor Control Pulse Width Modulation (MCPWM) channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t * | [out] | counter_value | Counter value |
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_get_counter_direction#
sl_status_t sl_si91x_pwm_get_counter_direction (uint8_t * counter_direction, sl_pwm_channel_t channel)
This API is used to get time period counter direction status of required Motor Control Pulse Width Modulation (MCPWM) channel whether counter up / down.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | counter_direction | Pointer to the counter direction (up/down) of type uint8_t |
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_control_dead_time#
sl_status_t sl_si91x_pwm_control_dead_time (sl_pwm_dead_time_t dead_time, uint32_t flag)
Controls dead time insertion at rise edge (or) fall edge of any four channels.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_dead_time_t | [in] | dead_time | Enum of type sl_pwm_dead_time_t |
| uint32_t | [in] | flag | ORing of the following values: (In the range of 0 - 65535).
|
Dead time applies only to PWM output pair, which are in complementary mode.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_clear_interrupt#
sl_status_t sl_si91x_pwm_clear_interrupt (uint32_t flag)
This API is used to clear the interrupts of Motor Control Pulse Width Modulation (MCPWM)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | flag | The logical OR of different interrupts generated on multiple channels(in the range of 0-511). |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is a null pointer
sl_si91x_pwm_get_interrupt_status#
sl_status_t sl_si91x_pwm_get_interrupt_status (uint32_t flag, uint16_t * intr_status)
This API is used to get the interrupt status of interrupt flags of Motor Control Pulse Width Modulation (MCPWM).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | flag | Flag value (0 - 65535) |
| uint16_t * | [out] | intr_status | Pointer to interrupt status |
Events which are raised can be identified by checking the status.
Pre-conditions:
Returns
Interrupt status of the required interrupt flag
sl_si91x_pwm_configure_duty_cycle#
sl_status_t sl_si91x_pwm_configure_duty_cycle (sl_pwm_duty_cycle_t duty_cycle, uint32_t value, sl_pwm_channel_t channel)
This API is used to control duty cycle control parameters for the required Motor Control Pulse Width Modulation (MCPWM) channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_duty_cycle_t | [in] | duty_cycle | Enum of type sl_pwm_duty_cycle_t |
| uint32_t | [in] | value | This can be a logical OR of the following parameters:(Range 0 -127).
|
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
This API controls duty cycle parameters for the required Motor Control Pulse Width Modulation (MCPWM) channel. It can also enable (or prevent) duty cycle updating.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_output_override#
sl_status_t sl_si91x_pwm_output_override (sl_pwm_override_t override, sl_pwm_output_t pwm_output)
This API is used to control the output override operation of Motor Control Pulse Width Modulation (MCPWM).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_override_t | [in] | override | Enum of type sl_pwm_override_t |
| sl_pwm_output_t | [in] | pwm_output | PWM output override of type sl_pwm_output_t |
This API controls MCPWM's output override operation. It enables you to enable or disable PWM output override.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_control_override#
sl_status_t sl_si91x_pwm_control_override (sl_pwm_override_t override, sl_pwm_output_override_t value)
This API is used to control the override control parameter and output is in sync with PWM time period depending on operating mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_override_t | [in] | override | Enum of type sl_pwm_override_t |
| sl_pwm_output_override_t | [in] | value | Output override to be in sync with PWM time period sl_pwm_output_override_t |
This API is used for controlling the override control parameters and also the output is synchronized with the PWM time period, depending on the operating mode.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_control_override_value#
sl_status_t sl_si91x_pwm_control_override_value (sl_pwm_override_t override, sl_pwm_output_t pwm_output, sl_pwm_override_value_t value)
This API is used to control override value for the required output of Motor Control Pulse Width Modulation (MCPWM)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_override_t | [in] | override | Enum of type sl_pwm_override_t |
| sl_pwm_output_t | [in] | pwm_output | PWM output override of type sl_pwm_output_t |
| sl_pwm_override_value_t | [in] | value | Override value of type sl_pwm_override_value_t |
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_control_output_fault#
sl_status_t sl_si91x_pwm_control_output_fault (sl_pwm_output_fault_t output_fault, uint32_t value)
This API is used to control output fault in pwm module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_output_fault_t | [in] | output_fault | Enum of type sl_pwm_output_fault_t |
| uint32_t | [in] | value | This can be a logical OR of the below parameters: (in the range of 0 - 65535)
|
This API is used to control output fault in pwm override control parameters for the required PWM output.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_control_special_event_trigger#
sl_status_t sl_si91x_pwm_control_special_event_trigger (sl_pwm_event_t event)
This API is used to control the special event trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_event_t | [in] | event | Enum of type sl_pwm_event_t |
This API controls the generation of a special event trigger for the required channel of the Motor Control Pulse Width Modulation (MCPWM).
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_select_dead_time#
sl_status_t sl_si91x_pwm_select_dead_time (sl_pwm_dead_time_t dead_time, uint32_t value)
This API is used to control the dead time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_dead_time_t | [in] | dead_time | Enum of type sl_pwm_dead_time_t |
| uint32_t | [in] | value | This can be a logical OR of the below parameters: (in the range of 0 - 4095).
|
This API is used to control dead time control parameters for the required channel.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_set_duty_cycle#
sl_status_t sl_si91x_pwm_set_duty_cycle (uint32_t duty_cycle, sl_pwm_channel_t channel)
This API is used to select duty cycle for the required Motor Control Pulse Width Modulation (MCPWM) channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | duty_cycle | Duty cycle value (0 - 65535). |
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_get_duty_cycle#
sl_status_t sl_si91x_pwm_get_duty_cycle (sl_pwm_channel_t channel, uint32_t * duty_cycle)
This API is used to get duty cycle for the required Motor Control Pulse Width Modulation (MCPWM) channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
| uint32_t * | [out] | duty_cycle | Pointer to the duty cycle value |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_enable_external_trigger#
sl_status_t sl_si91x_pwm_enable_external_trigger (sl_pwm_trigger_t enable)
This API is used to enables an external trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_trigger_t | [in] | enable | Controlling external trigger of type sl_pwm_trigger_t |
This API is used to enables the use of an external trigger for base time counter increment or decrement of Motor Control Pulse Width Modulation (MCPWM).
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_get_time_period#
sl_status_t sl_si91x_pwm_get_time_period (sl_pwm_channel_t channel, uint16_t * time_period)
Get time period for the required channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_channel_t | [in] | channel | Channel number (1 to 4) of type sl_pwm_channel_t |
| uint16_t * | [out] | time_period | Pointer to read time period |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_init#
sl_status_t sl_si91x_pwm_init (sl_pwm_init_t * pwm_init)
This API is used to initialize PWM pins and clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_init_t * | [in] | pwm_init | Pointer to the structure of type sl_pwm_init_t |
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_fault_init#
sl_status_t sl_si91x_pwm_fault_init (sl_pwm_fault_init_t * pwm_fault)
This API is used to initialize PWM event pins.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_fault_init_t * | [in] | pwm_fault | Pointer to the structure of type sl_pwm_fault_init_t |
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is null pointer
sl_si91x_pwm_reset_channel_disable#
sl_status_t sl_si91x_pwm_reset_channel_disable (sl_pwm_channel_t channel)
This API is used to disable the reset for the required channel of MCPWM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_channel_t | [in] | channel | Channel number (0 to 3) of type sl_pwm_channel_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success
sl_si91x_pwm_reset_counter_disable#
sl_status_t sl_si91x_pwm_reset_counter_disable (sl_pwm_channel_t channel)
This API is used to disable the counter reset for the required channel of MCPWM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_pwm_channel_t | [in] | channel | Channel number (0 to 3) of type sl_pwm_channel_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER - The parameter is an invalid argument
SL_STATUS_OK - Success