Serial Input-Output#
Introduction#
Serial Input/Output (SIO) refers to a method of data transfer where information is sent and received sequentially, one bit at a time, over a single communication channel. This communication can occur between different electronic devices, such as micro-controllers, sensors, or other components.
Key features of SIO include:
SIO Functionality is supported by Eight GPIO pins.
Detects a 32-bit pattern on the input pins.
SIO will transmit or receive the MSB First.
Configuration#
Various parameters SPI bit order, SPI clock, MOSI channel, MISO channel, SPI CS channel, bit length, SPI mode can be configured. Various parameters UART baud rate, bit length, parity, receive channel selection, transmit channel selection, stop bits can be configured with below given Enumerations.
For more information on configuring available parameters refer to the respective peripheral example readme document.
Usage#
Data is transferred over SIO SPI after it has been initialized and configured. A callback API is then called to register the callback at the moment of the event. Before transfer has begin, chip select assert is to be done. In order to do this test, the MISO and MOSI pins must be connected in loopback mode.
After transfer completion, chip select de-assert is to be done using When the transfer complete event is generated, it compares the sent and received data.
Data is sent and received by SIO UART after it has been initiated and configured. A callback API is then called to register the callback at the moment of the event. Subsequently, the transfer buffer will transmit the required number of bytes, and the receive buffer will obtain the data bytes. It compares the sent and received data when the receive complete event is created.
Modules#
Enumerations#
SIO-UART Events.
SIO-SPI bit width configurations.
SIO-SPI MSB/LSB first configurations.
SIO-UART bit length configurations.
SIO-UART parity configurations.
SIO-UART stop bit configurations.
Typedefs#
SIO-SPI configuration structure.
SIO-SPI Transfer structure.
SIO-I2S configuration structure.
SIO-I2S Transfer structure.
SIO-UART configuration structure.
SIO-I2S callback function pointer.
SIO-SPI callback function pointer.
SIO_UART callback function pointer.
SIO-I2C configuration structure.
Variables#
Release version number.
Major version number.
Minor version number.
SIO SPI CS port.
SIO SPI CS pin.
SIO SPI CS mux.
SIO SPI CS pad.
SIO SPI CLK port.
SIO SPI CLK pin.
SIO SPI CLK mux.
SIO SPI CLK pad.
SIO SPI MOSI port.
SIO SPI MOSI pin.
SIO SPI MOSI mux.
SIO SPI MOSI pad.
SIO SPI MISO port.
SIO SPI MISO pin.
SIO SPI MISO mux.
SIO SPI MISO pad.
SIO UART TX port.
SIO UART TX pin.
SIO UART TX mux.
SIO UART TX pad.
SIO UART RX port.
SIO UART RX pin.
SIO UART RX mux.
SIO UART RX pad.
SIO I2C SDA port.
SIO I2C SDA pin.
SIO I2C SDA mux.
SIO I2C SDA pad.
SIO I2C SCL port.
SIO I2C SCL pin.
SIO I2C SCL mux.
SIO I2C SCL pad.
Functions#
Initialize the SIO module.
Initialize the SIO-SPI module.
This API is used to De-initialize SIO module.
Initialize SIO SPI pins and clock.
Initialize SIO UART pins and clock.
Initialize SIO I2C pins and clock.
Assert the SIO SPI chip select.
De-assert the SIO SPI chip select.
Register the user callback function.
Un-register the user callback function, i.e., clear the callback function address and disables IRQ handler.
Transfer the SIO SPI data.
Get the SIO version.
Initialize SIO-UART, i.e., set baud rate, parity, channel selection, stop bits, and data length.
Send the data over SIO-UART in non-blocking mode.
Send the data over SIO-UART in blocking mode.
Read data from SIO-UART in non-blocking mode.
Read data from UART in blocking mode.
Register the user callback function.
Write data using SIO-I2C.
Read data using SIO-I2C.
Transfer data using SIO-I2C.
Generate I2C start in SIO.
Generate I2C stop in SIO.
Un-register the user callback function.
Used when UART receive is done.
Configure pin detection mode to be considered for GPIO interrupt.
Match the pattern with data to be detected.
Generate the shift clock.
Select SIO peripheral clock.
Shift the number of bits.
Enable/disable the flow control bit.
Load data to buffer in reverse order.
Enable the common swap interrupt.
Disable the common swap interrupt.
Mask the common swap interrupt.
Unmask the common swap interrupt.
Read the common swap interrupt status.
Enable the common shift interrupt.
Disable the common shift interrupt.
Mask the common shift interrupt.
Unmask the common shift interrupt.
Read the common shift interrupt status.
Select edge of the clock cycle for sampling bits.
Read SIO buffer register.
Write into SIO buffer register.
Macros#
SIO-SPI channel 0.
SIO-SPI channel 1.
SIO-SPI channel 2.
SIO-SPI channel 3.
SIO-SPI channel 4.
SIO-SPI channel 5.
SIO-SPI channel 6.
SIO-SPI channel 7.
Enumeration Documentation#
sl_sio_spi_event_t#
sl_sio_spi_event_t
SIO-SPI Events.
| Enumerator | |
|---|---|
| SL_SIO_SPI_TX_DONE | SIO-SPI Transfer done event. |
| SL_SIO_SPI_RX_DONE | SIO-SPI Receive done event. |
sl_sio_uart_event_t#
sl_sio_uart_event_t
SIO-UART Events.
| Enumerator | |
|---|---|
| SL_SIO_UART_TX_DONE | SIO-UART transfer done event. |
| SL_SIO_UART_RX_DONE | SIO-UART receive done event. |
| SL_SIO_UART_PARITY_ERR | SIO-UART parity error. |
| SL_SIO_UART_FRAMING_ERR | SIO-UART framing error. |
| SL_SIO_UART_RECEIVE_CHAR | SIO-UART receive character. |
sl_sio_spi_mode_t#
sl_sio_spi_mode_t
SIO-SPI modes configurations.
| Enumerator | |
|---|---|
| SL_SIO_SPI_MODE_0 | SIO-SPI mode 0. |
| SL_SIO_SPI_MODE_3 | SIO-SPI mode 3. |
sl_sio_spi_bit_width_t#
sl_sio_spi_bit_width_t
SIO-SPI bit width configurations.
| Enumerator | |
|---|---|
| SL_SIO_SPI_BIT_8 | SIO-SPI bit width 8. |
| SL_SIO_SPI_BIT_16 | SIO-SPI bit width 16. |
sl_sio_spi_msb_lsb_t#
sl_sio_spi_msb_lsb_t
SIO-SPI MSB/LSB first configurations.
| Enumerator | |
|---|---|
| SL_SIO_SPI_LSB_FIRST | SIO-SPI LSB first. |
| SL_SIO_SPI_MSB_FIRST | SIO-SPI MSB first. |
sl_sio_spi_bit_length_t#
sl_sio_spi_bit_length_t
SIO-UART bit length configurations.
| Enumerator | |
|---|---|
| SL_SIO_UART_BIT_8 | SIO-SPI bit length 8. |
| SL_SIO_UART_BIT_16 | SIO-SPI bit length 16. |
sl_sio_spi_parity_t#
sl_sio_spi_parity_t
SIO-UART parity configurations.
| Enumerator | |
|---|---|
| SL_SIO_UART_EVEN_PARITY | SIO-SPI even parity. |
| SL_SIO_UART_ODD_PARITY | SIO-SPI odd parity. |
sl_sio_spi_stop_bit_t#
sl_sio_spi_stop_bit_t
SIO-UART stop bit configurations.
| Enumerator | |
|---|---|
| SL_SIO_UART_STOP_BIT_1 | SIO-UART stop bit 1. |
| SL_SIO_UART_STOP_BIT_2 | SIO-UART stop bit 2. |
Typedef Documentation#
sl_sio_spi_xfer_config_t#
typedef stc_sio_spi_xfer_t sl_sio_spi_xfer_config_t
SIO-SPI Transfer structure.
sl_sio_i2s_config_t#
typedef stc_sio_i2s_config_t sl_sio_i2s_config_t
SIO-I2S configuration structure.
sl_sio_i2s_xfer_config_t#
typedef stc_sio_i2s_xfer_t sl_sio_i2s_xfer_config_t
SIO-I2S Transfer structure.
sl_sio_uart_config_t#
typedef stc_sio_uart_config_t sl_sio_uart_config_t
SIO-UART configuration structure.
sl_sio_i2s_callback_t#
typedef sio_i2s_func_ptr_t sl_sio_i2s_callback_t
SIO-I2S callback function pointer.
sl_sio_spi_callback_t#
typedef sio_Spi_func_ptr_t sl_sio_spi_callback_t
SIO-SPI callback function pointer.
sl_sio_uart_callback_t#
typedef sio_Uart_func_ptr_t sl_sio_uart_callback_t
SIO_UART callback function pointer.
sl_sio_i2c_config_t#
typedef stc_sio_i2c_config_t sl_sio_i2c_config_t
SIO-I2C configuration structure.
Variable Documentation#
Function Documentation#
sl_si91x_sio_init#
sl_status_t sl_si91x_sio_init (void )
Initialize the SIO module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
It initializes the SIO GPIO's and enables the SIO module clock.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_FAIL (0x0001) - Fail, SIO initialization failed
SL_STATUS_OK (0x0000) - Success, SIO initialization successful
sl_si91x_sio_spi_init#
sl_status_t sl_si91x_sio_spi_init (sl_sio_spi_config_t * configuration)
Initialize the SIO-SPI module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sio_spi_config_t * | [in] | configuration | - Pointer to SIO-SPI configuration structure sl_sio_spi_config_t |
It configures the SPI mode, bit length, bit order, SIO frequency, and the SIO channels for the SPI transfer lines.
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success, SPI initialization done properly
sl_si91x_sio_deinit#
void sl_si91x_sio_deinit (void )
This API is used to De-initialize SIO module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_sio_spi_pin_initialization#
sl_status_t sl_si91x_sio_spi_pin_initialization (sl_sio_spi_t * sio_spi_init)
Initialize SIO SPI pins and clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sio_spi_t * | [in] | sio_spi_init | : Pointer to the structure of type sl_sio_spi_t |
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is a null pointer
sl_si91x_sio_uart_pin_initialization#
sl_status_t sl_si91x_sio_uart_pin_initialization (sl_sio_uart_t * sio_uart_init)
Initialize SIO UART pins and clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sio_uart_t * | [in] | sio_uart_init | : Pointer to the structure of type sl_sio_uart_t |
This holds the UART Tx, Rx pins configuration.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is a null pointer
sl_si91x_sio_i2c_pin_initialization#
sl_status_t sl_si91x_sio_i2c_pin_initialization (sl_sio_i2c_t * sio_i2c_init)
Initialize SIO I2C pins and clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sio_i2c_t * | [in] | sio_i2c_init | : Pointer to the structure of type sl_sio_i2c_t |
This holds the I2C SDA, SCL pins configuration.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK - Success
SL_STATUS_NULL_POINTER - The parameter is a null pointer
sl_si91x_sio_spi_cs_assert#
sl_status_t sl_si91x_sio_spi_cs_assert (uint8_t chip_select_num)
Assert the SIO SPI chip select.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | chip_select_num | - Chip select number (0 to 7) |
This tells peripheral that it should wake up and receive / send data and is also used when multiple peripherals are present to select the one you'd like to communicate with.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success
sl_si91x_sio_spi_cs_deassert#
sl_status_t sl_si91x_sio_spi_cs_deassert (uint8_t chip_select_num)
De-assert the SIO SPI chip select.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | chip_select_num | - Chip select number (0 to 7) |
This is used to disable after the last byte is transmitted / received.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success
sl_si91x_sio_spi_register_event_callback#
sl_status_t sl_si91x_sio_spi_register_event_callback (sl_sio_spi_callback_t callback_event)
Register the user callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sio_spi_callback_t | [in] | callback_event | - Pointer to the function sl_sio_spi_callback_t which needs to be called at the time of interrupt. |
It registers the callback, i.e., stores the callback function address and pass to the variable that is called in Interrupt Handler. If another callback is registered without unregistering previous callback then, it returns an error code, so it is mandatory to unregister the callback before registering another callback. It will returns error if any callback is already registered.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK (0x0000) - Success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_BUSY (0x0004) - Driver is busy
sl_si91x_sio_spi_unregister_event_callback#
void sl_si91x_sio_spi_unregister_event_callback (void )
Un-register the user callback function, i.e., clear the callback function address and disables IRQ handler.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_sio_spi_transfer#
sl_status_t sl_si91x_sio_spi_transfer (sl_sio_spi_xfer_config_t * xfer_config)
Transfer the SIO SPI data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sio_spi_xfer_config_t * | [in] | xfer_config | - Pointer to SIO-SPI transfer configuration structure sl_sio_spi_xfer_config_t |
It is used to make the SIO-SPI transfer in non-blocking mode.
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success
sl_si91x_sio_get_version#
sl_sio_version_t sl_si91x_sio_get_version (void )
Get the SIO version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
It is used to get the release, SQA and DEV version of the SIO module. Returns
returns structure of type sl_sio_version_t
sl_si91x_sio_uart_init#
sl_status_t sl_si91x_sio_uart_init (sl_sio_uart_config_t * configuration)
Initialize SIO-UART, i.e., set baud rate, parity, channel selection, stop bits, and data length.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sio_uart_config_t * | [in] | configuration | - Pointer to SIO-UART configuration structure sl_sio_uart_config_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success, UART initialization done properly
sl_si91x_sio_uart_send#
sl_status_t sl_si91x_sio_uart_send (const void * buffer, uint16_t length)
Send the data over SIO-UART in non-blocking mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const void * | [in] | buffer | - data pointer to send |
| uint16_t | [in] | length | - data length |
Transmit bytes from the buffer using an interrupt service. Will return immediately, but cannot be called again until the previous call has finished.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success
sl_si91x_sio_uart_send_blocking#
sl_status_t sl_si91x_sio_uart_send_blocking (const void * buffer, uint16_t length)
Send the data over SIO-UART in blocking mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const void * | [in] | buffer | - data pointer to send |
| uint16_t | [in] | length | - number of bytes to send |
Transmit bytes from the buffer using a blocking send byte function. Does not return until all bytes are sent.
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success
sl_si91x_sio_uart_read#
sl_status_t sl_si91x_sio_uart_read (void * data_buffer, uint16_t num_bytes)
Read data from SIO-UART in non-blocking mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | [out] | data_buffer | - data buffer pointer to read |
| uint16_t | [in] | num_bytes | - number of bytes read |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success
sl_si91x_sio_uart_read_blocking#
sl_status_t sl_si91x_sio_uart_read_blocking (void * data_buffer, uint16_t num_bytes)
Read data from UART in blocking mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | [out] | data_buffer | - data buffer pointer to read |
| uint16_t | [in] | num_bytes | - number of bytes read |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0x0000) - Success
sl_si91x_sio_uart_register_event_callback#
sl_status_t sl_si91x_sio_uart_register_event_callback (sl_sio_uart_callback_t callback_event)
Register the user callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sio_uart_callback_t | [in] | callback_event | - Pointer to the function sl_sio_uart_callback_t which needs to be called at the time of interrupt. |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_OK (0x0000) - Success
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_BUSY (0x0004) - Driver is busy
sl_si91x_sio_i2c_write#
sl_status_t sl_si91x_sio_i2c_write (stc_sio_i2c_config_t * configuration, uint8_t address, uint8_t * data, uint16_t length)
Write data using SIO-I2C.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| stc_sio_i2c_config_t * | [in] | configuration | - pointer to the I2C configuration structure stc_sio_i2c_config_t in SIO module |
| uint8_t | [in] | address | - slave address(1- 255). |
| uint8_t * | [in] | data | - pointer to the data |
| uint16_t | [in] | length | - data length |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_i2c_read#
sl_status_t sl_si91x_sio_i2c_read (stc_sio_i2c_config_t * configuration, uint8_t address, uint8_t * data, uint16_t length)
Read data using SIO-I2C.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| stc_sio_i2c_config_t * | [in] | configuration | - pointer to the I2C configuration structure stc_sio_i2c_config_t in SIO module |
| uint8_t | [in] | address | - slave address(1- 255). |
| uint8_t * | [out] | data | - pointer to the data |
| uint16_t | [in] | length | - data length |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_i2c_transfer#
sl_status_t sl_si91x_sio_i2c_transfer (stc_sio_i2c_config_t * configuration, uint8_t address, uint8_t * tx_buffer, uint16_t tx_length, uint8_t * rx_buffer, uint16_t rx_length)
Transfer data using SIO-I2C.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| stc_sio_i2c_config_t * | [in] | configuration | - Pointer to the I2C configuration structure stc_sio_i2c_config_t in SIO module |
| uint8_t | [in] | address | - Slave address (1- 255). |
| uint8_t * | [in] | tx_buffer | - Pointer to the data transmit buffer |
| uint16_t | [in] | tx_length | - TX data length |
| uint8_t * | [out] | rx_buffer | - Pointer to the data receive buffer |
| uint16_t | [in] | rx_length | - RX data length |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_i2c_generate_start#
void sl_si91x_sio_i2c_generate_start (void )
Generate I2C start in SIO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Pre-condition:
Returns
none
sl_si91x_sio_i2c_generate_stop#
void sl_si91x_sio_i2c_generate_stop (void )
Generate I2C stop in SIO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Pre-conditions:
Returns
none
sl_si91x_sio_uart_unregister_event_callback#
void sl_si91x_sio_uart_unregister_event_callback (void )
Un-register the user callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Pre-conditions:
Returns
none
sl_si91x_sio_uart_rx_done#
void sl_si91x_sio_uart_rx_done (void )
Used when UART receive is done.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Pre-conditions:
Returns
none
sl_si91x_sio_configure_interrupt#
sl_status_t sl_si91x_sio_configure_interrupt (en_sio_channels_t channel, interrupt_flag_t flag)
Configure pin detection mode to be considered for GPIO interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
| interrupt_flag_t | [in] | flag | - GPIO interrupt generated interrupt_flag_t
|
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_match_pattern#
sl_status_t sl_si91x_sio_match_pattern (en_sio_channels_t channel, pattern_match_t pattern, uint8_t slice, uint32_t slice_pattern)
Match the pattern with data to be detected.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
| pattern_match_t | [in] | pattern | - Pattern match bit to be enabled for pattern match to take place pattern_match_t
|
| uint8_t | [in] | slice | - Slice number (0,1,2,8,9,10) to select. |
| uint32_t | [in] | slice_pattern | - Pattern to match for selected slice |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_shift_clock#
sl_status_t sl_si91x_sio_shift_clock (uint32_t divider, en_sio_channels_t channel)
Generate the shift clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | divider | - Desired clock frequency configuration |
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_select_clock#
sl_status_t sl_si91x_sio_select_clock (en_sio_channels_t channel, clock_type_t clock)
Select SIO peripheral clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
| clock_type_t | [in] | clock | - Clock used for shift operations clock_type_t
|
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_position_counter#
sl_status_t sl_si91x_sio_position_counter (en_sio_channels_t channel, uint32_t data_shift)
Shift the number of bits.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
| uint32_t | [in] | data_shift | - Number of shifts to happen before reloading register with data. Value to be set = (total no. of valid bits in shift register/ no. of bits per shift) - 1 |
Number of shifts to happen before reloading the shift register with data/pausing the operation. i.e. value to be set = (total no. of valid bits in shift register/ number of bits per shift) – 1
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_control_flow#
sl_status_t sl_si91x_sio_control_flow (en_sio_channels_t channel, flow_control_t flow_control)
Enable/disable the flow control bit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
| flow_control_t | [in] | flow_control | - It decides whether to continue data shifting based on data present in shift register validation flow_control_t
|
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_reverse_load#
sl_status_t sl_si91x_sio_reverse_load (en_sio_channels_t channel, reverse_load_t reverse)
Load data to buffer in reverse order.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
| reverse_load_t | [in] | reverse | - If data to be shifted out MSB first, it is to be set reverse_load_t |
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_set_interrupt#
sl_status_t sl_si91x_sio_set_interrupt (en_sio_channels_t channel)
Enable the common swap interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_clear_interrupt#
sl_status_t sl_si91x_sio_clear_interrupt (en_sio_channels_t channel)
Disable the common swap interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_mask_interrupt#
sl_status_t sl_si91x_sio_mask_interrupt (en_sio_channels_t channel)
Mask the common swap interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-conditions:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_unmask_interrupt#
sl_status_t sl_si91x_sio_unmask_interrupt (en_sio_channels_t channel)
Unmask the common swap interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_get_interrupt_status#
uint32_t sl_si91x_sio_get_interrupt_status (void )
Read the common swap interrupt status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Pre-condition:
Returns
returns interrupt status
sl_si91x_sio_set_shift_interrupt#
sl_status_t sl_si91x_sio_set_shift_interrupt (en_sio_channels_t channel)
Enable the common shift interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_clear_shift_interrupt#
sl_status_t sl_si91x_sio_clear_shift_interrupt (en_sio_channels_t channel)
Disable the common shift interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_mask_shift_interrupt#
sl_status_t sl_si91x_sio_mask_shift_interrupt (en_sio_channels_t channel)
Mask the common shift interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_unmask_shift_interrupt#
sl_status_t sl_si91x_sio_unmask_shift_interrupt (en_sio_channels_t channel)
Unmask the common shift interrupt.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_shift_interrupt_status#
uint32_t sl_si91x_sio_shift_interrupt_status (void )
Read the common shift interrupt status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] | - SIO channel to be selected en_sio_channels_t |
Pre-condition:
Returns
returns shift interrupt status
sl_si91x_sio_edge_select#
sl_status_t sl_si91x_sio_edge_select (en_sio_channels_t channel, edge_select_t edge_sel)
Select edge of the clock cycle for sampling bits.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
| edge_select_t | [in] | edge_sel | - Select the edge for bit sample to start edge_select_t
|
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success
sl_si91x_sio_read_buffer#
uint32_t sl_si91x_sio_read_buffer (en_sio_channels_t channel)
Read SIO buffer register.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
Pre-condition:
Returns
returns data from buffer
sl_si91x_sio_write_buffer#
sl_status_t sl_si91x_sio_write_buffer (en_sio_channels_t channel, uint32_t data)
Write into SIO buffer register.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| en_sio_channels_t | [in] | channel | - SIO channel to be selected en_sio_channels_t |
| uint32_t | [in] | data | - Data to be written to buffer |
Pre-condition:
Returns
returns status 0 if successful, else error code as follows:
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument
SL_STATUS_NULL_POINTER (0x0022n) - The parameter is null pointer
SL_STATUS_OK (0X000) - Success