Structure to hold the port and pin of SIO UART.
Public Attributes#
uint8_t
SIO UART TX port.
uint8_t
SIO UART TX pin.
uint8_t
SIO UART TX mux.
uint8_t
SIO UART TX pad.
uint8_t
SIO UART RX port.
uint8_t
SIO UART RX pin.
uint8_t
SIO UART RX mux.
uint8_t
SIO UART RX pad.
Public Attribute Documentation#
uart_tx_port#
uint8_t sl_sio_uart_t::uart_tx_port
SIO UART TX port.
Definition at line
165
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h
uart_tx_pin#
uint8_t sl_sio_uart_t::uart_tx_pin
SIO UART TX pin.
Definition at line
166
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h
uart_tx_mux#
uint8_t sl_sio_uart_t::uart_tx_mux
SIO UART TX mux.
Definition at line
167
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h
uart_tx_pad#
uint8_t sl_sio_uart_t::uart_tx_pad
SIO UART TX pad.
Definition at line
168
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h
uart_rx_port#
uint8_t sl_sio_uart_t::uart_rx_port
SIO UART RX port.
Definition at line
169
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h
uart_rx_pin#
uint8_t sl_sio_uart_t::uart_rx_pin
SIO UART RX pin.
Definition at line
170
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h
uart_rx_mux#
uint8_t sl_sio_uart_t::uart_rx_mux
SIO UART RX mux.
Definition at line
171
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h
uart_rx_pad#
uint8_t sl_sio_uart_t::uart_rx_pad
SIO UART RX pad.
Definition at line
172
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h