Structure to hold the threshold detection configuration parameters.

Public Attributes#

uint16_t

Threshold_1.

uint16_t

Threshold_2.

uint8_t *

Threshold_1 condition like Equal, Grater, Lesser.

uint8_t *

Threshold_2 condition like Equal, Grater, Lesser.

uint8_t

Public Attribute Documentation#

threshold1#

uint16_t sl_adc_threshold_config_t::threshold1

Threshold_1.


Definition at line 151 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h

threshold2#

uint16_t sl_adc_threshold_config_t::threshold2

Threshold_2.


Definition at line 152 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h

threshold1_cond#

uint8_t* sl_adc_threshold_config_t::threshold1_cond

Threshold_1 condition like Equal, Grater, Lesser.


Definition at line 153 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h

threshold2_cond#

uint8_t* sl_adc_threshold_config_t::threshold2_cond

Threshold_2 condition like Equal, Grater, Lesser.


Definition at line 154 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h

range#

uint8_t sl_adc_threshold_config_t::range

Definition at line 155 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h