Structure representing HTTP server request URI parameters.
This structure holds the URI path and query parameters for an HTTP server request. It is used to parse and manage the request URI and its associated parameters.
Public Attributes#
char *
URI path. Must be a null-terminated string.
Array of query parameters.
uint16_t
Number of query parameters received in the URI.
Public Attribute Documentation#
query_parameters#
sl_http_server_uri_query_parameter_t sl_http_server_request_uri_t::query_parameters[MAX_QUERY_PARAMETERS]
Array of query parameters.
query_parameter_count#
uint16_t sl_http_server_request_uri_t::query_parameter_count
Number of query parameters received in the URI.