MQTT Client broker information structure.
This structure holds the information required to connect to an MQTT broker, including the broker's IP address, port number, connection encryption status, connection timeout, keep-alive interval, and keep-alive retries.
Public Attributes#
IP address of the broker.
Port number of the broker.
Indicates if the connection is encrypted. This field would be deprecated in future releases. Users are recommended to use tls_flags in sl_mqtt_client_configuration_t.
MQTT connection timeout in milliseconds.
Keep-alive interval of the MQTT connection in seconds.
Number of MQTT ping retries.
Public Attribute Documentation#
is_connection_encrypted#
bool sl_mqtt_broker_t::is_connection_encrypted
Indicates if the connection is encrypted. This field would be deprecated in future releases. Users are recommended to use tls_flags in sl_mqtt_client_configuration_t.
keep_alive_interval#
uint16_t sl_mqtt_broker_t::keep_alive_interval
Keep-alive interval of the MQTT connection in seconds.