MQTT Client credentials structure.

This structure holds the credentials required for the MQTT client to authenticate with the broker. It includes the lengths of the username and password, and a flexible array to store both the username and password.

Public Attributes#

uint16_t

Length of the username. Should not exceed 120 bytes including NULL termination character.

uint16_t

Length of the password. Should not exceed 60 bytes including NULL termination character.

uint8_t

Flexible array to store both the username and password.

Public Attribute Documentation#

username_length#

uint16_t sl_mqtt_client_credentials_t::username_length

Length of the username. Should not exceed 120 bytes including NULL termination character.


password_length#

uint16_t sl_mqtt_client_credentials_t::password_length

Length of the password. Should not exceed 60 bytes including NULL termination character.


data#

uint8_t sl_mqtt_client_credentials_t::data[]

Flexible array to store both the username and password.