Structure to hold the clock configuration parameters.
Public Attributes#
uint16_t
Division factor (0 to 1023).
uint32_t
SoC PLL clock frequency.
uint32_t
SoC PLL reference clock frequency.
Public Attribute Documentation#
division_factor#
uint16_t sl_dac_clock_config_t::division_factor
Division factor (0 to 1023).
Definition at line
120
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_dac.h
soc_pll_clock#
uint32_t sl_dac_clock_config_t::soc_pll_clock
SoC PLL clock frequency.
Definition at line
121
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_dac.h
soc_pll_reference_clock#
uint32_t sl_dac_clock_config_t::soc_pll_reference_clock
SoC PLL reference clock frequency.
Definition at line
122
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_dac.h