USART#
Introduction#
USART is used in communication through wired medium in both synchronous and asynchronous fashion.
In synchronous mode, both full duplex and half duplex (single wire) modes are supported.


A USART frame consists of:
Start bit: Indicates the beginning of a data frame.
Data bits: The actual data to be transmitted (typically 7 or 8 bits).
Parity bit: Optional bit for error checking.
Stop bit: Indicates the end of a data frame.
USART is widely used in embedded systems due to its simplicity and versatility. Some common applications include:
Sensor data acquisition: Reading data from sensors like temperature, humidity, pressure, etc.
Actuator control: Sending commands to motors, servos, and other actuators.
Human-machine interface (HMI): Communicating with keyboards, displays, and other user interface devices.
Debug and logging: Sending diagnostic information to a computer for analysis.
Communication with other devices: Interfacing with modules like GPS, Bluetooth, Wi-Fi, etc.
Configuration#
USART can be configured using several parameters, including:
Transmit Mode:
Synchronous mode (sl_si91x_usart_transfer_data).
Asynchronous mode (sl_si91x_usart_async_send_data).
Receive Mode:
Synchronous mode (sl_si91x_usart_transfer_data).
Asynchronous mode (sl_si91x_usart_async_receive_data).
Note
In synchronous mode, USART signals are given out on the interface, and interface signals are given to the USART module, blocking inputs to UART.
In asynchronous mode, UART signals are given out on the interface, and interface signals are given to the UART module, blocking inputs to USART.
For more information on configuring available parameters, see the respective peripheral example readme document.
Usage#
USART has to be initialized and configured first by calling sl_si91x_usart_init. The DMA (Direct Memory Access) controller in the USART driver will enable efficient data transfer, thus reducing CPU overhead. Initialization of the DMA for UART/USART will also be done with the same USART init function, if DMA is enabled for data transfers. The other common functions include the following:
You can use this in two modes:
Full Duplex Mode:
Set synchronous mode.
Write data to TX FIFO.
Write count to RX_CNT.
Set auto_flow_ctrl if controlled transfers on the interface.
Half Duplex Mode:
Transmit Mode:
Reset full_duplex_mode.
Set tx_mode.
Reset rx_mode.
Write data to TX_FIFO by polling the FIFO full/afull status.
Receive Mode:
Reset full_duplex_mode.
Set rx_mode.
Reset tx_mode.
Write RX_CNT with the number of bytes to be received.
Read data from RX_FIFO by polling the RX FIFO empty/aempty status.
The other common functions include the following:
Modules#
sl_si91x_usart_control_config_t
Enumerations#
Enumeration for USART/UART events.
Enumeration for general power states used in this peripheral.
Enumeration for USART data bits configuration.
Enumeration for USART parity selection.
Enumeration for USART modem control selection.
Enumeration for USART stop bits selection.
Enumeration for hardware flow control selection.
Enumeration for USART mode selection.
Enumeration for USART miscellaneous control selection.
Typedefs#
Alias for ARM_USART_SignalEvent_t type.
Alias for ARM_USART_Status type.
Alias for ARM_POWER_STATE type.
Alias for ARM_USART_MODEM_CONTROL type.
Alias for ARM_USART_MODEM_STATUS type.
Alias for ARM_USART_CAPABILITIES type.
Alias for ARM_DRIVER_USART type.
Alias for USART_RESOURCES type.
Alias for a constant void pointer type, used as a handle for USART resources.
Functions#
To initialize the USART/UART module.
To uninitialize the USART/UART module.
To register the user callback function for USART events.
To unregister the user callback function for USART events.
To register the user callback function for multiple USART instances.
To unregister the user callback function for multiple USART instances.
To send the USART data when USART/UART is configured.
To send data in async mode when USART/UART is configured.
To receive data when USART/UART is configured.
To receive data in async mode when USART/UART is configured.
To send and receive data when USART in Synchronous mode is enabled.
To get the TX data count of USART/UART.
To get the RX data count of USART/UART.
To control and configure the USART/UART module in different configurations.
To configure the USART interface with non-UC configurations.
To get the USART/UART status.
To set the USART modem control line.
To get the USART modem control status.
To get the USART version.
To get the USART configurations set in the module, such as baud rate, parity bit, stop bits, etc.
Enumeration Documentation#
usart_event_typedef_t#
usart_event_typedef_t
Enumeration for USART/UART events.
This enumeration defines the various events that can occur in the USART/UART interface. Each event corresponds to a specific condition or status change in the USART/UART operation.
| Enumerator | |
|---|---|
| SL_USART_EVENT_SEND_COMPLETE | Send complete event. |
| SL_USART_EVENT_RECEIVE_COMPLETE | Receive complete event. |
| SL_USART_EVENT_TRANSFER_COMPLETE | Transfer complete event. |
| SL_USART_EVENT_TX_COMPLETE | TX complete event. |
| SL_USART_EVENT_TX_UNDERFLOW | TX underflow event. |
| SL_USART_EVENT_RX_OVERFLOW | RX overflow event. |
| SL_USART_EVENT_RX_TIMEOUT | RX timeout event. |
| SL_USART_EVENT_RX_BREAK | RX break event. |
| SL_USART_EVENT_RX_FRAMING_ERROR | RX framing error event. |
| SL_USART_EVENT_RX_PARITY_ERROR | RX parity error event. |
| SL_USART_EVENT_CTS | CTS (Clear to Send) event. |
| SL_USART_EVENT_DSR | DSR (Data Set Ready) event. |
| SL_USART_EVENT_DCD | DCD (Data Carrier Detect) event. |
| SL_USART_EVENT_RI | RI (Ring Indicator) event. |
power_mode_typedef_t#
power_mode_typedef_t
Enumeration for general power states used in this peripheral.
This enumeration defines the various power states that can be used to control the power mode of the peripheral. Each state corresponds to a specific power configuration.
| Enumerator | |
|---|---|
| SL_POWER_OFF | Power off state. |
| SL_POWER_LOW | Low power state. |
| SL_POWER_FULL | Full power state. |
| SL_POWER_MODE_LAST | Last power mode for validation purposes. |
usart_databits_typedef_t#
usart_databits_typedef_t
Enumeration for USART data bits configuration.
This enumeration defines the possible data bit configurations for the USART interface. The user can select the appropriate data bit setting based on their application requirements.
| Enumerator | |
|---|---|
| SL_USART_DATA_BITS_5 | 5 data bits. |
| SL_USART_DATA_BITS_6 | 6 data bits. |
| SL_USART_DATA_BITS_7 | 7 data bits. |
| SL_USART_DATA_BITS_8 | 8 data bits. |
usart_parity_typedef_t#
usart_parity_typedef_t
Enumeration for USART parity selection.
This enumeration defines the possible parity configurations for the USART interface. The user can select the appropriate parity setting based on their application requirements.
| Enumerator | |
|---|---|
| SL_USART_NO_PARITY | No parity. |
| SL_USART_EVEN_PARITY | Even parity. |
| SL_USART_ODD_PARITY | Odd parity. |
usart_modem_control_typedef_t#
usart_modem_control_typedef_t
Enumeration for USART modem control selection.
This enumeration defines the possible modem control configurations for the USART interface. The user can select the appropriate modem control setting based on their application requirements.
| Enumerator | |
|---|---|
| SL_USART_RTS_CLEAR | Clear RTS (Request to Send). |
| SL_USART_RTS_SET | Set RTS (Request to Send). |
| SL_USART_DTR_CLEAR | Clear DTR (Data Terminal Ready). |
| SL_USART_DTR_SET | Set DTR (Data Terminal Ready). |
| SL_USART_MODEM_CONTROL_LAST | Last modem control option for validation purposes. |
usart_stopbit_typedef_t#
usart_stopbit_typedef_t
Enumeration for USART stop bits selection.
This enumeration defines the possible stop bit configurations for the USART interface, used for asynchronous operation. The user can select the appropriate stop bit setting based on their application requirements.
| Enumerator | |
|---|---|
| SL_USART_STOP_BITS_1 | 1 stop bit. |
| SL_USART_STOP_BITS_1_5 | 1.5 stop bits. |
| SL_USART_STOP_BITS_2 | 2 stop bits. |
usart_hwflowcontol_typedef_t#
usart_hwflowcontol_typedef_t
Enumeration for hardware flow control selection.
This enumeration defines the possible hardware flow control configurations for the USART interface. The user can select the appropriate flow control setting based on their application requirements.
| Enumerator | |
|---|---|
| SL_USART_FLOW_CONTROL_NONE | No hardware flow control. |
| SL_USART_FLOW_CONTROL_CTS | CTS signal is enabled for TX flow control. |
| SL_USART_FLOW_CONTROL_RTS | RTS signal is enabled for RX flow control. |
| SL_USART_FLOW_CONTROL_RTS_CTS | CTS and RTS signals are enabled for TX and RX flow control. |
usart_mode_typedef_t#
usart_mode_typedef_t
Enumeration for USART mode selection.
This enumeration defines the possible modes of operation for the USART interface. It is crucial to tailor the communication channel to the specific requirements of a system.
| Enumerator | |
|---|---|
| SL_USART_MODE_ASYNCHRONOUS | Asynchronous mode. |
| SL_USART_MODE_SYNCHRONOUS_MASTER | Synchronous mode master. |
| SL_USART_MODE_SYNCHRONOUS_SLAVE | Synchronous mode slave. |
| SL_USART_MODE_SINGLE_WIRE | UART Single-wire (half-duplex); arg = Baudrate. |
| SL_USART_MODE_IRDA | UART IrDA; arg = Baudrate. |
usart_misc_control_typedef_t#
usart_misc_control_typedef_t
Enumeration for USART miscellaneous control selection.
Note
UART provides the underlying serial communication, while IrDA enables the wireless transmission of that data using infrared light.
This enumeration defines the various miscellaneous control options available for the USART interface. These controls allow for fine-tuning and managing specific USART operations.
| Enumerator | |
|---|---|
| SL_USART_MISC_CONTROL_NONE | No miscellaneous control. |
| SL_USART_SET_DEFAULT_TX_VALUE | Set default TX value. |
| SL_USART_CONTROL_TX | Control the transfer line. |
| SL_USART_CONTROL_RX | Control the receive line. |
| SL_USART_CONTROL_BREAK | Set USART control break. |
| SL_USART_ABORT_SEND | Abort the send operation. |
| SL_USART_ABORT_RECEIVE | Abort the receive operation. |
| SL_USART_ABORT_TRANSFER | Abort the transfer operation. |
Typedef Documentation#
sl_usart_signal_event_t#
typedef ARM_USART_SignalEvent_t sl_usart_signal_event_t
Alias for ARM_USART_SignalEvent_t type.
sl_usart_power_state_t#
typedef ARM_POWER_STATE sl_usart_power_state_t
Alias for ARM_POWER_STATE type.
sl_usart_modem_control_t#
typedef ARM_USART_MODEM_CONTROL sl_usart_modem_control_t
Alias for ARM_USART_MODEM_CONTROL type.
sl_usart_modem_status_t#
typedef ARM_USART_MODEM_STATUS sl_usart_modem_status_t
Alias for ARM_USART_MODEM_STATUS type.
sl_usart_capabilities_t#
typedef ARM_USART_CAPABILITIES sl_usart_capabilities_t
Alias for ARM_USART_CAPABILITIES type.
sl_usart_handle_t#
typedef const void* sl_usart_handle_t
Alias for a constant void pointer type, used as a handle for USART resources.
Function Documentation#
sl_si91x_usart_init#
sl_status_t sl_si91x_usart_init (usart_peripheral_t usart_instance, sl_usart_handle_t * usart_handle)
To initialize the USART/UART module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| usart_peripheral_t | [in] | usart_instance | The USART instance (USART_0, UART_1, ULPUART). |
| sl_usart_handle_t * | [in] | usart_handle | Pointer to the USART/UART driver. |
This function configures the clocks for the USART/UART module and also initializes the DMA for UART/USART if DMA is enabled for data transfers.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, UART/USART initialization done properly.
SL_STATUS_FAIL (0x0001) - Function failed, UART/USART initialization failed.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_deinit#
sl_status_t sl_si91x_usart_deinit (sl_usart_handle_t usart_handle)
To uninitialize the USART/UART module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
This function will disable the clocks for the USART/UART module and also de-initialize the DMA for UART/USART if DMA is enabled for data transfers.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, UART/USART deinitialization done properly.
SL_STATUS_FAIL (0x0001) - Fail, UART/USART deinitialization failed.
Note
When the USART/UART module is used in combination with other peripherals, while deinitializing in the application, see the notes below:
Whenever sl_si91x_usart_deinit() gets called, it will disable the clock for the peripheral. To power off the peripheral, we have to power down the power domain (PERI_EFUSE) which contains the different peripherals mentioned below: i.e., USART, UART, I2C, SSI Master, SSI Slave, Generic-SPI Master, I2S Master, I2S Slave, Micro-DMA Controller, Config Timer, Random-Number Generator, CRC Accelerator, SIO, QEI, MCPWM, and EFUSE. Use the below API to power down the particular power domain if other peripherals are not being used: sl_si91x_peri_efuse_power_down(power_down);
A few peripherals (ULP Peripherals, UULP Peripherals, GPDMA, and SDIO-SPI) have separate domains; those can be powered down independently. For additional details, see the Power architecture section in the Hardware Reference Manual. Here, ULP_UART has a separate power domain ULPSS_PWRGATE_ULP_UART, which can be powered down independently. See the rsi_power_save.h file for all power gate definitions.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_register_event_callback#
sl_status_t sl_si91x_usart_register_event_callback (sl_usart_signal_event_t callback_event)
To register the user callback function for USART events.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_signal_event_t | [in] | callback_event | Pointer to the function which needs to be called at the time of interrupt. |
This API registers a user-defined callback function for USART events. If another callback is registered without unregistering the previous callback, it returns an error code. Therefore, it is mandatory to unregister the callback before registering another callback.
Pre-condition:
sl_si91x_usart_set_configuration must be called prior.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_BUSY (0x0004) - Driver is busy.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_unregister_event_callback#
void sl_si91x_usart_unregister_event_callback (void )
To unregister the user callback function for USART events.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This API unregisters a user-defined callback function for USART events. It is mandatory to unregister the current callback before registering a new one.
sl_si91x_usart_multiple_instance_register_event_callback#
sl_status_t sl_si91x_usart_multiple_instance_register_event_callback (usart_peripheral_t usart_instance, sl_usart_signal_event_t callback_event)
To register the user callback function for multiple USART instances.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| usart_peripheral_t | [in] | usart_instance | The USART instance. |
| sl_usart_signal_event_t | [in] | callback_event | Pointer to the function which needs to be called at the time of interrupt. |
This function registers a user-defined callback function for multiple USART instances (e.g., USART_0, UART_1, ULP_UART). This API should be used to handle different USART instances.
Pre-condition:
sl_si91x_usart_set_configuration must be called prior.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_BUSY (0x0004) - Driver is busy.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_multiple_instance_unregister_event_callback#
void sl_si91x_usart_multiple_instance_unregister_event_callback (usart_peripheral_t usart_instance)
To unregister the user callback function for multiple USART instances.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| usart_peripheral_t | [in] | usart_instance | This is the USART instance. |
This function unregisters a user-defined callback function for multiple USART instances (e.g., USART_0, UART_1, ULP_UART). This API should be used to handle different USART instances.
sl_si91x_usart_send_data#
sl_status_t sl_si91x_usart_send_data (sl_usart_handle_t usart_handle, const void * data, uint32_t data_length)
To send the USART data when USART/UART is configured.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
| const void * | [in] | data | Pointer to the variable which contains transfer data. |
| uint32_t | [in] | data_length | Length of the data to be sent. |
If DMA mode is set, this function will configure the DMA channel and enable the DMA channel, then transfer the data pointed to it. Otherwise, it fills the data to the transfer FIFO and transfers the data.
Pre-conditions:
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, data transfer completed.
SL_STATUS_FAIL (0x0001) - Function failed, data transfer failed.
SL_STATUS_BUSY (0x0004) - Busy, data transfer is already in progress.
SL_STATUS_INVALID_PARAMETER (0x0021) - Invalid parameter.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_async_send_data#
sl_status_t sl_si91x_usart_async_send_data (sl_usart_handle_t usart_handle, const void * data, uint32_t data_length)
To send data in async mode when USART/UART is configured.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
| const void * | [in] | data | Pointer to the variable which contains the data to be transferred. |
| uint32_t | [in] | data_length | Length of the data to be transferred. |
This function returns immediately (non-blocking) and data transfer happens asynchronously. Once the data transfer completes, the registered user callback gets invoked.
Pre-conditions:
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, data transfer completed.
SL_STATUS_FAIL (0x0001) - Function failed, data transfer failed.
SL_STATUS_BUSY (0x0004) - Busy, data transfer is already in progress.
SL_STATUS_INVALID_PARAMETER (0x0021) - Invalid parameter.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_receive_data#
sl_status_t sl_si91x_usart_receive_data (sl_usart_handle_t usart_handle, void * data, uint32_t data_length)
To receive data when USART/UART is configured.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
| void * | [in] | data | Pointer to the variable which will store the received data. |
| uint32_t | [in] | data_length | Length of the data to be received. |
If DMA mode is set, this function configures the DMA channel, enables the DMA channel, and receives data via DMA. If DMA mode is not set, it receives the data from FIFO.
Pre-conditions:
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, data received successfully.
SL_STATUS_FAIL (0x0001) - Function failed, data transfer failed.
SL_STATUS_BUSY (0x0004) - Busy, data transfer is already in progress.
SL_STATUS_INVALID_PARAMETER (0x0021) - Invalid parameter.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_async_receive_data#
sl_status_t sl_si91x_usart_async_receive_data (sl_usart_handle_t usart_handle, void * data, uint32_t data_length)
To receive data in async mode when USART/UART is configured.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
| void * | [in] | data | Pointer to the variable which will store the received data. |
| uint32_t | [in] | data_length | Length of the data to be received. |
This function returns immediately (non-blocking) and data reception happens asynchronously. Once the data reception completes, the registered user callback gets invoked.
Pre-conditions:
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, data received successfully.
SL_STATUS_FAIL (0x0001) - Function failed, data transfer failed.
SL_STATUS_BUSY (0x0004) - Busy, data transfer is already in progress.
SL_STATUS_INVALID_PARAMETER (0x0021) - Invalid parameter.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_transfer_data#
sl_status_t sl_si91x_usart_transfer_data (sl_usart_handle_t usart_handle, const void * data_out, void * data_in, uint32_t data_length)
To send and receive data when USART in Synchronous mode is enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
| const void * | [in] | data_out | Pointer to the variable which will store the data to be transferred. |
| void * | [in] | data_in | Pointer to the variable which will store the received data. |
| uint32_t | [in] | data_length | Length of the data to be received. |
This function sends and receives data to and from the USART transmitter and receiver in synchronous mode of operation. It configures the DMA channel and enables the DMA channel, if DMA mode is set, and transfers the data pointed to it; otherwise, it transfers the data from FIFO.
Pre-conditions:
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, data transfer completed.
SL_STATUS_FAIL (0x0001) - Function failed, data transfer failed.
SL_STATUS_BUSY (0x0004) - Busy, data transfer is already in progress.
SL_STATUS_INVALID_PARAMETER (0x0021) - Invalid parameter.
Note
This function is to be used in USART mode only (i.e., synchronous mode). In asynchronous mode, use sl_si91x_usart_receive_data() and sl_si91x_usart_send_data().
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_get_tx_data_count#
uint32_t sl_si91x_usart_get_tx_data_count (sl_usart_handle_t usart_handle)
To get the TX data count of USART/UART.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | This is the pointer to the USART/UART driver. |
This function returns the number of bytes transferred by the USART/UART. It can be used to check the progress of data transmission.
Returns
uint32_t The number of bytes transferred.
sl_si91x_usart_get_rx_data_count#
uint32_t sl_si91x_usart_get_rx_data_count (sl_usart_handle_t usart_handle)
To get the RX data count of USART/UART.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | This is the pointer to the USART/UART driver. |
This function returns the number of bytes received by the USART/UART. It can be used to check the progress of data reception.
Returns
uint32_t The number of bytes received.
sl_si91x_usart_set_configuration#
sl_status_t sl_si91x_usart_set_configuration (sl_usart_handle_t usart_handle, sl_si91x_usart_control_config_t * control_configuration)
To control and configure the USART/UART module in different configurations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
| sl_si91x_usart_control_config_t * | [in] | control_configuration | Pointer to the USART configurations. |
This function configures the USART in different configurations such as USART mode, data bits, parity, stop bits, flow control, and baud rate.
Note
control_configuration - This parameter is used to pass the respective peripheral configuration when
USART_UC, UART_UC, ULP_UART_UC macros are disabled for a particular instance. When these macros are enabled, configurations are taken directly from the UC and this parameter is not considered.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, UART/USART initialization done properly.
SL_STATUS_BUSY (0x0004) - Busy, data transfer is already in progress.
SL_STATUS_NOT_SUPPORTED (0x000F) - Feature not supported.
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument.
SL_STATUS_INVALID_MODE (0x0024) - USART invalid mode of operation.
For more information on status codes, see SL STATUS DOCUMENTATION.
sli_si91x_usart_set_non_uc_configuration#
sl_status_t sli_si91x_usart_set_non_uc_configuration (sl_usart_handle_t usart_handle, sl_si91x_usart_control_config_t * control_configuration)
To configure the USART interface with non-UC configurations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
| sl_si91x_usart_control_config_t * | [in] | control_configuration | Pointer to the USART configurations. |
This internal function configures the USART interface with different configurations, such as USART mode, data bits, parity, stop bits, flow control, and baud rate. This API will not pick the configurations from USART UC.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, UART/USART initialization done properly.
SL_STATUS_BUSY (0x0004) - Busy, data transfer is already in progress.
SL_STATUS_NOT_SUPPORTED (0x000F) - Feature not supported.
SL_STATUS_INVALID_PARAMETER (0x0021) - The parameter is an invalid argument.
SL_STATUS_INVALID_MODE (0x0024) - USART invalid mode of operation.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_get_status#
sl_usart_status_t sl_si91x_usart_get_status (sl_usart_handle_t usart_handle)
To get the USART/UART status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
This function returns the USART/UART transfer and receive status. It provides information about the current state of the USART/UART, including:
TX busy
RX busy
TX underflow
RX overflow
RX break
RX framing error
RX parity error
Returns
sl_usart_status_t The status of the USART/UART.
sl_si91x_usart_set_modem_control#
sl_status_t sl_si91x_usart_set_modem_control (sl_usart_handle_t usart_handle, sl_usart_modem_control_t control)
To set the USART modem control line.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
| sl_usart_modem_control_t | [in] | control | The USART modem control. |
This function sets the USART modem control line based on the provided control parameter.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, UART/USART initialization done properly.
SL_STATUS_NOT_SUPPORTED (0x000F) - Feature not supported.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_usart_get_modem_status#
sl_usart_modem_status_t sl_si91x_usart_get_modem_status (sl_usart_handle_t usart_handle)
To get the USART modem control status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_usart_handle_t | [in] | usart_handle | Pointer to the USART/UART driver. |
This function returns the status of the USART modem control lines, indicating whether the states are active or not.
Returns
sl_usart_modem_status_t The status of the USART modem control lines.
sl_si91x_usart_get_version#
sl_usart_version_t sl_si91x_usart_get_version (void )
To get the USART version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function returns the version information of the USART driver. It can be used to check the driver version for compatibility and debugging purposes.
Returns
sl_usart_version_t The version information of the USART driver.
sl_si91x_usart_get_configurations#
sl_status_t sl_si91x_usart_get_configurations (uint8_t usart_module, sl_si91x_usart_control_config_t * usart_config)
To get the USART configurations set in the module, such as baud rate, parity bit, stop bits, etc.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | usart_module | USART peripheral type:
|
| sl_si91x_usart_control_config_t * | [in] | usart_config | Pointer to the USART configurations structure. |
This function retrieves the current configurations of the specified USART module.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success, UART/USART configurations retrieved successfully.
SL_STATUS_NULL_POINTER (0x0022) - Invalid NULL pointer received as argument.
For more information on status codes, see SL STATUS DOCUMENTATION.