PSRAM configuration handle structure.
Public Attributes#
PSRAMDevType
PSRAM Device enum value.
Device ID struct.
uint32_t
Device Density in bits.
uint32_t
Max frequency for normal read.
uint32_t
Max frequency for fast read.
PSRAMRWType
Read-Write type configuration.
spi_config_t
SPI Config for QSPI interface.
uint16_t
Default burst wrap size.
uint16_t
Toggle Burst Wrap size.
Public Attribute Documentation#
deviceName#
PSRAMDevType sl_psram_info_type_t::deviceName
PSRAM Device enum value.
Definition at line
205
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h
deviceID#
sl_psram_id_type_t sl_psram_info_type_t::deviceID
Device ID struct.
Definition at line
206
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h
devDensity#
uint32_t sl_psram_info_type_t::devDensity
Device Density in bits.
Definition at line
207
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h
normalReadMAXFrequency#
uint32_t sl_psram_info_type_t::normalReadMAXFrequency
Max frequency for normal read.
Definition at line
208
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h
fastReadMAXFrequency#
uint32_t sl_psram_info_type_t::fastReadMAXFrequency
Max frequency for fast read.
Definition at line
209
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h
rwType#
PSRAMRWType sl_psram_info_type_t::rwType
Read-Write type configuration.
Definition at line
210
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h
spi_config#
spi_config_t sl_psram_info_type_t::spi_config
SPI Config for QSPI interface.
Definition at line
211
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h
defaultBurstWrapSize#
uint16_t sl_psram_info_type_t::defaultBurstWrapSize
Default burst wrap size.
Definition at line
212
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h
toggleBurstWrapSize#
uint16_t sl_psram_info_type_t::toggleBurstWrapSize
Toggle Burst Wrap size.
Definition at line
213
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h