Structure to hold the port and pin configurations for different events.

This structure defines the configuration parameters for the PWM GPIO related to fault events. It includes settings for the port, pin, mux, and pad.

Public Attributes#

uint8_t

PWM GPIO port.

uint8_t

PWM GPIO pin.

uint8_t

PWM GPIO mux.

uint8_t

PWM GPIO pad.

Public Attribute Documentation#

port#

uint8_t sl_pwm_fault_init_t::port

PWM GPIO port.


Definition at line 421 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

pin#

uint8_t sl_pwm_fault_init_t::pin

PWM GPIO pin.


Definition at line 422 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

mux#

uint8_t sl_pwm_fault_init_t::mux

PWM GPIO mux.


Definition at line 423 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h

pad#

uint8_t sl_pwm_fault_init_t::pad

PWM GPIO pad.


Definition at line 424 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_pwm.h