Structure to hold the clock configuration parameters.
Public Attributes#
uint16_t
Clock division factor.
uint16_t
Interface PLL control value.
uint32_t
Interface PLL clock frequency.
uint32_t
Interface PLL reference clock frequency.
uint32_t
SoC PLL clock frequency.
uint32_t
SoC PLL reference clock frequency.
uint8_t
SoC PLL count value.
Public Attribute Documentation#
division_factor#
uint16_t sl_ssi_clock_config_t::division_factor
Clock division factor.
Definition at line
148
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h
intf_pll_500_control_value#
uint16_t sl_ssi_clock_config_t::intf_pll_500_control_value
Interface PLL control value.
Definition at line
149
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h
intf_pll_clock#
uint32_t sl_ssi_clock_config_t::intf_pll_clock
Interface PLL clock frequency.
Definition at line
150
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h
intf_pll_reference_clock#
uint32_t sl_ssi_clock_config_t::intf_pll_reference_clock
Interface PLL reference clock frequency.
Definition at line
151
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h
soc_pll_clock#
uint32_t sl_ssi_clock_config_t::soc_pll_clock
SoC PLL clock frequency.
Definition at line
152
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h
soc_pll_reference_clock#
uint32_t sl_ssi_clock_config_t::soc_pll_reference_clock
SoC PLL reference clock frequency.
Definition at line
153
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h
soc_pll_mm_count_value#
uint8_t sl_ssi_clock_config_t::soc_pll_mm_count_value
SoC PLL count value.
Definition at line
154
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ssi.h