GPDMA#

Introduction#

The GPDMA (General Purpose Direct Memory Access) peripheral enables efficient data transfers between memory and peripherals or between memory regions without CPU intervention. This offloads the CPU, reduces latency, and improves overall system performance.

Key Features:

  1. Supports multiple independent DMA channels.

  2. Configurable channel priorities.

  3. Supports memory-to-memory, memory-to-peripheral, peripheral-to-memory, and peripheral-to-peripheral transfers.

  4. Flexible data width and burst size configuration.

  5. Linked list (descriptor-based) transfer support for complex or large data moves.

  6. FIFO buffer allocation for optimized throughput.

  7. Callback support for transfer completion and error handling.

  8. Hardware flow control options.

Configuration#

The GPDMA can be configured for various transfer types and operational modes, including:

  • Memory-to-Memory: Direct transfer between two memory locations.

  • Memory-to-Peripheral: Transfer from memory to a peripheral register.

  • Peripheral-to-Memory: Transfer from a peripheral register to memory.

  • Peripheral-to-Peripheral: Transfer between two peripheral registers.

  • Linked List Mode: Use descriptors for chained or scatter-gather transfers.

  • FIFO Allocation: Assign FIFO buffers to channels for burst transfers.

  • Callback Registration: Register callbacks for transfer complete, descriptor fetch, and error events. These configurations are encapsulated in the sl_si91x_gpdma_channel_config_t and related structures, and initialized using the provided GPDMA APIs.

For more details on configuration parameters, see the respective peripheral example readme document.

Usage#

After defining the GPDMA configuration structures and passing the appropriate parameters, the following functions can be used to initialize and operate the GPDMA peripheral. The typical flow for implementation is as follows:

  1. Initialize the GPDMA driver: sl_si91x_gpdma_init

  2. Allocate a DMA channel: sl_si91x_gpdma_allocate_channel

  3. Register callbacks for transfer and error events: sl_si91x_gpdma_register_callbacks

  4. Allocate and configure descriptors as needed: sl_si91x_gpdma_allocate_descriptor, sl_si91x_gpdma_build_descriptor

  5. Start a transfer: sl_si91x_gpdma_transfer

  6. Optionally allocate FIFO buffers: sl_si91x_gpdma_allocate_fifo

  7. Stop or deallocate the channel when done: sl_si91x_gpdma_stop_transfer, sl_si91x_gpdma_deallocate_channel

Modules#

sl_gpdma_callback_pointer_t

sl_gpdma_channel_data_t

sl_si91x_gpdma_resources_Data_t

Enumerations#

enum
SL_GPDMA_HRESP_ERROR_CB = 0
SL_GPDMA_DESCRIPTOR_FETCH_DONE_CB = 1
SL_GPDMA_TRANSFER_DONE_CB = 2
SL_GPDMA_GPDMAC_ERROR_CB = 3
}

Enumeration that holds 8-bit codes used by the callback_type parameter in the sl_si91x_gpdma_unregister_callbacks function.

Typedefs#

typedef void(*

Callback function type.

typedef RSI_GPDMA_DESC_T

GPDMA descriptor structure.

typedef GPDMA_DATACONTEXT_T

GPDMA data context structure.

GPDMA descriptor configuration structure.

typedef RSI_GPDMA_HANDLE_T

GPDMA handle type.

typedef RSI_GPDMA_CHA_CFG_T

GPDMA channel configuration structure.

typedef RSI_GPDMA_INIT_T

GPDMA initialization structure.

typedef gpdmaTransferCompleteCB

GPDMA transfer complete callback type.

Functions#

sl_status_t

To initialize the GPDMA peripheral.

sl_status_t
sl_si91x_gpdma_allocate_channel(uint32_t *channel_no, uint32_t priority, uint32_t max_transfer_size)

To allocate a GPDMA channel for the transfer.

sl_status_t

To deallocate the GPDMA channel.

sl_status_t
sl_si91x_gpdma_register_callbacks(uint32_t channel_no, sl_gpdma_callback_pointer_t *callback_t)

To register the GPDMA callbacks (transfer complete & error).

sl_status_t
sl_si91x_gpdma_unregister_callbacks(uint32_t channel_no, uint8_t callback_type)

To unregister the GPDMA callbacks (transfer complete and error).

sl_status_t
sl_si91x_gpdma_transfer(uint32_t channel, void *src, void *dest)

To start a simple memory-to-memory DMA transfer.

sl_status_t
sl_si91x_gpdma_stop_transfer(uint32_t channel_no)

To stop the GPDMA transfer.

sl_status_t
sl_si91x_gpdma_allocate_descriptor(sl_si91x_gpdma_descriptor_t *pDesc_memory, uint32_t transfer_size, uint32_t channel_number)

Allocates a GPDMA descriptor with default config for given channel based on tranfer size.

sl_status_t
sl_Si91x_gpdma_deallocate_descriptor(uint32_t channel_number)

Deallocates a DMA descriptor for the specified channel number.

sl_status_t
sl_si91x_gpdma_build_descriptor(sl_si91x_gpdma_descriptor_t *pDescriptor_memory, sl_si91x_gpdma_descriptor_config_t *pDesc_config, uint32_t transfer_size, uint32_t channel_number)

Builds a GPDMA descriptor with the specified configuration.

sl_status_t
sl_si91x_gpdma_allocate_fifo(uint32_t channel_no, uint32_t fifo_size)

Allocates a FIFO buffer of the specified size to a GPDMA channel.

sl_status_t
sl_si91x_get_channel_fifo_size(uint32_t channel_no, uint32_t *fifo_size)

Gets the FIFO size of a specified GPDMA channel.

sl_status_t
sl_si91x_gpdma_get_channel_status(uint32_t channel_number)

Gets the current status of a specified GPDMA channel.

sl_status_t

This function deinitializes the GPDMA driver.

Macros#

#define

Status code indicates that the DMA channel already allocated for another transfer.

#define

Status code indicates that no DMA channel is available for allocation.

#define

Status code indicates that the DMA channel is already unallocated.

#define

Status code indicates that channel is not allocated for DMA transfer.

#define

Status code indicates that the channel is not available for allocation.

#define

Status code indicates that no DMA channel is available for allocation.

#define

Status code indicates that the descriptor memory buffer is already allocated.

#define

Status code indicates that the descriptor memory buffer is not sufficient.

#define

Status code indicates that the channel is not allocated for DMA transfer.

#define

Status code indicates that Memory buffer is not allocated for the given channel.

#define

Maximum GPDMA channel priority.

#define

Data width 8 bits.

#define

Data width 16 bits.

#define

Data width 32 bits.

#define

GPDMA controller.

#define

Source peripheral.

#define

Destination peripheral.

#define

Source and destination peripherals.

#define

Memory to memory transfer.

#define

Memory to peripheral transfer.

#define

Peripheral to memory transfer.

#define

Peripheral to peripheral transfer.

#define

Master 0.

#define

Master 1.

#define

AHB burst size 1.

#define

AHB burst size 4.

#define

AHB burst size 8.

#define

AHB burst size 16.

#define

AHB burst size 20.

#define

AHB burst size 24.

#define

AHB burst size 28.

#define

AHB burst size 32.

#define

Destination data burst size.

#define

Source data burst size.

#define

Enable link list fetch done interrupt.

#define

Disable link list fetch done interrupt.

#define

DMA controller controls flow control.

#define

Source peripheral controls flow control.

#define

Destination peripheral controls flow control.

#define

Source and destination peripheral controls flow control.

#define

Enable link list mode.

#define

Disable link list mode.

#define

Enable source FIFO mode.

#define

Disable source FIFO mode.

#define

Enable destination FIFO mode.

#define

Disable destination FIFO mode.

#define

Enable memory fill.

#define

Disable memory fill.

#define

Memory one fill.

#define

Memory zero fill.

#define

Enable DMA protection.

#define

Disable DMA protection.

#define

Maximum transfer size per descriptor.

#define

Maximum FIFO size.

#define

Maximum number of callback types.

Enumeration Documentation#

sl_gpdma_callback_code_t#

sl_gpdma_callback_code_t

Enumeration that holds 8-bit codes used by the callback_type parameter in the sl_si91x_gpdma_unregister_callbacks function.

This enumeration defines the 8-bit codes for different types of DMA callbacks that can be unregistered.

Enumerator
SL_GPDMA_HRESP_ERROR_CB

HRESP error callback code.

SL_GPDMA_DESCRIPTOR_FETCH_DONE_CB

Descriptor fetch done callback code.

SL_GPDMA_TRANSFER_DONE_CB

Transfer done callback code.

SL_GPDMA_GPDMAC_ERROR_CB

GPDMA controller error callback code.


Typedef Documentation#

sl_gpdma_callback_t#

typedef void(* sl_gpdma_callback_t) () )()

Callback function type.


sl_si91x_gpdma_descriptor_t#

typedef RSI_GPDMA_DESC_T sl_si91x_gpdma_descriptor_t

GPDMA descriptor structure.


sl_si91x_gpdma_data_context_t#

typedef GPDMA_DATACONTEXT_T sl_si91x_gpdma_data_context_t

GPDMA data context structure.


sl_si91x_gpdma_descriptor_config_t#

typedef sl_si91x_gpdma_descriptor_t sl_si91x_gpdma_descriptor_config_t

GPDMA descriptor configuration structure.


sl_si91x_gpdma_handle_t#

typedef RSI_GPDMA_HANDLE_T sl_si91x_gpdma_handle_t

GPDMA handle type.


sl_si91x_gpdma_channel_config_t#

typedef RSI_GPDMA_CHA_CFG_T sl_si91x_gpdma_channel_config_t

GPDMA channel configuration structure.


sl_si91x_gpdma_init_t#

typedef RSI_GPDMA_INIT_T sl_si91x_gpdma_init_t

GPDMA initialization structure.


sl_si91x_gpdma_transfer_complete_cb#

typedef gpdmaTransferCompleteCB sl_si91x_gpdma_transfer_complete_cb

GPDMA transfer complete callback type.


Function Documentation#

sl_si91x_gpdma_init#

sl_status_t sl_si91x_gpdma_init ()

To initialize the GPDMA peripheral.

This API

  1. Enables the GPDMA clock

  2. Clears GPDMA NVIC interrupt

  3. Enables GPDMA NVIC interrupt

  4. Masks GPDMA interruptsAssigns

  5. Clears GPDMA interrupts

Returns

  • sl_status_t Initialization status:

    • SL_STATUS_OK - Initialization success.

    • SL_STATUS_NOT_INITIALIZED - Initialization failed.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpdma_allocate_channel#

sl_status_t sl_si91x_gpdma_allocate_channel (uint32_t * channel_no, uint32_t priority, uint32_t max_transfer_size)

To allocate a GPDMA channel for the transfer.

Parameters
TypeDirectionArgument NameDescription
uint32_t *[in]channel_no

Pointer to the channel number variable:

  • 0xFF: Automatically allocates an available channel for DMA transfer.

  • 0-7: Allocates the given channel for GPDMA transfer.

uint32_t[in]priority

Priority of the channel:

  • 0: priority 1.

  • 1: priority 2.

  • 2: priority 2

  • 3: priority 3

uint32_t[in]max_transfer_size

Maximum transfer size in the given channel.

This API checks the available GPDMA channels and allocates one. It sets the priority of the allocated channel and assigns the channel number to the channel_no variable. If no channel is available, it will return SL_GPDMA_NO_CHANNEL_AVAILABLE.

Note: Users can also initialize the desired channel number, and this API checks whether the desired channel is available and allocates the channel if available. If users want the driver to allocate an available channel, channel_no should be initialized to 0.

Returns

  • sl_status_t Channel allocation status:

    • SL_STATUS_OK - Channel allocated.

    • SL_STATUS_NOT_INITIALIZED - GPDMA not initialized.

    • SL_STATUS_INVALID_PARAMETER - Channel number is invalid.

    • SL_STATUS_GPDMA_NO_CHANNEL_AVAILABLE - All GPDMA channels are allocated.

    • SL_STATUS_GPDMA_CHANNEL_ALREADY_ALLOCATED - The desired channel is already allocated.

    • SL_STATUS_BUSY - Channel is busy.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpdma_deallocate_channel#

sl_status_t sl_si91x_gpdma_deallocate_channel (uint32_t channel_no)

To deallocate the GPDMA channel.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel_no

Channel number:

  • 0-7 for GPDMA.

This API deallocates the GPDMA channel if there is no ongoing transfer on the channel. Deallocating the channel will also unregister the callbacks for transfer complete and error.

Returns

  • sl_status_t Channel deallocation status:

    • SL_STATUS_OK - Channel deallocated.

    • SL_STATUS_BUSY - Cannot deallocate channel due to an ongoing transfer.

    • SL_STATUS_NOT_INITIALIZED - GPDMA not initialized.

    • SL_STATUS_INVALID_PARAMETER - Channel number is invalid.

    • SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED - Given channel is not allocated For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpdma_register_callbacks#

sl_status_t sl_si91x_gpdma_register_callbacks (uint32_t channel_no, sl_gpdma_callback_pointer_t * callback_t)

To register the GPDMA callbacks (transfer complete & error).

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel_no

Channel number:

  • 0-7 for GPDMA.

sl_gpdma_callback_pointer_t *[in]callback_t

Pointer to the structure containing callback functions.

This API registers the GPDMA callbacks for transfer complete and error events. The user must update the sl_dma_callback_t structure and pass its address to this function. A separate callback can be present for transfer complete and error for each channel.

Returns

  • sl_status_t Callback registration status:

    • SL_STATUS_OK - Callback registered successfully.

    • SL_STATUS_NOT_INITIALIZED - GPDMA peripheral not initialized.

    • SL_STATUS_INVALID_PARAMETER - Invalid channel number.

    • SL_STATUS_NULL_POINTER - Callback pointer is NULL.

    • SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED - Given channel is not allocated.

    • SL_STATUS_BUSY - channel is busy.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpdma_unregister_callbacks#

sl_status_t sl_si91x_gpdma_unregister_callbacks (uint32_t channel_no, uint8_t callback_type)

To unregister the GPDMA callbacks (transfer complete and error).

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel_no

Channel number:

  • 0-7 for UDMA0.

uint8_t[in]callback_type

Unregister the GPDMA callbacks based on the callback type (8-bit callback number):

  • SL_GPDMA_HRESP_ERROR_CB: Unregister HRESP error callback.

  • SL_GPDMA_DESCRIPTOR_FETCH_DONE_CB: Unregister descriptor fetch done callback.

  • SL_GPDMA_TRANSFER_DONE_CB: Unregister transfer complete callback.

  • SL_GPDMA_GPDMAC_ERROR_CB: Unregister GPDMA controller error callback.

This API unregisters the DMA callbacks for transfer complete and error events. Users need to update the 8-bit variable callback_type and pass it to the function. Each bit is mapped to a specific callback.

Returns

  • sl_status_t Callback unregistration status:

    • SL_STATUS_OK - Callback unregistered successfully.

    • SL_STATUS_NOT_INITIALIZED - GPDMA peripheral not initialized.

    • SL_STATUS_INVALID_PARAMETER - Invalid channel number or callback type.

    • SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED - Given channel is not allocated.

    • SL_STATUS_BUSY - Channel is busy.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpdma_transfer#

sl_status_t sl_si91x_gpdma_transfer (uint32_t channel, void * src, void * dest)

To start a simple memory-to-memory DMA transfer.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel

Channel number: 0-7

void *[in]src

Source address.

void *[in]dest

Destination address.

This API configures the DMA channel descriptor and initiates a simple memory-to-memory DMA transfer. Users need to pass the source address and destination address of the transfer along with the channel number.

Returns

  • sl_status_t DMA transfer status:

    • SL_STATUS_OK - Transfer success.

    • SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED - Given channel is not allocated.

    • SL_STATUS_NOT_INITIALIZED - GPDMA peripheral not initialized.

    • SL_STATUS_SUSPENDED - Transfer initialization failed.

    • SL_STATUS_INVALID_PARAMETER - Channel number is invalid or source or destination is NULL.

    • SL_STATUS_BUSY - Channel is busy.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpdma_stop_transfer#

sl_status_t sl_si91x_gpdma_stop_transfer (uint32_t channel_no)

To stop the GPDMA transfer.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel_no

Channel number:

  • 0-7 for GPDMA.

This API stops any active transfer on the channel by disabling the GPDMA channel. If there is no active transfer on the channel, this function returns SL_STATUS_IDLE.

Returns

  • sl_status_t DMA transfer status:

    • SL_STATUS_OK - Transfer stopped successfully.

    • SL_STATUS_IDLE - There is no active transfer on the channel.

    • SL_STATUS_NOT_INITIALIZED - GPDMA peripheral not initialized.

    • SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED - Given channel is not allocated.

    • SL_STATUS_INVALID_PARAMETER - Invalid channel number.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpdma_allocate_descriptor#

sl_status_t sl_si91x_gpdma_allocate_descriptor (sl_si91x_gpdma_descriptor_t * pDesc_memory, uint32_t transfer_size, uint32_t channel_number)

Allocates a GPDMA descriptor with default config for given channel based on tranfer size.

Parameters
TypeDirectionArgument NameDescription
sl_si91x_gpdma_descriptor_t *[inout]pDesc_memory

Pointer to the memory location where the descriptor will be allocated and initialized,this memory must be pre-allocated by the caller.

uint32_t[in]transfer_size

Size of the data transfer in bytes.

uint32_t[in]channel_number

GPDMA channel number 0-7 to be used for the transfer.

This function allocates GPDMA descriptor in the provided memory location, fills the descriptors with default values, and attaches it to the given channel. The descriptor is configured for the specified transfer size and channel number.

Returns

  • sl_status_t

    • SL_STATUS_OK: Descriptor successfully allocated and initialized.

    • SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_NOT_SUFFICIENT: descriptor memory buffer size is not sufficient.

    • SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_ALREADY_ALLOCATED : descriptor memory buffer already allocated to given channel.

    • SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED: Given channel is not allocated.

    • SL_STATUS_INVALID_PARAMETER: Invalid input parameters.

    • SL_STATUS_BUSY - Channel is busy. For more information on status codes, see SL STATUS DOCUMENTATION.


sl_Si91x_gpdma_deallocate_descriptor#

sl_status_t sl_Si91x_gpdma_deallocate_descriptor (uint32_t channel_number)

Deallocates a DMA descriptor for the specified channel number.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel_number

The channel number 0-7 from which to deallocate the descriptor.

This function deallocates a previously allocated DMA descriptor associated with the given channel number.

Returns

  • sl_status_t SL_STATUS_OK if the descriptor was successfully deallocated, SL_STATUS_INVALID_PARAMETER if the channel number is invalid, SL_STATUS_BUSY if the transfer is still in progress in given channel, SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED given channel is not allocated,

Note

  • The channel must be disabled before calling this function to avoid unpredictable behavior. For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpdma_build_descriptor#

sl_status_t sl_si91x_gpdma_build_descriptor (sl_si91x_gpdma_descriptor_t * pDescriptor_memory, sl_si91x_gpdma_descriptor_config_t * pDesc_config, uint32_t transfer_size, uint32_t channel_number)

Builds a GPDMA descriptor with the specified configuration.

Parameters
TypeDirectionArgument NameDescription
sl_si91x_gpdma_descriptor_t *[inout]pDescriptor_memory

Pointer to the memory location where the descriptor will be built. This memory must be pre-allocated by the caller.

sl_si91x_gpdma_descriptor_config_t *[in]pDesc_config

Pointer to the configuration structure containing the descriptor settings.

uint32_t[in]transfer_size

The size of the data transfer in bytes.

uint32_t[in]channel_number

The GPDMA 0-7 channel number to be used for the transfer.

This function initializes a GPDMA descriptor with the provided configuration. The descriptor can then be used for GPDMA operations.

Returns

  • Status of the operation.

    • SL_STATUS_OK: If the descriptor was successfully built.

    • SL_STATUS_INVALID_PARAMETER: If any of the input parameters are invalid.

    • SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_NOT_SUFFICIENT: descriptor memory buffer size is not sufficient.

    • SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_ALREADY_ALLOCATED : descriptor memory buffer already allocated to given channel.

    • SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED: Given channel is not allocated.

    • SL_STATUS_BUSY - Channel is busy. For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_gpdma_allocate_fifo#

sl_status_t sl_si91x_gpdma_allocate_fifo (uint32_t channel_no, uint32_t fifo_size)

Allocates a FIFO buffer of the specified size to a GPDMA channel.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel_no

The GPDMA channel number to allocate the FIFO for.

uint32_t[in]fifo_size

The size of the FIFO buffer to allocate (in bytes).

This function allocates a FIFO (First In, First Out) buffer of the specified size to the selected GPDMA channel.

Returns

  • Status of the operation.

    • SL_STATUS_OK: If the FIFO was successfully allocated.

    • SL_STATUS_INVALID_PARAMETER: If the channel number is invalid or the FIFO size is not supported.

    • SL_STATUS_GPDMA_FIFO_MEMORY_NOT_AVAILABLE: If the FIFO memory is not available.

    • SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED: Given channel is not allocated.

    • SL_STATUS_BUSY - Channel is busy.

Note

  • The availability of channels and maximum FIFO size may vary based on hardware configuration. For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_get_channel_fifo_size#

sl_status_t sl_si91x_get_channel_fifo_size (uint32_t channel_no, uint32_t * fifo_size)

Gets the FIFO size of a specified GPDMA channel.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel_no

The GPDMA channel number to query

uint32_t *[out]fifo_size

Pointer to store the retrieved FIFO size value

This function retrieves the FIFO buffer size configured for the specified GPDMA channel.

Returns

  • sl_status_t SL_STATUS_OK if successful, SL_STATUS_INVALID_PARAMETER if channel number is invalid, SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED if given channel is not allocated.

Note

  • The channel number should be within the valid range of available GPDMA channels.


sl_si91x_gpdma_get_channel_status#

sl_status_t sl_si91x_gpdma_get_channel_status (uint32_t channel_number)

Gets the current status of a specified GPDMA channel.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]channel_number

The GPDMA channel number for which to get the status

This function retrieves the status of the specified GPDMA channel.

Returns

  • status of the operation.

    • SL_STATUS_OK: If the channel is free.

    • SL_STATUS_BUSY: If the transfer is in progress for given channel.

    • SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED: If the channel is not allocated.

    • SL_STATUS_GPDMA_CHANNEL_ALREADY_ALLOCATED: If the channel is already allocated.


sl_si91x_gpdma_deinit#

sl_status_t sl_si91x_gpdma_deinit (void )

This function deinitializes the GPDMA driver.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This API performs the following actions:

  1. Deinitializes the GPDMA driver by disabling the GPDMA clock and NVIC interrupt.

  2. Clears any pending interrupts and resets the GPDMA driver context to NULL.

  3. Clears the callback functions for transfer completion, descriptor fetch completion, HRESP error, and GPDMA controller error.

  4. Resets the GPDMA resource data and channel allocation data to the default state.

Returns

  • Status of the operation.


Macro Definition Documentation#

SL_STATUS_GPDMA_CHANNEL_ALLOCATED#

#define SL_STATUS_GPDMA_CHANNEL_ALLOCATED
Value:
  (sl_status_t)0x61

Status code indicates that the DMA channel already allocated for another transfer.


SL_STATUS_GPDMA_NO_CHANNEL_AVAILABLE#

#define SL_STATUS_GPDMA_NO_CHANNEL_AVAILABLE
Value:
  (sl_status_t)0x62

Status code indicates that no DMA channel is available for allocation.


SL_STATUS_GPDMA_CHANNEL_ALREADY_UNALLOCATED#

#define SL_STATUS_GPDMA_CHANNEL_ALREADY_UNALLOCATED
Value:
  (sl_status_t)0X63

Status code indicates that the DMA channel is already unallocated.


SL_STATUS_GPDMA_CHANNEL_UNALLOCATED#

#define SL_STATUS_GPDMA_CHANNEL_UNALLOCATED
Value:
  (sl_status_t)0X64

Status code indicates that channel is not allocated for DMA transfer.


SL_STATUS_GPDMA_CHANNEL_ALREADY_ALLOCATED#

#define SL_STATUS_GPDMA_CHANNEL_ALREADY_ALLOCATED
Value:
  (sl_status_t)0x65

Status code indicates that the channel is not available for allocation.


SL_STATUS_GPDMA_FIFO_MEMORY_NOT_AVAILABLE#

#define SL_STATUS_GPDMA_FIFO_MEMORY_NOT_AVAILABLE
Value:
  (sl_status_t)0x66

Status code indicates that no DMA channel is available for allocation.


SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_ALREADY_ALLOCATED#

#define SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_ALREADY_ALLOCATED
Value:
  (sl_status_t)0x67

Status code indicates that the descriptor memory buffer is already allocated.


SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_NOT_SUFFICIENT#

#define SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_NOT_SUFFICIENT
Value:
  (sl_status_t)0x68

Status code indicates that the descriptor memory buffer is not sufficient.


SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED#

#define SL_STATUS_GPDMA_CHANNEL_NOT_ALLOCATED
Value:
  (sl_status_t)0x69

Status code indicates that the channel is not allocated for DMA transfer.


SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_NOT_ALLOCATED#

#define SL_STATUS_GPDMA_DESCRIPTOR_MEMORY_BUFFER_NOT_ALLOCATED
Value:
  (sl_status_t)0x6A

Status code indicates that Memory buffer is not allocated for the given channel.


SL_GPDMA_MAX_CHANNEL_PRIORITY#

#define SL_GPDMA_MAX_CHANNEL_PRIORITY
Value:
3

Maximum GPDMA channel priority.


SL_GPDMA_DATA_WIDTH_8#

#define SL_GPDMA_DATA_WIDTH_8
Value:
0x0

Data width 8 bits.


SL_GPDMA_DATA_WIDTH_16#

#define SL_GPDMA_DATA_WIDTH_16
Value:
0x1

Data width 16 bits.


SL_GPDMA_DATA_WIDTH_32#

#define SL_GPDMA_DATA_WIDTH_32
Value:
0x2

Data width 32 bits.


SL_GPDMACONTROLLER#

#define SL_GPDMACONTROLLER
Value:
0x0

GPDMA controller.


SL_SOURCE_PERIPHERAL#

#define SL_SOURCE_PERIPHERAL
Value:
0x1

Source peripheral.


SL_DESTINATION_PERIPHERAL#

#define SL_DESTINATION_PERIPHERAL
Value:
0x2

Destination peripheral.


SL_SRC_AND_DEST_PERIPHERALS#

#define SL_SRC_AND_DEST_PERIPHERALS
Value:
0x3

Source and destination peripherals.


SL_GPDMA_MEMORY_TO_MEMORY#

#define SL_GPDMA_MEMORY_TO_MEMORY
Value:
0x0

Memory to memory transfer.


SL_GPDMA_MEMORY_TO_PERIPHERAL#

#define SL_GPDMA_MEMORY_TO_PERIPHERAL
Value:
0x1

Memory to peripheral transfer.


SL_GPDMA_PERIPHERAL_TO_MEMORY#

#define SL_GPDMA_PERIPHERAL_TO_MEMORY
Value:
0x2

Peripheral to memory transfer.


SL_GPDMA_PERIPHERAL_TO_PERIPHERAL#

#define SL_GPDMA_PERIPHERAL_TO_PERIPHERAL
Value:
0x3

Peripheral to peripheral transfer.


SL_GPDMA_MASTER_ZERO#

#define SL_GPDMA_MASTER_ZERO
Value:
0x0

Master 0.


SL_GPDMA_MASTER_ONE#

#define SL_GPDMA_MASTER_ONE
Value:
0x1

Master 1.


SL_GPDMA_AHBBURST_SIZE_1#

#define SL_GPDMA_AHBBURST_SIZE_1
Value:
0b000

AHB burst size 1.


SL_GPDMA_AHBBURST_SIZE_4#

#define SL_GPDMA_AHBBURST_SIZE_4
Value:
0b001

AHB burst size 4.


SL_GPDMA_AHBBURST_SIZE_8#

#define SL_GPDMA_AHBBURST_SIZE_8
Value:
0b010

AHB burst size 8.


SL_GPDMA_AHBBURST_SIZE_16#

#define SL_GPDMA_AHBBURST_SIZE_16
Value:
0b011

AHB burst size 16.


SL_GPDMA_AHBBURST_SIZE_20#

#define SL_GPDMA_AHBBURST_SIZE_20
Value:
0b100

AHB burst size 20.


SL_GPDMA_AHBBURST_SIZE_24#

#define SL_GPDMA_AHBBURST_SIZE_24
Value:
0b101

AHB burst size 24.


SL_GPDMA_AHBBURST_SIZE_28#

#define SL_GPDMA_AHBBURST_SIZE_28
Value:
0b110

AHB burst size 28.


SL_GPDMA_AHBBURST_SIZE_32#

#define SL_GPDMA_AHBBURST_SIZE_32
Value:
0b111

AHB burst size 32.


SL_GPDMA_DESTINATION_DATA_BURST#

#define SL_GPDMA_DESTINATION_DATA_BURST
Value:
16

Destination data burst size.


SL_GPDMA_SOURCE_DATA_BURST#

#define SL_GPDMA_SOURCE_DATA_BURST
Value:
16

Source data burst size.


SL_LINK_LIST_INTERRUPT_ENABLE#

#define SL_LINK_LIST_INTERRUPT_ENABLE
Value:
1

Enable link list fetch done interrupt.


SL_LINK_LIST_INTERRUPT_DISABLE#

#define SL_LINK_LIST_INTERRUPT_DISABLE
Value:
0

Disable link list fetch done interrupt.


SL_GPDMAC_FL0W_CTRL#

#define SL_GPDMAC_FL0W_CTRL
Value:
0x0

DMA controller controls flow control.


SL_SOURCE_PERIPHERAL_CTRL#

#define SL_SOURCE_PERIPHERAL_CTRL
Value:
0x1

Source peripheral controls flow control.


SL_DESTINATION_PERIIPHERAL_CTRL#

#define SL_DESTINATION_PERIIPHERAL_CTRL
Value:
0x2

Destination peripheral controls flow control.


SL_SOURCE_DESTIATION_PERIPHERAL_CTRL#

#define SL_SOURCE_DESTIATION_PERIPHERAL_CTRL
Value:
0x3

Source and destination peripheral controls flow control.


SL_LINK_LIST_MODE_ENABLE#

#define SL_LINK_LIST_MODE_ENABLE
Value:
1

Enable link list mode.


SL_LINK_LIST_MODE_DISABLE#

#define SL_LINK_LIST_MODE_DISABLE
Value:
0

Disable link list mode.


SL_SOURCE_FIFO_MODE_ENABLE#

#define SL_SOURCE_FIFO_MODE_ENABLE
Value:
1

Enable source FIFO mode.


SL_SOURCE_FIFO_MODE_DISABLE#

#define SL_SOURCE_FIFO_MODE_DISABLE
Value:
0

Disable source FIFO mode.


SL_DESTINATION_FIFO_MODE_ENABLE#

#define SL_DESTINATION_FIFO_MODE_ENABLE
Value:
1

Enable destination FIFO mode.


SL_DESTINATION_FIFO_MODE_DISABLE#

#define SL_DESTINATION_FIFO_MODE_DISABLE
Value:
0

Disable destination FIFO mode.


SL_MEMORY_FILL_ENABLE#

#define SL_MEMORY_FILL_ENABLE
Value:
1

Enable memory fill.


SL_MEMORY_FILL_DISABLE#

#define SL_MEMORY_FILL_DISABLE
Value:
0

Disable memory fill.


SL_MEMORY_ONE_FILL#

#define SL_MEMORY_ONE_FILL
Value:
1

Memory one fill.


SL_MEMORY_ZERO_FILL#

#define SL_MEMORY_ZERO_FILL
Value:
0

Memory zero fill.


SL_DMA_PROTECTION_ENABLE#

#define SL_DMA_PROTECTION_ENABLE
Value:
1

Enable DMA protection.


SL_DMA_PROTECTION_DISABLE#

#define SL_DMA_PROTECTION_DISABLE
Value:
0

Disable DMA protection.


MAX_TRANSFER_PER_DESCRIPTOR#

#define MAX_TRANSFER_PER_DESCRIPTOR
Value:
4095

Maximum transfer size per descriptor.


SL_GPDMA_MAX_FIFO_SIZE#

#define SL_GPDMA_MAX_FIFO_SIZE
Value:
64

Maximum FIFO size.


SL_GPDMA_MAX_CALLBACK_TYPE#

#define SL_GPDMA_MAX_CALLBACK_TYPE
Value:
3

Maximum number of callback types.