LFN connection parameters.

Public Attributes#

uint8_t

Duration of LPA listening slot (millisecond) Specification range [15, 255].

uint8_t

Number of slots for which an LFN shall listen for LPA frames Specification range [1, 255].

Public Attribute Documentation#

discovery_slot_time_ms#

uint8_t sl_wisun_lfn_params_connection_t::discovery_slot_time_ms

Duration of LPA listening slot (millisecond) Specification range [15, 255].


Definition at line 54 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

discovery_slots#

uint8_t sl_wisun_lfn_params_connection_t::discovery_slots

Number of slots for which an LFN shall listen for LPA frames Specification range [1, 255].


Definition at line 57 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h