LFN network parameters.

Public Attributes#

uint16_t

Recommended address registration lifetime to be used by an LFN (minutes) Specification range [1440, 5040].

uint8_t

Interval during which an LFN waits for an FFN NA(EARO) response (minutes) Specification range [30, 120].

Public Attribute Documentation#

lfn_registration_lifetime_m#

uint16_t sl_wisun_lfn_params_network_t::lfn_registration_lifetime_m

Recommended address registration lifetime to be used by an LFN (minutes) Specification range [1440, 5040].


lfn_na_wait_duration_m#

uint8_t sl_wisun_lfn_params_network_t::lfn_na_wait_duration_m

Interval during which an LFN waits for an FFN NA(EARO) response (minutes) Specification range [30, 120].