LFN data layer parameters.
Public Attributes#
uint32_t
Time between LFN sampled listening points (milliseconds)
uint32_t
Minimum acceptable LFN unicast interval (milliseconds)
uint32_t
Maximum acceptable LFN unicast interval (milliseconds)
uint8_t
The number of LFN Broadcast Sync Period (parent defined) after which, having not received any messaging from its parent, an LFN assumes the parent is lost.
Public Attribute Documentation#
unicast_interval_ms#
uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_ms
Time between LFN sampled listening points (milliseconds)
Definition at line
65
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
unicast_interval_min_ms#
uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_min_ms
Minimum acceptable LFN unicast interval (milliseconds)
Definition at line
67
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
unicast_interval_max_ms#
uint32_t sl_wisun_lfn_params_data_layer_t::unicast_interval_max_ms
Maximum acceptable LFN unicast interval (milliseconds)
Definition at line
69
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
lfn_maintain_parent_time#
uint8_t sl_wisun_lfn_params_data_layer_t::lfn_maintain_parent_time
The number of LFN Broadcast Sync Period (parent defined) after which, having not received any messaging from its parent, an LFN assumes the parent is lost.
Specification range [1, 60]
Definition at line
74
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h