RPL parameters set.
Public Attributes#
RPL first DIS maximum delay (seconds)
RPL DIS maximum delay (seconds)
Delay for preferred parent selection after first DIO reception (seconds)
Maximum period of NS probes used to get samples for ETX calculation (seconds)
Number of samples used to calculate ETX during join state 4.
Number of samples used to refresh ETX.
RPL max candidate parents.
RPL max parents.
Public Attribute Documentation#
dis_max_delay_first_s#
uint16_t sl_wisun_params_rpl::dis_max_delay_first_s
RPL first DIS maximum delay (seconds)
136
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
dis_max_delay_s#
uint16_t sl_wisun_params_rpl::dis_max_delay_s
RPL DIS maximum delay (seconds)
138
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
init_parent_selection_s#
uint16_t sl_wisun_params_rpl::init_parent_selection_s
Delay for preferred parent selection after first DIO reception (seconds)
140
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
etx_probe_period_max_s#
uint16_t sl_wisun_params_rpl::etx_probe_period_max_s
Maximum period of NS probes used to get samples for ETX calculation (seconds)
142
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
etx_samples_init#
uint8_t sl_wisun_params_rpl::etx_samples_init
Number of samples used to calculate ETX during join state 4.
144
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
etx_samples_refresh#
uint8_t sl_wisun_params_rpl::etx_samples_refresh
Number of samples used to refresh ETX.
146
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
candidate_parents_max#
uint8_t sl_wisun_params_rpl::candidate_parents_max
RPL max candidate parents.
148
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
parents_max#
uint8_t sl_wisun_params_rpl::parents_max
RPL max parents.
150
of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h