LFN parameter set.
Public Attributes#
uint16_t
Version of this API.
LFN connection parameters.
LFN data layer parameters.
LFN network parameters.
LFN power parameters.
Public Attribute Documentation#
version#
uint16_t sl_wisun_lfn_params_t::version
Version of this API.
This field allows to store the parameters in an NVM and check on reload that they are compatible with the stack if there was an update.
connection#
sl_wisun_lfn_params_connection_t sl_wisun_lfn_params_t::connection
LFN connection parameters.
data_layer#
sl_wisun_lfn_params_data_layer_t sl_wisun_lfn_params_t::data_layer
LFN data layer parameters.