BR parameter set.
Public Attributes#
PAN configuration parameter set.
DHCP server parameter set.
PAN discovery parameter set.
Authentication parameter set.
Enable authentication of FAN 1.0 routers.
LFN parent parameter set.
MAC parameter set.
Misc parameter set.
MPL parameter set.
Maximum number of nodes supported by border router at once.
Reserved, set to zero.
RPL parameter set.
Traffic parameter set.
Version of this API.
Public Attribute Documentation#
configuration#
sl_wisun_br_params_configuration_t sl_wisun_br_connection_params_t::configuration
PAN configuration parameter set.
discovery#
sl_wisun_br_params_discovery_t sl_wisun_br_connection_params_t::discovery
PAN discovery parameter set.
eapol#
sl_wisun_br_params_eapol_t sl_wisun_br_connection_params_t::eapol
Authentication parameter set.
enable_ffn10#
uint8_t sl_wisun_br_connection_params_t::enable_ffn10
Enable authentication of FAN 1.0 routers.
lfn_parent#
sl_wisun_br_params_lfn_parent_t sl_wisun_br_connection_params_t::lfn_parent
LFN parent parameter set.
pan_capacity#
uint32_t sl_wisun_br_connection_params_t::pan_capacity
Maximum number of nodes supported by border router at once.
version#
uint32_t sl_wisun_br_connection_params_t::version
Version of this API.
This field allows to store the parameters in an NVM and check on reload that they are compatible with the stack if there was an update.