Traffic parameter set.

Public Attributes#

uint16_t

Maximum Receive Unit (MRU) for fragmented IPv6 packets in bytes. A larger packet will be silently discarded.

uint16_t

Maximum Transmission Unit (MTU) for 6LoWPAN packets in bytes. A larger packet will be fragmented using 6LoWPAN fragmentation.

uint8_t

Maximum number of 6LoWPAN/IPv6 fragments to send in a single EDFE transaction (0 to 10). 0 disables EDFE for fragmented packets.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

ipv6_mru#

uint16_t sl_wisun_params_traffic_s::ipv6_mru

Maximum Receive Unit (MRU) for fragmented IPv6 packets in bytes. A larger packet will be silently discarded.


lowpan_mtu#

uint16_t sl_wisun_params_traffic_s::lowpan_mtu

Maximum Transmission Unit (MTU) for 6LoWPAN packets in bytes. A larger packet will be fragmented using 6LoWPAN fragmentation.


max_edfe_fragment_count#

uint8_t sl_wisun_params_traffic_s::max_edfe_fragment_count

Maximum number of 6LoWPAN/IPv6 fragments to send in a single EDFE transaction (0 to 10). 0 disables EDFE for fragmented packets.


reserved#

uint8_t sl_wisun_params_traffic_s::reserved[3]

Reserved, set to zero.