Authentication parameter set.

Public Attributes#

uint8_t

If true, allow join state 2 to be skipped using cached credentials from the previous connection.

uint16_t

GTK_MAX_MISMATCH (minutes) Maximum time between a SUP detecting a GTKHASH mismatch and the SUP initiating Msg1 of the authentication flow.

uint16_t

Deprecated.

uint16_t

Deprecated.

uint16_t

Max delay of first key request (seconds)

uint16_t

Deprecated.

uint8_t

Maximum retransmission count.

uint16_t

Maximum duration for retransmissions (seconds)

uint16_t
uint16_t

Initial retransmission time (seconds)

uint16_t

LGTK_MAX_MISMATCH (minutes) Maximum time between a SUP detecting a LGTKHASH mismatch and the SUP initiating Msg1 of the authentication flow.

uint32_t

PMK lifetime (minutes)

uint32_t

PTK lifetime (minutes)

uint8_t

Reserved, set to zero.

uint16_t
uint8_t
uint16_t

Deprecated.

Public Attribute Documentation#

allow_skip#

uint8_t sl_wisun_params_eapol_s::allow_skip

If true, allow join state 2 to be skipped using cached credentials from the previous connection.


gtk_max_mismatch_m#

uint16_t sl_wisun_params_eapol_s::gtk_max_mismatch_m

GTK_MAX_MISMATCH (minutes) Maximum time between a SUP detecting a GTKHASH mismatch and the SUP initiating Msg1 of the authentication flow.


gtk_request_imax_m#

uint16_t sl_wisun_params_eapol_s::gtk_request_imax_m

Deprecated.


gtk_request_imin_m#

uint16_t sl_wisun_params_eapol_s::gtk_request_imin_m

Deprecated.


initial_key_max_s#

uint16_t sl_wisun_params_eapol_s::initial_key_max_s

Max delay of first key request (seconds)


initial_key_min_s#

uint16_t sl_wisun_params_eapol_s::initial_key_min_s

Deprecated.


initial_key_retry_limit#

uint8_t sl_wisun_params_eapol_s::initial_key_retry_limit

Maximum retransmission count.


initial_key_retry_max_limit_s#

uint16_t sl_wisun_params_eapol_s::initial_key_retry_max_limit_s

Maximum duration for retransmissions (seconds)


initial_key_retry_max_s#

uint16_t sl_wisun_params_eapol_s::initial_key_retry_max_s

Deprecated.


initial_key_retry_min_s#

uint16_t sl_wisun_params_eapol_s::initial_key_retry_min_s

Initial retransmission time (seconds)


lgtk_max_mismatch_m#

uint16_t sl_wisun_params_eapol_s::lgtk_max_mismatch_m

LGTK_MAX_MISMATCH (minutes) Maximum time between a SUP detecting a LGTKHASH mismatch and the SUP initiating Msg1 of the authentication flow.


pmk_lifetime_m#

uint32_t sl_wisun_params_eapol_s::pmk_lifetime_m

PMK lifetime (minutes)


ptk_lifetime_m#

uint32_t sl_wisun_params_eapol_s::ptk_lifetime_m

PTK lifetime (minutes)


reserved#

uint8_t sl_wisun_params_eapol_s::reserved[3]

Reserved, set to zero.


sec_prot_retry_timeout_s#

uint16_t sl_wisun_params_eapol_s::sec_prot_retry_timeout_s

Deprecated.


sec_prot_trickle#

sl_wisun_trickle_params_t sl_wisun_params_eapol_s::sec_prot_trickle

Deprecated.


sec_prot_trickle_expirations#

uint8_t sl_wisun_params_eapol_s::sec_prot_trickle_expirations

Deprecated.


temp_min_timeout_s#

uint16_t sl_wisun_params_eapol_s::temp_min_timeout_s

Deprecated.