Traffic parameter set.
Public Attributes#
Maximum Receive Unit (MRU) for fragmented IPv6 packets in bytes. A larger packet will be silently discarded.
Maximum Transmission Unit (MTU) for 6LoWPAN packets in bytes. A larger packet will be fragmented using 6LoWPAN fragmentation.
Maximum number of 6LoWPAN/IPv6 fragments to send in a single EDFE transaction (0 to 10). 0 disables EDFE for fragmented packets.
Reserved, set to zero.
Public Attribute Documentation#
ipv6_mru#
uint16_t sl_wisun_br_params_traffic_s::ipv6_mru
Maximum Receive Unit (MRU) for fragmented IPv6 packets in bytes. A larger packet will be silently discarded.
lowpan_mtu#
uint16_t sl_wisun_br_params_traffic_s::lowpan_mtu
Maximum Transmission Unit (MTU) for 6LoWPAN packets in bytes. A larger packet will be fragmented using 6LoWPAN fragmentation.
max_edfe_fragment_count#
uint8_t sl_wisun_br_params_traffic_s::max_edfe_fragment_count
Maximum number of 6LoWPAN/IPv6 fragments to send in a single EDFE transaction (0 to 10). 0 disables EDFE for fragmented packets.