MAC statistics.
Public Attributes#
Number of successfully received broadcast MAC frames.
Number of transmitted broadcast MAC frames.
Number of MAC CCA attempts.
Number of failed MAC transmissions due to CCA.
Cumulated idle duration in seconds.
Radio TX duration in milliseconds.
Reserved, set to zero.
Number of retried MAC transmissions.
MAC RX availability percentage.
Amount of successfully received MAC data in bytes. FCS is not included.
Number of successfully received MAC frames.
Number of successfully received MAC frames discarded during processing.
Number of successfully received MAC frames using mode_switch.
Number of failed reception using mode switch (no data after PHR or MDR Command).
Amount of transmitted MAC data in bytes. FCS is not included.
Number of transmitted MAC frames.
Number of failed MAC transmissions.
Number of transmitted MAC frames using mode switch.
Number of failed MAC frames transmission using mode switch.
Highest number of frames in the MAC transmission queue.
Current number of frames in the MAC transmission queue.
Public Attribute Documentation#
bc_rx_count#
uint32_t sl_wisun_statistics_mac_t::bc_rx_count
Number of successfully received broadcast MAC frames.
bc_tx_count#
uint32_t sl_wisun_statistics_mac_t::bc_tx_count
Number of transmitted broadcast MAC frames.
cca_attempts_count#
uint32_t sl_wisun_statistics_mac_t::cca_attempts_count
Number of MAC CCA attempts.
failed_cca_count#
uint32_t sl_wisun_statistics_mac_t::failed_cca_count
Number of failed MAC transmissions due to CCA.
idle_duration_s#
uint32_t sl_wisun_statistics_mac_t::idle_duration_s
Cumulated idle duration in seconds.
radio_tx_duration_ms#
uint32_t sl_wisun_statistics_mac_t::radio_tx_duration_ms
Radio TX duration in milliseconds.
rx_availability_percentage#
uint8_t sl_wisun_statistics_mac_t::rx_availability_percentage
MAC RX availability percentage.
rx_bytes#
uint32_t sl_wisun_statistics_mac_t::rx_bytes
Amount of successfully received MAC data in bytes. FCS is not included.
rx_drop_count#
uint32_t sl_wisun_statistics_mac_t::rx_drop_count
Number of successfully received MAC frames discarded during processing.
rx_ms_count#
uint32_t sl_wisun_statistics_mac_t::rx_ms_count
Number of successfully received MAC frames using mode_switch.
rx_ms_failed_count#
uint32_t sl_wisun_statistics_mac_t::rx_ms_failed_count
Number of failed reception using mode switch (no data after PHR or MDR Command).
tx_bytes#
uint32_t sl_wisun_statistics_mac_t::tx_bytes
Amount of transmitted MAC data in bytes. FCS is not included.
tx_failed_count#
uint32_t sl_wisun_statistics_mac_t::tx_failed_count
Number of failed MAC transmissions.
tx_ms_count#
uint32_t sl_wisun_statistics_mac_t::tx_ms_count
Number of transmitted MAC frames using mode switch.
tx_ms_failed_count#
uint32_t sl_wisun_statistics_mac_t::tx_ms_failed_count
Number of failed MAC frames transmission using mode switch.
tx_queue_peak#
uint16_t sl_wisun_statistics_mac_t::tx_queue_peak
Highest number of frames in the MAC transmission queue.
tx_queue_size#
uint16_t sl_wisun_statistics_mac_t::tx_queue_size
Current number of frames in the MAC transmission queue.