Public Attributes#

The ID of the source node.

uint8_t

uint8_t 1, bit 0-6 - Can represent endpoints from 1-127 unless used as a bitmask where endpoint 1-7 is represented.

uint8_t

uint8_t 1, bit 7 - Reserved

Public Attribute Documentation#

nodeId#

node_id_t _MULTICHAN_SOURCE_NODE_ID_::nodeId

The ID of the source node.


Definition at line 27 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

endpoint#

uint8_t _MULTICHAN_SOURCE_NODE_ID_::endpoint

uint8_t 1, bit 0-6 - Can represent endpoints from 1-127 unless used as a bitmask where endpoint 1-7 is represented.


Definition at line 30 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h

res#

uint8_t _MULTICHAN_SOURCE_NODE_ID_::res

uint8_t 1, bit 7 - Reserved


Definition at line 32 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h