Public Attributes#

void(*
uint8_t

Will be returned with transmit status Allows application to recognize frames.

uint8_t

Number of new destinations Array containing new destinations.

Public Attribute Documentation#

Handle#

void(* SRequestNewRouteDestinations::Handle) (void)

Definition at line 1757 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

iDestinationCount#

uint8_t SRequestNewRouteDestinations::iDestinationCount

Will be returned with transmit status Allows application to recognize frames.


Definition at line 1759 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

aNewDestinations#

uint8_t SRequestNewRouteDestinations::aNewDestinations[ZW_MAX_CACHED_RETURN_ROUTE_DESTINATIONS]

Number of new destinations Array containing new destinations.


Definition at line 1761 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h