Cluster Commands: Calendar#
This group describes the CLI commands for the Calendar cluster. Listed below is a description of the cluster: This cluster provides attributes and commands to assist applications in developing time and date based protocol.
Macros#
zcl calendar get-calendar [earliestStartTime:4] [minIssuerEventId:4] [numberOfCalendars:1] [calendarType:1] [providerId:4]
zcl calendar get-day-profiles [providerId:4] [issuerCalendarId:4] [startDayId:1] [numberOfDays:1]
zcl calendar get-week-profiles [providerId:4] [issuerCalendarId:4] [startWeekId:1] [numberOfWeeks:1]
zcl calendar get-seasons [providerId:4] [issuerCalendarId:4]
zcl calendar get-special-days [startTime:4] [numberOfEvents:1] [calendarType:1] [providerId:4] [issuerCalendarId:4]
zcl calendar get-cancellation
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_CALENDAR#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_CALENDAR
zcl calendar get-calendar [earliestStartTime:4] [minIssuerEventId:4] [numberOfCalendars:1] [calendarType:1] [providerId:4]
This command initiates PublishCalendar command(s) for scheduled Calendar updates.
earliestStartTime - UTC_TIME
minIssuerEventId - INT32U
numberOfCalendars - INT8U
calendarType - CalendarType [ENUM8]
providerId - INT32U See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_DAY_PROFILES#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_DAY_PROFILES
zcl calendar get-day-profiles [providerId:4] [issuerCalendarId:4] [startDayId:1] [numberOfDays:1]
This command initiates one or more PublishDayProfile commands for the referenced Calendar.
providerId - INT32U
issuerCalendarId - INT32U
startDayId - INT8U
numberOfDays - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_WEEK_PROFILES#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_WEEK_PROFILES
zcl calendar get-week-profiles [providerId:4] [issuerCalendarId:4] [startWeekId:1] [numberOfWeeks:1]
This command initiates one or more PublishWeekProfile commands for the referenced Calendar.
providerId - INT32U
issuerCalendarId - INT32U
startWeekId - INT8U
numberOfWeeks - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_SEASONS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_SEASONS
zcl calendar get-seasons [providerId:4] [issuerCalendarId:4]
This command initiates one or more PublishSeasons commands for the referenced Calendar.
providerId - INT32U
issuerCalendarId - INT32U
EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_SPECIAL_DAYS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_SPECIAL_DAYS
zcl calendar get-special-days [startTime:4] [numberOfEvents:1] [calendarType:1] [providerId:4] [issuerCalendarId:4]
This command initiates one or more PublishSpecialDays commands for the scheduled Special Day Table updates.
startTime - UTC_TIME
numberOfEvents - INT8U
calendarType - CalendarType [ENUM8]
providerId - INT32U
issuerCalendarId - INT32U See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_CANCELLATION#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_CALENDAR_GET_CANCELLATION
zcl calendar get-cancellation
This command initiates the return of the last CancelCalendar command held on the associated server.