Modules#
Identify Server#
API and Callbacks for the Identify Cluster Server Component.
Silicon Labs implementation of the Identify cluster. It requires extending to integrate the code with the hardware, for example to make a light blink during identify.
This group describes the CLI commands for the Identify cluster. Listed below is a description of the cluster: Attributes and commands for putting a device into Identification mode (e.g. flashing a light).
Macros#
zcl identify off [endpoint:1]
zcl identify on [endpoint:1] [time:2]
zcl identify id [identifyTime:2]
zcl identify query
zcl identify ez-mode [action:1]
zcl identify trigger [effectId:1] [effectVariant:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_OFF#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_OFF
zcl identify off [endpoint:1]
Writes the IdentifyTime attribute
endpoint - INT8U - The endpoint on which to stop identifying
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_ON#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ZCL_IDENTIFY_ON
zcl identify on [endpoint:1] [time:2]
Writes the IdentifyTime attribute
endpoint - INT8U - The endpoint on the device which should begin identifying
time - INT16U - The number of seconds to spend identifying
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ID#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_ID
zcl identify id [identifyTime:2]
Command description for Identify
identifyTime - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_QUERY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_QUERY
zcl identify query
Command description for IdentifyQuery
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_EZ_MODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_EZ_MODE
zcl identify ez-mode [action:1]
Invoke EZMode on an Identify Server
action - BITMAP8
EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_TRIGGER#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_IDENTIFY_TRIGGER
zcl identify trigger [effectId:1] [effectVariant:1]
Command description for TriggerEffect
effectId - IdentifyEffectIdentifier [ENUM8]
effectVariant - IdentifyEffectVariant [ENUM8] See Also